<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Set GPIO input pull-down in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Set-GPIO-input-pull-down/m-p/787130#M121957</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Community,&lt;/P&gt;&lt;P&gt;I'm working on i.MX6 Dual Lite sabre-SD.&lt;/P&gt;&lt;P&gt;I'm trying to set gpio to input pull-down.&lt;/P&gt;&lt;P&gt;Here is my settings in dtsi.&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&amp;nbsp;MX6QDL_PAD_SD2_CMD__GPIO1_IO11&amp;nbsp; 0x80000000&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But this settings will set gpio input pull-high.&lt;/P&gt;&lt;P&gt;How can I set it to input pull-down?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advanced!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 12 Oct 2018 06:15:49 GMT</pubDate>
    <dc:creator>wangtsungli</dc:creator>
    <dc:date>2018-10-12T06:15:49Z</dc:date>
    <item>
      <title>Set GPIO input pull-down</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Set-GPIO-input-pull-down/m-p/787130#M121957</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Community,&lt;/P&gt;&lt;P&gt;I'm working on i.MX6 Dual Lite sabre-SD.&lt;/P&gt;&lt;P&gt;I'm trying to set gpio to input pull-down.&lt;/P&gt;&lt;P&gt;Here is my settings in dtsi.&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&amp;nbsp;MX6QDL_PAD_SD2_CMD__GPIO1_IO11&amp;nbsp; 0x80000000&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But this settings will set gpio input pull-high.&lt;/P&gt;&lt;P&gt;How can I set it to input pull-down?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advanced!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Oct 2018 06:15:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Set-GPIO-input-pull-down/m-p/787130#M121957</guid>
      <dc:creator>wangtsungli</dc:creator>
      <dc:date>2018-10-12T06:15:49Z</dc:date>
    </item>
    <item>
      <title>Re: Set GPIO input pull-down</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Set-GPIO-input-pull-down/m-p/787131#M121958</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi tsung&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"8" means that pin does not need config according to documentation :&lt;/P&gt;&lt;P&gt;linux/Documentation/devicetree/bindings/pinctrl/fsl,imx-pinctrl.txt&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/Documentation/devicetree/bindings/pinctrl/fsl,imx-pinctrl.txt?h=imx_4.1.15_2.0.0_ga" title="https://source.codeaurora.org/external/imx/linux-imx/tree/Documentation/devicetree/bindings/pinctrl/fsl,imx-pinctrl.txt?h=imx_4.1.15_2.0.0_ga"&gt;fsl,imx-pinctrl.txt\pinctrl\bindings\devicetree\Documentation - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;so one can remove it and set appropriate pull bits as described in sect.36.4.460 Pad Control Register&lt;/P&gt;&lt;P&gt;(IOMUXC_SW_PAD_CTL_PAD_SD2_CMD) i.MX6DQ Reference Manual&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Oct 2018 08:02:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Set-GPIO-input-pull-down/m-p/787131#M121958</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-10-12T08:02:16Z</dc:date>
    </item>
  </channel>
</rss>