<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Synchronizing between drivers in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Synchronizing-between-drivers/m-p/786927#M121919</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using imx6ull based board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a connected same ADC device in ecspi3 and ecspi4. So that it uses the same device driver.&lt;/P&gt;&lt;P&gt;Each device generated ADC ready interrupts at every 10 msec.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to implement a 5msec delay between the devices. i.e. if I'm getting interrupt from device1 first means after 5msec interrupt from device2 should be received.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Simply, Delay between interrupts of the same device is 10msec and delay between the devices is 5mesc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How to implement this in kernel?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 04 Sep 2018 05:58:03 GMT</pubDate>
    <dc:creator>mathew_k_t</dc:creator>
    <dc:date>2018-09-04T05:58:03Z</dc:date>
    <item>
      <title>Synchronizing between drivers</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Synchronizing-between-drivers/m-p/786927#M121919</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using imx6ull based board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a connected same ADC device in ecspi3 and ecspi4. So that it uses the same device driver.&lt;/P&gt;&lt;P&gt;Each device generated ADC ready interrupts at every 10 msec.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to implement a 5msec delay between the devices. i.e. if I'm getting interrupt from device1 first means after 5msec interrupt from device2 should be received.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Simply, Delay between interrupts of the same device is 10msec and delay between the devices is 5mesc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How to implement this in kernel?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Sep 2018 05:58:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Synchronizing-between-drivers/m-p/786927#M121919</guid>
      <dc:creator>mathew_k_t</dc:creator>
      <dc:date>2018-09-04T05:58:03Z</dc:date>
    </item>
  </channel>
</rss>