<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックimx6q) How to test SPI, UART, CAN ?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6q-How-to-test-SPI-UART-CAN/m-p/786833#M121904</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;I want to test imx6q-sabresd. The device driver seems to be properly configured.&lt;/P&gt;&lt;P&gt;I want to know if there are test codes.&lt;/P&gt;&lt;P&gt;For example, the test code can transfer the spi data of the imx6 board to another board.&lt;/P&gt;&lt;P&gt;(The data received from the imx6 board can do something else through the test code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ps. add questions.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 04 Sep 2018 09:38:13 GMT</pubDate>
    <dc:creator>ktc7270</dc:creator>
    <dc:date>2018-09-04T09:38:13Z</dc:date>
    <item>
      <title>imx6q) How to test SPI, UART, CAN ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6q-How-to-test-SPI-UART-CAN/m-p/786833#M121904</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;I want to test imx6q-sabresd. The device driver seems to be properly configured.&lt;/P&gt;&lt;P&gt;I want to know if there are test codes.&lt;/P&gt;&lt;P&gt;For example, the test code can transfer the spi data of the imx6 board to another board.&lt;/P&gt;&lt;P&gt;(The data received from the imx6 board can do something else through the test code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ps. add questions.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Sep 2018 09:38:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6q-How-to-test-SPI-UART-CAN/m-p/786833#M121904</guid>
      <dc:creator>ktc7270</dc:creator>
      <dc:date>2018-09-04T09:38:13Z</dc:date>
    </item>
    <item>
      <title>Re: imx6q) How to test SPI, UART, CAN ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6q-How-to-test-SPI-UART-CAN/m-p/786834#M121905</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi kangta&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for testing one can use unit tests described in Chapter 9 Unit Tests attached Linux Manual&lt;/P&gt;&lt;P&gt;imx-test&lt;BR /&gt;&lt;A href="https://source.codeaurora.org/external/imx/imx-test/tree/?h=imx_4.9.88_2.0.0_ga"&gt;https://source.codeaurora.org/external/imx/imx-test/tree/?h=imx_4.9.88_2.0.0_ga&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Sep 2018 23:17:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6q-How-to-test-SPI-UART-CAN/m-p/786834#M121905</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-09-04T23:17:39Z</dc:date>
    </item>
    <item>
      <title>Re: imx6q) How to test SPI, UART, CAN ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6q-How-to-test-SPI-UART-CAN/m-p/786837#M121908</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;if users use i.MX6Q board designed by Forlinx, generally the related codes are provided.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Rgds,&lt;/P&gt;&lt;P&gt;Grace&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Sep 2018 08:16:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6q-How-to-test-SPI-UART-CAN/m-p/786837#M121908</guid>
      <dc:creator>winy2014</dc:creator>
      <dc:date>2018-09-06T08:16:54Z</dc:date>
    </item>
  </channel>
</rss>