<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Explanation of pixel-bitrate, CSI1_PHY_REF clk and CSI1_CORE clk from MIPI-CSI2 in i.MX8M?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Explanation-of-pixel-bitrate-CSI1-PHY-REF-clk-and-CSI1-CORE-clk/m-p/786827#M121902</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm porting&amp;nbsp;a new MIPI 4-lane camera with bayer raw format to i.MX8M. But the image doesn't come out. I would like to know the relationship between pixel-rate and the settings of&amp;nbsp;IMX8MQ_CLK_CSI1_PHY_REF_SRC and IMX8MQ_CLK_CSI1_CORE_SRC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My&amp;nbsp;camera been configured by follow settings:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;The camera use 4-lanes to output Bayer RAW, DPHY=400MHz, 800Mbps.&lt;/LI&gt;&lt;LI&gt;The current pixel&amp;nbsp;rate is:&amp;nbsp;1920x1080x30fps= 62,208,000 pixels/second.&lt;/LI&gt;&lt;LI&gt;The pixel format is RAW8, bitrate is: 62,208,000x8 = 497,664,000bps.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And for the MIPI-CSI2 receiver settings on i.MX8 (fsl-imx8mq.dtsi) is:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;IMX8MQ_CLK_CSI1_CORE_DIV: 266MHz&lt;/LI&gt;&lt;LI&gt;IMX8MQ_CLK_CSI1_PHY_REF_DIV: 200MHz&lt;/LI&gt;&lt;LI&gt;IMX8MQ_CLK_CSI1_ESC_DIV: 66MHz&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;Q1.&lt;/SPAN&gt;&amp;nbsp;Should the PHY_REF clock be configured by 200MHz,&amp;nbsp;400MHz or 800MHz,&amp;nbsp;when&amp;nbsp;my camera is running at 400MHz/800Mbps?&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;Q2.&lt;/SPAN&gt; Do you named 4-lane mode by Quad Pixel Mode?&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;Q3.&lt;/SPAN&gt; To set the MIPI-CSI core_clk properly, it should be faster than the&amp;nbsp;&lt;SPAN&gt;actual bitrate at&lt;/SPAN&gt; &lt;SPAN&gt;single&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;lane: 496,664,000/4 = 124,416,000bps, or just faster than 496,664,000bps?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;Q4.&lt;/SPAN&gt; A&lt;SPAN&gt;ccording to &lt;A _jive_internal="true" href="https://community.nxp.com/message/1065269?commentID=1065269#comment-1065269" rel="noopener noreferrer" target="_blank"&gt;this thread&lt;/A&gt;, I could&amp;nbsp;&amp;nbsp;modify device tree and&amp;nbsp;&lt;SPAN&gt;IMX8MQ_CLK_CSI1_CORE_SRC by&amp;nbsp;clk-imx8mq.c&lt;/SPAN&gt;?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;IMG alt="pastedImage_3.png" src="https://community.nxp.com/t5/image/serverpage/image-id/68720i546DC238ADCC10F7/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm studying the reference manual, and got confused&amp;nbsp;by&amp;nbsp;clk, clk_ui descriptions and the device tree parameters:&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;Q5.&lt;/SPAN&gt; Which clock is mapped to IMX8MQ_CLK_CSI1_CORE_SRC? the clk or clk_ui?&lt;/P&gt;&lt;P&gt;&lt;SPAN class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;IMG alt="pastedImage_2.png" src="https://community.nxp.com/t5/image/serverpage/image-id/68622i3195719518D1FF0B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The current progress&amp;nbsp;of my porting&amp;nbsp;is I'm stuck at mx6s_capture.c, so I'm trying to find out if all the clock had been settle properly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the IRQ handler been triggered several times, but no any image comes to buffer (mx6s_csi_frame_done() not been called ever). And there's no error bit been set in status register (CSI_CSISR).&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="keyword token"&gt;static&lt;/SPAN&gt; irqreturn_t &lt;SPAN class="token function"&gt;mx6s_csi_irq_handler&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt; irq&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;data&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
 &lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;

 &lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;status &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt; BIT_DMA_TSF_DONE_FB1&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&amp;amp;&lt;/SPAN&gt;
 &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;status &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt; BIT_DMA_TSF_DONE_FB2&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
 &lt;SPAN class="comment token"&gt;/* For both FB1 and FB2 interrupter bits set case,
 * CSI DMA is work in one of FB1 and FB2 buffer,
 * but software can not know the state.
 * Skip it to avoid base address updated
 * when csi work in field0 and field1 will write to
 * new base address.
 * PDM TKT230775 */&lt;/SPAN&gt;
 &lt;SPAN class="token function"&gt;pr_debug&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="string token"&gt;"Skip two frames\n"&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;else&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;status &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt; BIT_DMA_TSF_DONE_FB1&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
 &lt;SPAN class="token function"&gt;mx6s_csi_frame_done&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;csi_dev&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; false&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;else&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;status &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt; BIT_DMA_TSF_DONE_FB2&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
 &lt;SPAN class="token function"&gt;mx6s_csi_frame_done&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;csi_dev&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; false&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;I'm also checked the CSI_CSICR[31:16] for&amp;nbsp;the "frame count", and the value is not zero, and&amp;nbsp;not matched with the frame count inside the output_frame_count register of camera.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;and looking&amp;nbsp;forward for your reply.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 02 Nov 2020 14:09:07 GMT</pubDate>
    <dc:creator>michaeltang</dc:creator>
    <dc:date>2020-11-02T14:09:07Z</dc:date>
    <item>
      <title>Explanation of pixel-bitrate, CSI1_PHY_REF clk and CSI1_CORE clk from MIPI-CSI2 in i.MX8M?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Explanation-of-pixel-bitrate-CSI1-PHY-REF-clk-and-CSI1-CORE-clk/m-p/786827#M121902</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm porting&amp;nbsp;a new MIPI 4-lane camera with bayer raw format to i.MX8M. But the image doesn't come out. I would like to know the relationship between pixel-rate and the settings of&amp;nbsp;IMX8MQ_CLK_CSI1_PHY_REF_SRC and IMX8MQ_CLK_CSI1_CORE_SRC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My&amp;nbsp;camera been configured by follow settings:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;The camera use 4-lanes to output Bayer RAW, DPHY=400MHz, 800Mbps.&lt;/LI&gt;&lt;LI&gt;The current pixel&amp;nbsp;rate is:&amp;nbsp;1920x1080x30fps= 62,208,000 pixels/second.&lt;/LI&gt;&lt;LI&gt;The pixel format is RAW8, bitrate is: 62,208,000x8 = 497,664,000bps.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And for the MIPI-CSI2 receiver settings on i.MX8 (fsl-imx8mq.dtsi) is:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;IMX8MQ_CLK_CSI1_CORE_DIV: 266MHz&lt;/LI&gt;&lt;LI&gt;IMX8MQ_CLK_CSI1_PHY_REF_DIV: 200MHz&lt;/LI&gt;&lt;LI&gt;IMX8MQ_CLK_CSI1_ESC_DIV: 66MHz&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;Q1.&lt;/SPAN&gt;&amp;nbsp;Should the PHY_REF clock be configured by 200MHz,&amp;nbsp;400MHz or 800MHz,&amp;nbsp;when&amp;nbsp;my camera is running at 400MHz/800Mbps?&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;Q2.&lt;/SPAN&gt; Do you named 4-lane mode by Quad Pixel Mode?&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;Q3.&lt;/SPAN&gt; To set the MIPI-CSI core_clk properly, it should be faster than the&amp;nbsp;&lt;SPAN&gt;actual bitrate at&lt;/SPAN&gt; &lt;SPAN&gt;single&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;lane: 496,664,000/4 = 124,416,000bps, or just faster than 496,664,000bps?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;Q4.&lt;/SPAN&gt; A&lt;SPAN&gt;ccording to &lt;A _jive_internal="true" href="https://community.nxp.com/message/1065269?commentID=1065269#comment-1065269" rel="noopener noreferrer" target="_blank"&gt;this thread&lt;/A&gt;, I could&amp;nbsp;&amp;nbsp;modify device tree and&amp;nbsp;&lt;SPAN&gt;IMX8MQ_CLK_CSI1_CORE_SRC by&amp;nbsp;clk-imx8mq.c&lt;/SPAN&gt;?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;IMG alt="pastedImage_3.png" src="https://community.nxp.com/t5/image/serverpage/image-id/68720i546DC238ADCC10F7/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm studying the reference manual, and got confused&amp;nbsp;by&amp;nbsp;clk, clk_ui descriptions and the device tree parameters:&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;Q5.&lt;/SPAN&gt; Which clock is mapped to IMX8MQ_CLK_CSI1_CORE_SRC? the clk or clk_ui?&lt;/P&gt;&lt;P&gt;&lt;SPAN class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;IMG alt="pastedImage_2.png" src="https://community.nxp.com/t5/image/serverpage/image-id/68622i3195719518D1FF0B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The current progress&amp;nbsp;of my porting&amp;nbsp;is I'm stuck at mx6s_capture.c, so I'm trying to find out if all the clock had been settle properly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the IRQ handler been triggered several times, but no any image comes to buffer (mx6s_csi_frame_done() not been called ever). And there's no error bit been set in status register (CSI_CSISR).&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="keyword token"&gt;static&lt;/SPAN&gt; irqreturn_t &lt;SPAN class="token function"&gt;mx6s_csi_irq_handler&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt; irq&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;data&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
 &lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;

 &lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;status &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt; BIT_DMA_TSF_DONE_FB1&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&amp;amp;&lt;/SPAN&gt;
 &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;status &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt; BIT_DMA_TSF_DONE_FB2&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
 &lt;SPAN class="comment token"&gt;/* For both FB1 and FB2 interrupter bits set case,
 * CSI DMA is work in one of FB1 and FB2 buffer,
 * but software can not know the state.
 * Skip it to avoid base address updated
 * when csi work in field0 and field1 will write to
 * new base address.
 * PDM TKT230775 */&lt;/SPAN&gt;
 &lt;SPAN class="token function"&gt;pr_debug&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="string token"&gt;"Skip two frames\n"&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;else&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;status &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt; BIT_DMA_TSF_DONE_FB1&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
 &lt;SPAN class="token function"&gt;mx6s_csi_frame_done&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;csi_dev&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; false&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;else&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;status &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt; BIT_DMA_TSF_DONE_FB2&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
 &lt;SPAN class="token function"&gt;mx6s_csi_frame_done&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;csi_dev&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; false&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;I'm also checked the CSI_CSICR[31:16] for&amp;nbsp;the "frame count", and the value is not zero, and&amp;nbsp;not matched with the frame count inside the output_frame_count register of camera.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;and looking&amp;nbsp;forward for your reply.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Nov 2020 14:09:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Explanation-of-pixel-bitrate-CSI1-PHY-REF-clk-and-CSI1-CORE-clk/m-p/786827#M121902</guid>
      <dc:creator>michaeltang</dc:creator>
      <dc:date>2020-11-02T14:09:07Z</dc:date>
    </item>
    <item>
      <title>Re: Explanation of pixel-bitrate, CSI1_PHY_REF clk and CSI1_CORE clk from MIPI-CSI2 in i.MX8M?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Explanation-of-pixel-bitrate-CSI1-PHY-REF-clk-and-CSI1-CORE-clk/m-p/786828#M121903</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i.MX8M processor has 2 MIPI-CSI2 interfaces.&lt;BR /&gt;Each one support up to 4 data lanes&lt;BR /&gt;It supports from 80Mbps to 1.5Gbps data rate in high speed operation&lt;BR /&gt;Amd it supports 10Mbps data rate in low power operation&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Nov 2019 08:09:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Explanation-of-pixel-bitrate-CSI1-PHY-REF-clk-and-CSI1-CORE-clk/m-p/786828#M121903</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2019-11-14T08:09:07Z</dc:date>
    </item>
  </channel>
</rss>