<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Error Using MfgTool iMXRT1052 QSPI Flash Boot</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Error-Using-MfgTool-iMXRT1052-QSPI-Flash-Boot/m-p/786061#M121837</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am attempting to bring up a board that has an iMXRT1052 connected to a QuadSPI Flash that is meant to be the boot location for the code. The XIP examples that I have used on the EVKB board work just fine. I am attempting to use the MfgTool on the board through USB to program the flash. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can create the boot_image.sb file using the tool, but when I start the MfgTool to program the flash I get "kStatus_FlexSPINOR_SFDP_NotFound" as an error message in the log file and the MfgTool fails. My boot pins are set to the serial download mode and the device shows up properly in the MfgTool before I attempt to program.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For a test I am trying to use the SDK evkbimxrt1050_hello_world example and have modified the XIP code to run from QSPI according to the Application Notes provided on NXP's page. I am also able to use the FlexSpi Nor Polling Transfer example project to correctly read and program the flash so I know the flash is electrically sound.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using MCUXpresso V10.2 and SDK 2.4.0 for the EVKB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any idea on what I could be doing wrong here?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Eric&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 06 Jul 2018 14:31:40 GMT</pubDate>
    <dc:creator>ebollerman</dc:creator>
    <dc:date>2018-07-06T14:31:40Z</dc:date>
    <item>
      <title>Error Using MfgTool iMXRT1052 QSPI Flash Boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-Using-MfgTool-iMXRT1052-QSPI-Flash-Boot/m-p/786061#M121837</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am attempting to bring up a board that has an iMXRT1052 connected to a QuadSPI Flash that is meant to be the boot location for the code. The XIP examples that I have used on the EVKB board work just fine. I am attempting to use the MfgTool on the board through USB to program the flash. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can create the boot_image.sb file using the tool, but when I start the MfgTool to program the flash I get "kStatus_FlexSPINOR_SFDP_NotFound" as an error message in the log file and the MfgTool fails. My boot pins are set to the serial download mode and the device shows up properly in the MfgTool before I attempt to program.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For a test I am trying to use the SDK evkbimxrt1050_hello_world example and have modified the XIP code to run from QSPI according to the Application Notes provided on NXP's page. I am also able to use the FlexSpi Nor Polling Transfer example project to correctly read and program the flash so I know the flash is electrically sound.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using MCUXpresso V10.2 and SDK 2.4.0 for the EVKB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any idea on what I could be doing wrong here?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Eric&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Jul 2018 14:31:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-Using-MfgTool-iMXRT1052-QSPI-Flash-Boot/m-p/786061#M121837</guid>
      <dc:creator>ebollerman</dc:creator>
      <dc:date>2018-07-06T14:31:40Z</dc:date>
    </item>
    <item>
      <title>Re: Error Using MfgTool iMXRT1052 QSPI Flash Boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-Using-MfgTool-iMXRT1052-QSPI-Flash-Boot/m-p/786062#M121838</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eric&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;issue is communicated internally.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jul 2018 23:39:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-Using-MfgTool-iMXRT1052-QSPI-Flash-Boot/m-p/786062#M121838</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-07-12T23:39:10Z</dc:date>
    </item>
    <item>
      <title>Re: Error Using MfgTool iMXRT1052 QSPI Flash Boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-Using-MfgTool-iMXRT1052-QSPI-Flash-Boot/m-p/786063#M121839</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are experiencing the same problem with the design on our board.&amp;nbsp; We are using the optional 'secondary pinmux' port pins to connect to our QSPI flash.&amp;nbsp; We can load and run the "evkbimxrt1050_flexspi_nor_polling_transfer" example project from RAM.&amp;nbsp; It erases, writes, reads, and verifies the external QSPI flash device on our board.&amp;nbsp; We are using the ISSI IS25LP016D-JBLE (16Mb) part.&amp;nbsp; We are unable to load our XIP image using the MfgTool (BLHost) over UART (no OpenSDA chip on our board) and receive the following message: "kStatus_FlexSPINOR_SFDP_NotFound", when we try using the blhost -V -p COM7,115200 -- configure-memory 0x09 0x2000 command.&amp;nbsp; We have tried several QCB (QSPI Configuration Block) option settings with the -- fill-memory 0x2000 0x04 0xC0000006; 0xC0000046 ('secondary pinmux' setting); 0xC0000106 (Quad Enable in bit 6 on this device); 0xC0000146, etc. None work.&amp;nbsp; A similar error is received while trying to load the "evkbimxrt1050_led_blinky" image using the MCUXpresso IDE via a LPC-Link2 over the SWJ-DP interface (using SWD).&amp;nbsp; We get this message:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/72926i0192D8EC14446E97/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When using the following &lt;STRONG style="font-size: 11.0pt; "&gt;&lt;EM&gt;Project Properties-&amp;gt;C/C++ Build-&amp;gt;MCU Settings&lt;/EM&gt;&lt;/STRONG&gt;:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_4.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/73521iAC519291905EBAD9/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yet, again, when we load and run the "evkbimxrt1050_flexspi_nor_polling_transfer" example project from RAM, everything works as expected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using MCUXpresso IDE v10.3.0 [Build 2200] [2018-12-03] and SDK_2.x_EVKB_IMXRT1050 version 2.4.2, manifest version 3.3.0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help will be greatly appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards and thanks in advance,&lt;/P&gt;&lt;P&gt;-Roger&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Apr 2019 13:30:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-Using-MfgTool-iMXRT1052-QSPI-Flash-Boot/m-p/786063#M121839</guid>
      <dc:creator>rogerc1894</dc:creator>
      <dc:date>2019-04-08T13:30:07Z</dc:date>
    </item>
    <item>
      <title>Re: Error Using MfgTool iMXRT1052 QSPI Flash Boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-Using-MfgTool-iMXRT1052-QSPI-Flash-Boot/m-p/786064#M121840</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Roger, I'm having a similar error using NXP-MCUBootUtility, V1.4.0.&amp;nbsp; We are using the ISSI IS25WP064AJBLE part using the same pins as the EVKB board.&amp;nbsp; I've tried a PEMicro Multilink, and a Segger JLink.&amp;nbsp; I even routed my own SWD interface adapter to try to problem my 1052 board using a HID to control the reset line and a UART for the sdphost and blhost commands.&amp;nbsp; The process gets stuck at the same&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;"kStatus_FlexSPINOR_SFDP_NotFound", when we try using the blhost&amp;nbsp; -p COM5,115200 -- configure-memory 0x09 0x2000 command.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;I haven't verified that I can run the&amp;nbsp;&lt;SPAN&gt;"evkbimxrt1050_flexspi_nor_polling_transfer" on my board, but that's next.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;If I solve the problem, I'll let you know.&amp;nbsp; Just wanted to let you know that I'm having the same problem!&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;Tim Ewald&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 May 2019 20:03:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-Using-MfgTool-iMXRT1052-QSPI-Flash-Boot/m-p/786064#M121840</guid>
      <dc:creator>timewald</dc:creator>
      <dc:date>2019-05-01T20:03:44Z</dc:date>
    </item>
    <item>
      <title>Re: Error Using MfgTool iMXRT1052 QSPI Flash Boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-Using-MfgTool-iMXRT1052-QSPI-Flash-Boot/m-p/786065#M121841</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I did the same think on my side, but when we use Hyperflash everything is working fine on the EVKB. My guest is that the ivt_flashloader.bin version K2.1.0 doesn't support correctly the QSPI flash as well as they should. I tryed to recompile the flashloader v K2.7.0 to solve it, but this new version doesn't work, I felt in BootLoader after the jump call.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 May 2019 15:22:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-Using-MfgTool-iMXRT1052-QSPI-Flash-Boot/m-p/786065#M121841</guid>
      <dc:creator>Lorac</dc:creator>
      <dc:date>2019-05-23T15:22:10Z</dc:date>
    </item>
    <item>
      <title>Re: Error Using MfgTool iMXRT1052 QSPI Flash Boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-Using-MfgTool-iMXRT1052-QSPI-Flash-Boot/m-p/786066#M121842</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;PS F:\MCUXpresso\Flashloader_RT1050_1.1\Tools\blhost\win&amp;gt; .\blhost.exe -u -- flash-erase-region 0x60000000 2048&lt;BR /&gt;Inject command 'flash-erase-region'&lt;BR /&gt;Successful generic response to command 'flash-erase-region'&lt;BR /&gt;Response status = 0 (0x0) Success.&lt;BR /&gt;PS F:\MCUXpresso\Flashloader_RT1050_1.1\Tools\blhost\win&amp;gt; .\blhost.exe -u -- flash-erase-region 0x60000000 0x10000&lt;BR /&gt;Inject command 'flash-erase-region'&lt;BR /&gt;Successful generic response to command 'flash-erase-region'&lt;BR /&gt;Response status = 0 (0x0) Success.&lt;BR /&gt;PS F:\MCUXpresso\Flashloader_RT1050_1.1\Tools\blhost\win&amp;gt; .\blhost.exe -u -- flash-erase-region 0x60000000 0x100000&lt;BR /&gt;Inject command 'flash-erase-region'&lt;BR /&gt;sendCommandGetResponse.readPacket error 5.&lt;BR /&gt;Response status = 10004 (0x2714) No response packet from target device.&lt;BR /&gt;PS F:\MCUXpresso\Flashloader_RT1050_1.1\Tools\blhost\win&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I found the issue, if the sector size is bigger than 64kB the command get back error message. That's probably normal??&lt;/P&gt;&lt;P&gt;CD&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 May 2019 18:43:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-Using-MfgTool-iMXRT1052-QSPI-Flash-Boot/m-p/786066#M121842</guid>
      <dc:creator>Lorac</dc:creator>
      <dc:date>2019-05-23T18:43:44Z</dc:date>
    </item>
    <item>
      <title>Re: Error Using MfgTool iMXRT1052 QSPI Flash Boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-Using-MfgTool-iMXRT1052-QSPI-Flash-Boot/m-p/786067#M121843</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;PS F:\MCUXpresso\Flashloader_RT1050_1.1\Tools\blhost\win&amp;gt; .\blhost.exe -u -- flash-erase-region 0x60000000 0x60000&lt;BR /&gt;Inject command 'flash-erase-region'&lt;BR /&gt;Successful generic response to command 'flash-erase-region'&lt;BR /&gt;Response status = 0 (0x0) Success.&lt;BR /&gt;PS F:\MCUXpresso\Flashloader_RT1050_1.1\Tools\blhost\win&amp;gt; .\blhost.exe -u -- flash-erase-region 0x60000000 0x68000&lt;BR /&gt;Inject command 'flash-erase-region'&lt;BR /&gt;Successful generic response to command 'flash-erase-region'&lt;BR /&gt;Response status = 0 (0x0) Success.&lt;BR /&gt;PS F:\MCUXpresso\Flashloader_RT1050_1.1\Tools\blhost\win&amp;gt; .\blhost.exe -u -- flash-erase-region 0x60000000 0x6F000&lt;BR /&gt;Inject command 'flash-erase-region'&lt;BR /&gt;sendCommandGetResponse.readPacket error 5.&lt;BR /&gt;Response status = 10004 (0x2714) No response packet from target device.&lt;BR /&gt;PS F:\MCUXpresso\Flashloader_RT1050_1.1\Tools\blhost\win&amp;gt; .\blhost.exe -u -- flash-erase-region 0x60000000 0x6A000&lt;BR /&gt;Inject command 'flash-erase-region'&lt;BR /&gt;sendCommandGetResponse.readPacket error 5.&lt;BR /&gt;Response status = 10004 (0x2714) No response packet from target device.&lt;BR /&gt;PS F:\MCUXpresso\Flashloader_RT1050_1.1\Tools\blhost\win&amp;gt; .\blhost.exe -u -- flash-erase-region 0x60000000 0x69000&lt;BR /&gt;Inject command 'flash-erase-region'&lt;BR /&gt;sendCommandGetResponse.readPacket error 5.&lt;BR /&gt;Response status = 10004 (0x2714) No response packet from target device.&lt;BR /&gt;PS F:\MCUXpresso\Flashloader_RT1050_1.1\Tools\blhost\win&amp;gt; .\blhost.exe -u -- flash-erase-region 0x60000000 0x68000&lt;BR /&gt;Inject command 'flash-erase-region'&lt;BR /&gt;Successful generic response to command 'flash-erase-region'&lt;BR /&gt;Response status = 0 (0x0) Success.&lt;BR /&gt;PS F:\MCUXpresso\Flashloader_RT1050_1.1\Tools\blhost\win&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It's probably that we reach a timeout in the flashloader during the erasing procedure. On my RT1050-EVKB, this point is between size of 0x68000 and 0x69000.&amp;nbsp;&lt;/P&gt;&lt;P&gt;CD&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 May 2019 18:51:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-Using-MfgTool-iMXRT1052-QSPI-Flash-Boot/m-p/786067#M121843</guid>
      <dc:creator>Lorac</dc:creator>
      <dc:date>2019-05-23T18:51:30Z</dc:date>
    </item>
    <item>
      <title>Re: Error Using MfgTool iMXRT1052 QSPI Flash Boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-Using-MfgTool-iMXRT1052-QSPI-Flash-Boot/m-p/786068#M121844</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;referenced to : cfg.ini&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;[profiles]&lt;/P&gt;&lt;P&gt;chip = MXRT105X&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[platform]&lt;/P&gt;&lt;P&gt;board =&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[LIST]&lt;/P&gt;&lt;P&gt;name = MXRT105x-DevBootSerialQSPIFlashXiP&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;EM&gt;reference to: ucl2.xml&lt;/EM&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;[...]&lt;/P&gt;&lt;P&gt;&amp;lt;LIST name="MXRT105x-DevBootSerialQSPIFlashXiP" desc="Manufacturing with Flashloader"&amp;gt;&lt;BR /&gt;&amp;lt;!-- Stage 1, load and execute Flashloader --&amp;gt; &lt;BR /&gt; &amp;lt;CMD state="BootStrap" type="boot" body="BootStrap" file="ivt_flashloader.bin" &amp;gt; Loading Flashloader. &amp;lt;/CMD&amp;gt;&lt;BR /&gt; &amp;lt;CMD state="BootStrap" type="jump" onError = "ignore"&amp;gt; Jumping to Flashloader. &amp;lt;/CMD&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;lt;!-- Stage 2, Program boot image into external memory using Flashloader --&amp;gt; &lt;BR /&gt; &amp;lt;CMD state="Blhost" type="blhost" body="get-property 1" &amp;gt; Get Property 1. &amp;lt;/CMD&amp;gt; &amp;lt;!--Used to test if flashloader runs successfully--&amp;gt;&lt;BR /&gt; &amp;lt;CMD state="Blhost" type="blhost" body="fill-memory 0x2000 4 0xc0000005"&amp;gt; Prepare Flash Configuration option &amp;lt;/CMD&amp;gt;&lt;BR /&gt; &amp;lt;CMD state="Blhost" type="blhost" body="configure-memory 0x9 0x2000"&amp;gt; Configure QuadSPI NOR Flash &amp;lt;/CMD&amp;gt;&lt;BR /&gt; &amp;lt;!-- This erase size need to be updated based on the actual boot image size--&amp;gt;&lt;BR /&gt; &amp;lt;CMD state="Blhost" type="blhost" timeout="15000" body="flash-erase-region 0x60000000 0x040000" &amp;gt; Erase 256kBytes &amp;lt;/CMD&amp;gt; &lt;BR /&gt; &amp;lt;CMD state="Blhost" type="blhost" timeout="15000" body="flash-erase-region 0x60040000 0x040000" &amp;gt; Erase 256kBytes &amp;lt;/CMD&amp;gt; &lt;BR /&gt; &amp;lt;CMD state="Blhost" type="blhost" timeout="15000" body="flash-erase-region 0x60080000 0x040000" &amp;gt; Erase 256kBytes &amp;lt;/CMD&amp;gt; &lt;BR /&gt; &amp;lt;CMD state="Blhost" type="blhost" timeout="15000" body="flash-erase-region 0x600C0000 0x040000" &amp;gt; Erase 256kBytes &amp;lt;/CMD&amp;gt; &lt;BR /&gt; &amp;lt;CMD state="Blhost" type="blhost" timeout="15000" body="write-memory 0x60000000 \"Profiles\\MXRT105x\\OS Firmware\\boot_image.bin\"" &amp;gt; Program Boot Image. &amp;lt;/CMD&amp;gt; &lt;BR /&gt; &amp;lt;CMD state="Blhost" type="blhost" body="Update QSPI Completed!"&amp;gt;Done&amp;lt;/CMD&amp;gt;&lt;BR /&gt;&amp;lt;/LIST&amp;gt;&lt;/P&gt;&lt;P&gt;[..]&lt;/P&gt;&lt;P&gt;Here is the solution. :smileyhappy:&lt;/P&gt;&lt;P&gt;CD&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 May 2019 19:08:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-Using-MfgTool-iMXRT1052-QSPI-Flash-Boot/m-p/786068#M121844</guid>
      <dc:creator>Lorac</dc:creator>
      <dc:date>2019-05-23T19:08:33Z</dc:date>
    </item>
  </channel>
</rss>