<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX6UL Boot ROM IOMUX configuration</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-Boot-ROM-IOMUX-configuration/m-p/785539#M121758</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've a new custom board with IMX6UL configured to boot on USDHC1 controller with an eMMC connected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can't find a document describing what's the IOMUX configuration used by the ROM Bootloader when it starts, in order for me to be sure that the way I connected some signals is correct.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My specific problem is related to the nRST signal of the eMMC which is connected to NAND_WP_B (which has the USDHC1_RESET_B function available). What I/O is used by the ROM Bootloader for this function?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have a document describing the complete I/O mapping used by the ROM Bootloader?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Dec 2018 09:22:10 GMT</pubDate>
    <dc:creator>christopheniclaes</dc:creator>
    <dc:date>2018-12-11T09:22:10Z</dc:date>
    <item>
      <title>IMX6UL Boot ROM IOMUX configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-Boot-ROM-IOMUX-configuration/m-p/785539#M121758</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've a new custom board with IMX6UL configured to boot on USDHC1 controller with an eMMC connected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can't find a document describing what's the IOMUX configuration used by the ROM Bootloader when it starts, in order for me to be sure that the way I connected some signals is correct.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My specific problem is related to the nRST signal of the eMMC which is connected to NAND_WP_B (which has the USDHC1_RESET_B function available). What I/O is used by the ROM Bootloader for this function?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have a document describing the complete I/O mapping used by the ROM Bootloader?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Dec 2018 09:22:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-Boot-ROM-IOMUX-configuration/m-p/785539#M121758</guid>
      <dc:creator>christopheniclaes</dc:creator>
      <dc:date>2018-12-11T09:22:10Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6UL Boot ROM IOMUX configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-Boot-ROM-IOMUX-configuration/m-p/785540#M121759</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Christophe&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I/O mapping can be found in Table 8-18. SD/MMC IOMUX Pin Configuration &lt;/P&gt;&lt;P&gt;i.MX6UL Reference Manual &lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Freference-manual%2FIMX6ULRM.pdf" rel="nofollow" target="_blank"&gt;http://www.nxp.com/docs/en/reference-manual/IMX6ULRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Dec 2018 00:08:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-Boot-ROM-IOMUX-configuration/m-p/785540#M121759</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-12-12T00:08:54Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6UL Boot ROM IOMUX configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-Boot-ROM-IOMUX-configuration/m-p/785541#M121760</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you! I missed this table in the Reference Manual!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Dec 2018 06:52:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-Boot-ROM-IOMUX-configuration/m-p/785541#M121760</guid>
      <dc:creator>christopheniclaes</dc:creator>
      <dc:date>2018-12-12T06:52:35Z</dc:date>
    </item>
  </channel>
</rss>