<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Boot issue using prebuilt  android images for i.mx6Q -SABRE (MCIMx6Q-SDB) from SD card(SD3) in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Boot-issue-using-prebuilt-android-images-for-i-mx6Q-SABRE/m-p/208078#M12152</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to boot-up the i.mx6Q quad core (MCIMx6Q-SDB) board by downloading the p rebuilt&amp;nbsp; demo images for android .I have perform the following steps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.&amp;nbsp; I have inserted the 8 GB SD card in SD3(J507) slot. I am using MFG tool( version Mfg tools Rel-12.09.01_GA_MX6Q_UPDATER)&amp;nbsp; to download images on SD card.I have put required images in android folder of mfgtool updater. (boot.img, recovery.img,system.img and u-boot.bin)&lt;/P&gt;&lt;P&gt;2. I am&amp;nbsp; settings boot switch sw6 as 00001100(1 to 8 bit) while it is in download mode. When MFG tool completed its download to the SD card, i power off the board and then reset the SW6 switch to 01000010 ( MMC2 (SD3) boot) but its not booting up.&lt;/P&gt;&lt;P&gt;3.&amp;nbsp; Some time it does not get the "booti" command and some times it stuck in downloading the u image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have checked the SD card using fdisk command and found that it has only one partition instead of it should have 9 partition.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any change in the step i mentioned above?. I am using prebuilt demo android images from (\image_imx-android-r13.4-ga_6qsabresd.tar\image_imx-android-r13.4-ga_6qsabresd\sabresd_6dq\SD) . Is there something missing here? Please help..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Hemal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 14 Dec 2012 11:38:56 GMT</pubDate>
    <dc:creator>hemalgandhi</dc:creator>
    <dc:date>2012-12-14T11:38:56Z</dc:date>
    <item>
      <title>Boot issue using prebuilt  android images for i.mx6Q -SABRE (MCIMx6Q-SDB) from SD card(SD3)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-issue-using-prebuilt-android-images-for-i-mx6Q-SABRE/m-p/208078#M12152</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to boot-up the i.mx6Q quad core (MCIMx6Q-SDB) board by downloading the p rebuilt&amp;nbsp; demo images for android .I have perform the following steps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.&amp;nbsp; I have inserted the 8 GB SD card in SD3(J507) slot. I am using MFG tool( version Mfg tools Rel-12.09.01_GA_MX6Q_UPDATER)&amp;nbsp; to download images on SD card.I have put required images in android folder of mfgtool updater. (boot.img, recovery.img,system.img and u-boot.bin)&lt;/P&gt;&lt;P&gt;2. I am&amp;nbsp; settings boot switch sw6 as 00001100(1 to 8 bit) while it is in download mode. When MFG tool completed its download to the SD card, i power off the board and then reset the SW6 switch to 01000010 ( MMC2 (SD3) boot) but its not booting up.&lt;/P&gt;&lt;P&gt;3.&amp;nbsp; Some time it does not get the "booti" command and some times it stuck in downloading the u image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have checked the SD card using fdisk command and found that it has only one partition instead of it should have 9 partition.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any change in the step i mentioned above?. I am using prebuilt demo android images from (\image_imx-android-r13.4-ga_6qsabresd.tar\image_imx-android-r13.4-ga_6qsabresd\sabresd_6dq\SD) . Is there something missing here? Please help..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Hemal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Dec 2012 11:38:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-issue-using-prebuilt-android-images-for-i-mx6Q-SABRE/m-p/208078#M12152</guid>
      <dc:creator>hemalgandhi</dc:creator>
      <dc:date>2012-12-14T11:38:56Z</dc:date>
    </item>
    <item>
      <title>Re: Boot issue using prebuilt  android images for i.mx6Q -SABRE (MCIMx6Q-SDB) from SD card(SD3)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-issue-using-prebuilt-android-images-for-i-mx6Q-SABRE/m-p/208079#M12153</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The mfgtool ucl2.xml does not have an Android -&amp;gt; SD programming profile, only -&amp;gt; eMMC.&lt;/P&gt;&lt;P&gt;This profile needs to be slightly modified to program the SD&lt;/P&gt;&lt;P&gt;(replace mmcblk0 with mmcblk1)&lt;/P&gt;&lt;P&gt;Verify the cfg.ini file is selecting this new SD profile.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You will also need to adjust the uboot commandline arguments to use the SD card.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Brett&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Dec 2012 14:51:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-issue-using-prebuilt-android-images-for-i-mx6Q-SABRE/m-p/208079#M12153</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2012-12-14T14:51:42Z</dc:date>
    </item>
    <item>
      <title>Re: Boot issue using prebuilt  android images for i.mx6Q -SABRE (MCIMx6Q-SDB) from SD card(SD3)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-issue-using-prebuilt-android-images-for-i-mx6Q-SABRE/m-p/208080#M12154</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Brett&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It works..I have changed the profile name in cfg.ini to Android-SabreSD-eMMC and &lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;replace mmcblk0 with mmcblk1&lt;/SPAN&gt; in this Android-SabreSD-eMMC provided in ucl2.xml file.&lt;/P&gt;&lt;P&gt;Also i have changed the uboot argument as mentioned below on uboot command line.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;setenv bootcmd booti mmc2 to boot from SD3 slot ( Using SD Card)&lt;/P&gt;&lt;P&gt;saveenv&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With this above changes it booted with android OS on HDMI display.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help!!!!!!!!!!!!!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Dec 2012 05:33:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-issue-using-prebuilt-android-images-for-i-mx6Q-SABRE/m-p/208080#M12154</guid>
      <dc:creator>hemalgandhi</dc:creator>
      <dc:date>2012-12-17T05:33:04Z</dc:date>
    </item>
  </channel>
</rss>