<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SDIO card detection failure with 4.9.88 kernel in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SDIO-card-detection-failure-with-4-9-88-kernel/m-p/781933#M121424</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi venkatesh&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for sd3 one can check linux/arch/arm/boot/dts/imx6sx-sdb-btwifi.dts&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6sx-sdb-btwifi.dts?h=imx_4.9.88_2.0.0_ga" title="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6sx-sdb-btwifi.dts?h=imx_4.9.88_2.0.0_ga"&gt;imx6sx-sdb-btwifi.dts\dts\boot\arm\arch - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;supported wifi modules are described on&lt;/P&gt;&lt;P&gt;wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html&lt;/P&gt;&lt;P&gt;For other modules one will have to ask driver from module vemdor for Linux L4.9.88.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Nov 2018 06:04:34 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-11-21T06:04:34Z</dc:date>
    <item>
      <title>SDIO card detection failure with 4.9.88 kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SDIO-card-detection-failure-with-4-9-88-kernel/m-p/781932#M121423</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Board used: IMX6SXSABRESD&lt;BR /&gt;Kernel image: It's yocto build&amp;nbsp; based on latest IMX yocto project user guide&lt;BR /&gt;kernel version: 4.9.88&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After a fresh boot up, SDIO card is inserted into SDIO 3.0 slot(J3) of the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It's showing up the SDIO initialization messages and unable to detect the card&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please find the attached log files. &lt;BR /&gt;bootlog.txt: Contains the kernel bootup prints&lt;BR /&gt;sdio_init_failure.txt: It's a sdio card detection failure log&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thanks,&lt;/P&gt;&lt;P&gt;venkatesh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Nov 2018 15:39:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SDIO-card-detection-failure-with-4-9-88-kernel/m-p/781932#M121423</guid>
      <dc:creator>venkatesh_dyaga</dc:creator>
      <dc:date>2018-11-20T15:39:40Z</dc:date>
    </item>
    <item>
      <title>Re: SDIO card detection failure with 4.9.88 kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SDIO-card-detection-failure-with-4-9-88-kernel/m-p/781933#M121424</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi venkatesh&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for sd3 one can check linux/arch/arm/boot/dts/imx6sx-sdb-btwifi.dts&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6sx-sdb-btwifi.dts?h=imx_4.9.88_2.0.0_ga" title="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6sx-sdb-btwifi.dts?h=imx_4.9.88_2.0.0_ga"&gt;imx6sx-sdb-btwifi.dts\dts\boot\arm\arch - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;supported wifi modules are described on&lt;/P&gt;&lt;P&gt;wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html&lt;/P&gt;&lt;P&gt;For other modules one will have to ask driver from module vemdor for Linux L4.9.88.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Nov 2018 06:04:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SDIO-card-detection-failure-with-4-9-88-kernel/m-p/781933#M121424</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-11-21T06:04:34Z</dc:date>
    </item>
  </channel>
</rss>