<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: How to add python library</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-add-python-library/m-p/781725#M121418</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Steven Yu,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Python fire library is not available on the i.MX Yocto BSP so you would need to manually add it to the image or to create a recipe in Yocto that installs this library. There is not an easy way to add it since it’s not integrated on the existing layers of the BSP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Nov 2018 18:20:06 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2018-11-22T18:20:06Z</dc:date>
    <item>
      <title>How to add python library</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-add-python-library/m-p/781724#M121417</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Support,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We use i.mx6 series and need Python fire library recently.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We use this command "bitbake -s | grep python" to check which library we can enable, however, we don't see fire library. Would you please advise how to add other Python library into system when compiling?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Steven Yu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Nov 2018 10:14:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-add-python-library/m-p/781724#M121417</guid>
      <dc:creator>stevenyu</dc:creator>
      <dc:date>2018-11-20T10:14:36Z</dc:date>
    </item>
    <item>
      <title>Re: How to add python library</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-add-python-library/m-p/781725#M121418</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Steven Yu,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Python fire library is not available on the i.MX Yocto BSP so you would need to manually add it to the image or to create a recipe in Yocto that installs this library. There is not an easy way to add it since it’s not integrated on the existing layers of the BSP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Nov 2018 18:20:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-add-python-library/m-p/781725#M121418</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2018-11-22T18:20:06Z</dc:date>
    </item>
  </channel>
</rss>