<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx28 ROM code</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx28-ROM-code/m-p/207968#M12138</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You are able to boot from the SD card using the on-chip ROM. That is supported and also used on the i.MX28EVK. No problems there.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can find more information on the ROM and boot process in i.MX28 Reference manual (Chapter 12).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 Feb 2012 12:42:36 GMT</pubDate>
    <dc:creator>VladanJovanovic</dc:creator>
    <dc:date>2012-02-03T12:42:36Z</dc:date>
    <item>
      <title>imx28 ROM code</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx28-ROM-code/m-p/207967#M12137</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does anybody know the about the pre programmed code in imx28 onchi ROM. I am basically looking for the code which reads SD card content. I am planning to have SD card slot in one of the boards we are developing based on imx28 processor. I want to put boot file, image files and&amp;nbsp;language files like things there.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Feb 2012 09:18:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx28-ROM-code/m-p/207967#M12137</guid>
      <dc:creator>RamanJamloki</dc:creator>
      <dc:date>2012-02-03T09:18:55Z</dc:date>
    </item>
    <item>
      <title>Re: imx28 ROM code</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx28-ROM-code/m-p/207968#M12138</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You are able to boot from the SD card using the on-chip ROM. That is supported and also used on the i.MX28EVK. No problems there.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can find more information on the ROM and boot process in i.MX28 Reference manual (Chapter 12).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Feb 2012 12:42:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx28-ROM-code/m-p/207968#M12138</guid>
      <dc:creator>VladanJovanovic</dc:creator>
      <dc:date>2012-02-03T12:42:36Z</dc:date>
    </item>
  </channel>
</rss>