<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can't get wlan0 interface up while using murata on linux-rel_imx_4.9.x_1.0.0_ga in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-t-get-wlan0-interface-up-while-using-murata-on-linux-rel-imx/m-p/780118#M121220</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jean,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in this case the problem will be the Murata drivers, so you may contact Murata to get the appropriate drivers.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 15 Jan 2018 21:09:33 GMT</pubDate>
    <dc:creator>Carlos_Musich</dc:creator>
    <dc:date>2018-01-15T21:09:33Z</dc:date>
    <item>
      <title>Can't get wlan0 interface up while using murata on linux-rel_imx_4.9.x_1.0.0_ga</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-t-get-wlan0-interface-up-while-using-murata-on-linux-rel-imx/m-p/780117#M121219</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guys,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm working an imx6ull board and murata device type 1DX&amp;nbsp; and i have some issues while using nxp linux release rel_imx_4.9.x_1.0.0_ga.&lt;/P&gt;&lt;P&gt;First of all i have tested the murata on linux version rel_imx_4.1.15_2.0.0 and everything was working fine. I upated the linux version to 4.9.x and the murata firmware also by downloading the correct one (4.9.11) on NXP website. The bcmdhd driver has been initialized correctly and i have issue with "HT clock" while trying to use wpa_supplicant to apply settings on wlan0 and to put it up by using this command :&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; wpa_supplicant -i wlan0 -Dnl80211 -c /etc/wpa_supplicant.conf -B&amp;amp;&lt;/P&gt;&lt;P&gt;I have attached all log files.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Issue log :&lt;/P&gt;&lt;P&gt;&amp;nbsp; dhdsdio_htclk: HT Avail timeout (1000000): clkctl 0x50&lt;BR /&gt;dhdsdio_htclk: HT Avail timeout (1000000): clkctl 0x50&lt;BR /&gt;dhdsdio_htclk: HT Avail timeout (1000000): clkctl 0x50&lt;BR /&gt;dhdsdio_htclk: HT Avail request error: retried 20 times. UNRECOVERABLE!&lt;BR /&gt;dhd_net_bus_devreset: dhd_bus_devreset: -1&lt;BR /&gt;dhd_open : wl_android_wifi_on failed (-1)&lt;BR /&gt;wl_android_wifi_off in&lt;BR /&gt;dhd_prot_ioctl : bus is down. we have nothing to do&lt;BR /&gt;dhd_net_bus_devreset: dhd_bus_devreset: -35&lt;BR /&gt;Could not set interface wlan0 flags (UP): Operation not permitted&lt;BR /&gt;nl80211: Could not set interface 'wlan0' UP&lt;BR /&gt;nl80211: deinit ifname=wlan0 disabled_11b_rates=0&lt;BR /&gt;wlan0: Failed to initialize driver interface&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is somebody has an idea?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Jean Gardy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jan 2018 11:39:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-t-get-wlan0-interface-up-while-using-murata-on-linux-rel-imx/m-p/780117#M121219</guid>
      <dc:creator>jeangardyvalent</dc:creator>
      <dc:date>2018-01-11T11:39:32Z</dc:date>
    </item>
    <item>
      <title>Re: Can't get wlan0 interface up while using murata on linux-rel_imx_4.9.x_1.0.0_ga</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-t-get-wlan0-interface-up-while-using-murata-on-linux-rel-imx/m-p/780118#M121220</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jean,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in this case the problem will be the Murata drivers, so you may contact Murata to get the appropriate drivers.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Jan 2018 21:09:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-t-get-wlan0-interface-up-while-using-murata-on-linux-rel-imx/m-p/780118#M121220</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2018-01-15T21:09:33Z</dc:date>
    </item>
  </channel>
</rss>