<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Setting the u-boot timeout in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Setting-the-u-boot-timeout/m-p/779943#M121187</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello there.&lt;/P&gt;&lt;P&gt;So I'm having a lot of trouble getting my kernel to work. It just halts on "starting kernel..." and doesn't do very much.&lt;/P&gt;&lt;P&gt;My main concern is that I don't know how to get more information out of the kernel to figure out why it is failing.&lt;/P&gt;&lt;P&gt;I'm working on an Itron board which is based on the imx28evk.&lt;/P&gt;&lt;P&gt;What I was hoping to do is start with u-boot. If I can make changes to U-Boot I can at least know that the changes I'm making in my build process are being reflected on the board.&lt;/P&gt;&lt;P&gt;I decided to change the u-boot 'press any key to enter setup' timeout figure.&lt;/P&gt;&lt;P&gt;However I don't know how to set this. The default appears to be 0 seconds, but where is this set? Somewhere in meta-freescale, or should I be looking at the source files themselves? I notice the bootdelay variable is there, but as far as I can tell, this can only be set with the setenv command which is no good.&lt;/P&gt;&lt;P&gt;How can I change this simple value so that when I put in my new SDCard image, it actually takes effect on the board?&lt;/P&gt;&lt;P&gt;Cheers&lt;/P&gt;&lt;P&gt;Ben&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 11 Dec 2017 17:13:36 GMT</pubDate>
    <dc:creator>benjaminblundel</dc:creator>
    <dc:date>2017-12-11T17:13:36Z</dc:date>
    <item>
      <title>Setting the u-boot timeout</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Setting-the-u-boot-timeout/m-p/779943#M121187</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello there.&lt;/P&gt;&lt;P&gt;So I'm having a lot of trouble getting my kernel to work. It just halts on "starting kernel..." and doesn't do very much.&lt;/P&gt;&lt;P&gt;My main concern is that I don't know how to get more information out of the kernel to figure out why it is failing.&lt;/P&gt;&lt;P&gt;I'm working on an Itron board which is based on the imx28evk.&lt;/P&gt;&lt;P&gt;What I was hoping to do is start with u-boot. If I can make changes to U-Boot I can at least know that the changes I'm making in my build process are being reflected on the board.&lt;/P&gt;&lt;P&gt;I decided to change the u-boot 'press any key to enter setup' timeout figure.&lt;/P&gt;&lt;P&gt;However I don't know how to set this. The default appears to be 0 seconds, but where is this set? Somewhere in meta-freescale, or should I be looking at the source files themselves? I notice the bootdelay variable is there, but as far as I can tell, this can only be set with the setenv command which is no good.&lt;/P&gt;&lt;P&gt;How can I change this simple value so that when I put in my new SDCard image, it actually takes effect on the board?&lt;/P&gt;&lt;P&gt;Cheers&lt;/P&gt;&lt;P&gt;Ben&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Dec 2017 17:13:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Setting-the-u-boot-timeout/m-p/779943#M121187</guid>
      <dc:creator>benjaminblundel</dc:creator>
      <dc:date>2017-12-11T17:13:36Z</dc:date>
    </item>
    <item>
      <title>Re: Setting the u-boot timeout</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Setting-the-u-boot-timeout/m-p/779944#M121188</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Benajmin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The variable is bootdelay and default is 3 seconds. If the BSP that you are using is not form NXP you may contact the developer of the BSP you are using for support.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/6839i8569CA8ECB3666AF/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Dec 2017 21:14:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Setting-the-u-boot-timeout/m-p/779944#M121188</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2017-12-11T21:14:01Z</dc:date>
    </item>
  </channel>
</rss>