<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Is bt.656 the only timing mode when using V4L2 Capture</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Is-bt-656-the-only-timing-mode-when-using-V4L2-Capture/m-p/779929#M121180</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;yes, if you want to use gated mode, you can modify this source code, if you want to use bt656 progressive mode, you can change the "INTERLACED" to "PROGRESSIVE"&lt;/P&gt;&lt;P&gt;if (ifparm.u.bt656.clock_curr == 0)&lt;/P&gt;&lt;P&gt;&amp;nbsp; csi_param.clk_mode = IPU_CSI_CLK_MODE_CCIR656_INTERLACED;&lt;/P&gt;&lt;P&gt;else&lt;/P&gt;&lt;P&gt;&amp;nbsp; csi_param.clk_mode = IPU_CSI_CLK_MODE_GATED_CLK;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Nov 2017 03:51:41 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2017-11-23T03:51:41Z</dc:date>
    <item>
      <title>Is bt.656 the only timing mode when using V4L2 Capture</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-bt-656-the-only-timing-mode-when-using-V4L2-Capture/m-p/779926#M121177</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In media/platform/mxc/capture/v4l2-int-device.h, there is only one input format defined : V4L2_IF_TYPE_BT656.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does this means that the only timing mode for CSI is BT.656 mode when using the imx6q-v4l2-capture IPU driver?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How to deal with a&amp;nbsp; sensor camera connected to CSI in gated mode ie with HSync VSync?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note : I use the terms BT.656 mode and gated mode as described into the IMX6DQRM&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Nov 2017 16:42:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-bt-656-the-only-timing-mode-when-using-V4L2-Capture/m-p/779926#M121177</guid>
      <dc:creator>axellagrange</dc:creator>
      <dc:date>2017-11-15T16:42:50Z</dc:date>
    </item>
    <item>
      <title>Re: Is bt.656 the only timing mode when using V4L2 Capture</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-bt-656-the-only-timing-mode-when-using-V4L2-Capture/m-p/779927#M121178</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;"How to deal with a&amp;nbsp; sensor camera connected to CSI in gated mode ie with HSync VSync?" what mode do you need? bt656 mode or gated mode? do you need to capture bt656 in gated mode?? de-interlacing?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Nov 2017 03:25:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-bt-656-the-only-timing-mode-when-using-V4L2-Capture/m-p/779927#M121178</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2017-11-21T03:25:00Z</dc:date>
    </item>
    <item>
      <title>Re: Is bt.656 the only timing mode when using V4L2 Capture</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-bt-656-the-only-timing-mode-when-using-V4L2-Capture/m-p/779928#M121179</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;I found my answer : into mxc_v4l2_capture.c,&amp;nbsp; bt656.clock_curr != 0 configures CSI in gated mode.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Nov 2017 15:42:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-bt-656-the-only-timing-mode-when-using-V4L2-Capture/m-p/779928#M121179</guid>
      <dc:creator>axellagrange</dc:creator>
      <dc:date>2017-11-21T15:42:55Z</dc:date>
    </item>
    <item>
      <title>Re: Is bt.656 the only timing mode when using V4L2 Capture</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-bt-656-the-only-timing-mode-when-using-V4L2-Capture/m-p/779929#M121180</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;yes, if you want to use gated mode, you can modify this source code, if you want to use bt656 progressive mode, you can change the "INTERLACED" to "PROGRESSIVE"&lt;/P&gt;&lt;P&gt;if (ifparm.u.bt656.clock_curr == 0)&lt;/P&gt;&lt;P&gt;&amp;nbsp; csi_param.clk_mode = IPU_CSI_CLK_MODE_CCIR656_INTERLACED;&lt;/P&gt;&lt;P&gt;else&lt;/P&gt;&lt;P&gt;&amp;nbsp; csi_param.clk_mode = IPU_CSI_CLK_MODE_GATED_CLK;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Nov 2017 03:51:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-bt-656-the-only-timing-mode-when-using-V4L2-Capture/m-p/779929#M121180</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2017-11-23T03:51:41Z</dc:date>
    </item>
  </channel>
</rss>