<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX6Q dual IPU problem</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-dual-IPU-problem/m-p/779825#M121165</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Levi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for ipu usage one can look at p.17 presentation&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-100482"&gt;A Deep Dive into Image Processing for i.MX 6 Series Applications Processors&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Muxing performed by IOMUXC_GPR registers described in IOMUX Chapter of i.MX6Q Reference Manual.&lt;/P&gt;&lt;P&gt;For configuring various configurations may be useful to look at BD boards, as they have many lcd options&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://boundarydevices.com/configuring-i-mx6-machines-different-screens-nitrogen6x-sabre-lite/" title="https://boundarydevices.com/configuring-i-mx6-machines-different-screens-nitrogen6x-sabre-lite/"&gt;Configuring i.MX6 boards for different screens - Boundary Devices&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://github.com/boundarydevices/linux-imx6/tree/boundary-imx_4.1.15_1.0.0_ga/arch/arm/boot/dts" title="https://github.com/boundarydevices/linux-imx6/tree/boundary-imx_4.1.15_1.0.0_ga/arch/arm/boot/dts"&gt;linux-imx6/arch/arm/boot/dts at boundary-imx_4.1.15_1.0.0_ga · boundarydevices/linux-imx6 · GitHub&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;in dts file one can pay attention to entries like "ipu2-di0".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 11 Dec 2017 23:26:49 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-12-11T23:26:49Z</dc:date>
    <item>
      <title>IMX6Q dual IPU problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-dual-IPU-problem/m-p/779824#M121164</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have heard IMX6Q has two IPUs Compared with IMX6DL having only one.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Then how to config to use both the two IPU?&lt;/P&gt;&lt;P&gt;My configration of device tree now is:&lt;/P&gt;&lt;P&gt;arch/arm/boot/dts/imx6q.dts:&lt;/P&gt;&lt;P&gt;&amp;amp;ldb {&lt;BR /&gt;&amp;nbsp;&lt;A href="mailto:lvds-channel@0"&gt;lvds-channel@0&lt;/A&gt; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;crtc = "ipu2-di0";&lt;BR /&gt;&amp;nbsp;};&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;A href="mailto:lvds-channel@1"&gt;lvds-channel@1&lt;/A&gt; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;crtc = "ipu2-di1";&lt;BR /&gt;&amp;nbsp;};&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;arch/arm/boot/dts/imx6q.dtsi:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;A href="mailto:lcd@0"&gt;lcd@0&lt;/A&gt; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;compatible = "fsl,lcd";&lt;BR /&gt;&amp;nbsp;&amp;nbsp;ipu_id = &amp;lt;0&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;disp_id = &amp;lt;0&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;default_ifmt = "RGB24";&lt;BR /&gt;&amp;nbsp;&amp;nbsp;pinctrl-names = "default";&lt;BR /&gt;&amp;nbsp;&amp;nbsp;pinctrl-0 = &amp;lt;&amp;amp;pinctrl_ipu1&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;status = "okay";&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; };&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please modify it to use both the two IPU.&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Best Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Levi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Dec 2017 12:14:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-dual-IPU-problem/m-p/779824#M121164</guid>
      <dc:creator>liweihua</dc:creator>
      <dc:date>2017-12-11T12:14:02Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q dual IPU problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-dual-IPU-problem/m-p/779825#M121165</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Levi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for ipu usage one can look at p.17 presentation&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-100482"&gt;A Deep Dive into Image Processing for i.MX 6 Series Applications Processors&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Muxing performed by IOMUXC_GPR registers described in IOMUX Chapter of i.MX6Q Reference Manual.&lt;/P&gt;&lt;P&gt;For configuring various configurations may be useful to look at BD boards, as they have many lcd options&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://boundarydevices.com/configuring-i-mx6-machines-different-screens-nitrogen6x-sabre-lite/" title="https://boundarydevices.com/configuring-i-mx6-machines-different-screens-nitrogen6x-sabre-lite/"&gt;Configuring i.MX6 boards for different screens - Boundary Devices&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://github.com/boundarydevices/linux-imx6/tree/boundary-imx_4.1.15_1.0.0_ga/arch/arm/boot/dts" title="https://github.com/boundarydevices/linux-imx6/tree/boundary-imx_4.1.15_1.0.0_ga/arch/arm/boot/dts"&gt;linux-imx6/arch/arm/boot/dts at boundary-imx_4.1.15_1.0.0_ga · boundarydevices/linux-imx6 · GitHub&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;in dts file one can pay attention to entries like "ipu2-di0".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Dec 2017 23:26:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-dual-IPU-problem/m-p/779825#M121165</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-12-11T23:26:49Z</dc:date>
    </item>
  </channel>
</rss>