<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: cfimager_imx error -37</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/cfimager-imx-error-37/m-p/779686#M121149</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your support.&lt;/P&gt;&lt;P&gt;Now I can create the boot SD Card, however if the firmware binary is big (around 27 MB), I have again the error -37.&lt;/P&gt;&lt;P&gt;With just the testing firmware around 2MB, it's work well.&lt;/P&gt;&lt;P&gt;Do you have any ideas about this? Does CFImager_imx.exe have limit for the binary?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Minh.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Jun 2018 10:50:11 GMT</pubDate>
    <dc:creator>minhnguyen</dc:creator>
    <dc:date>2018-06-21T10:50:11Z</dc:date>
    <item>
      <title>cfimager_imx error -37</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/cfimager-imx-error-37/m-p/779682#M121145</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a problem with the custom board with iMX6S5 processor.&lt;/P&gt;&lt;P&gt;I built the firmware SDK bare metal code and then trying to flash the binary file into SD Card with the "cfimager_imx.exe" as follow the example "uart1_led".&lt;/P&gt;&lt;P&gt;However I get an error as the ouput in the image follows:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/28417i3285785679A23D2D/image-size/large?v=v2&amp;amp;px=999" title="Erro37.JPG" alt="Erro37.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I have no idea about the error -37, can someone here help me to figure it out ?&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jun 2018 12:32:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/cfimager-imx-error-37/m-p/779682#M121145</guid>
      <dc:creator>minhnguyen</dc:creator>
      <dc:date>2018-06-13T12:32:10Z</dc:date>
    </item>
    <item>
      <title>Re: cfimager_imx error -37</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/cfimager-imx-error-37/m-p/779683#M121146</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Minh&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this error is FAILED_TO_WRITE_SECTOR , one can try other sd card&lt;/P&gt;&lt;P&gt;or with other card reader.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jun 2018 23:12:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/cfimager-imx-error-37/m-p/779683#M121146</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-06-13T23:12:25Z</dc:date>
    </item>
    <item>
      <title>Re: cfimager_imx error -37</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/cfimager-imx-error-37/m-p/779684#M121147</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried other new 2GB SD cards or with other card reader, the error -37 still happen.&lt;/P&gt;&lt;P&gt;I tried with other file system format types (NTFS or FAT32), the error still occur.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Nguyen.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jun 2018 13:09:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/cfimager-imx-error-37/m-p/779684#M121147</guid>
      <dc:creator>minhnguyen</dc:creator>
      <dc:date>2018-06-14T13:09:46Z</dc:date>
    </item>
    <item>
      <title>Re: cfimager_imx error -37</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/cfimager-imx-error-37/m-p/779685#M121148</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Minh&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;had you checked sect.4.Hardware setup to use CFImager.exe&lt;BR /&gt;CFImager_UserGuide.doc included in sdk, so correct drive letter was used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jun 2018 01:38:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/cfimager-imx-error-37/m-p/779685#M121148</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-06-15T01:38:49Z</dc:date>
    </item>
    <item>
      <title>Re: cfimager_imx error -37</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/cfimager-imx-error-37/m-p/779686#M121149</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your support.&lt;/P&gt;&lt;P&gt;Now I can create the boot SD Card, however if the firmware binary is big (around 27 MB), I have again the error -37.&lt;/P&gt;&lt;P&gt;With just the testing firmware around 2MB, it's work well.&lt;/P&gt;&lt;P&gt;Do you have any ideas about this? Does CFImager_imx.exe have limit for the binary?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Minh.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Jun 2018 10:50:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/cfimager-imx-error-37/m-p/779686#M121149</guid>
      <dc:creator>minhnguyen</dc:creator>
      <dc:date>2018-06-21T10:50:11Z</dc:date>
    </item>
  </channel>
</rss>