<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 YOCTO build error</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/YOCTO-build-error/m-p/779212#M121064</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I recently brought the NXP modular gateway developed by volansys. I nted to develop my stack using the YOCTO and proceeded using same, and package provided by NXP. I followed the instruction as mentioned in the following attached README.txt file.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I am getting one error, log error file I attached below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The error I am getting is as follows:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;DEBUG: Executing python function set_image_size&lt;BR /&gt;DEBUG: Python function set_image_size finished&lt;BR /&gt;DEBUG: Executing shell function do_image_sdcard&lt;BR /&gt;0+0 records in&lt;BR /&gt;0+0 records out&lt;BR /&gt;0 bytes (0 B) copied, 0.000439462 s, 0.0 kB/s&lt;BR /&gt;Model: (file)&lt;BR /&gt;Disk /home/user/work/automation/fsl-release-bsp/build-x11/tmp/work/imx6ulmg-poky-linux-gnueabi/volansys-image-gw/1.0-r0/deploy-volansys-image-gw-image-complete/volansys-modular-gateway-imx6ulmg-20180428043413.rootfs.sdcard: 3129MB&lt;BR /&gt;Sector size (logical/physical): 512B/512B&lt;BR /&gt;Partition Table: msdos&lt;BR /&gt;Disk Flags:&lt;/P&gt;&lt;P&gt;Number Start End Size Type File system Flags&lt;BR /&gt; 1 4194kB 12.6MB 8389kB primary lba&lt;BR /&gt; 2 12.6MB 3125MB 3112MB primary&lt;/P&gt;&lt;P&gt;998+0 records in&lt;BR /&gt;998+0 records out&lt;BR /&gt;510976 bytes (511 kB) copied, 0.0042858 s, 119 MB/s&lt;BR /&gt;mkfs.fat: warning - lowercase labels might not work properly with DOS or Windows&lt;BR /&gt;mkfs.fat 4.0 (2016-05-06)&lt;BR /&gt;Total number of sectors (16384) not a multiple of sectors per track (63)!&lt;BR /&gt;Add mtools_skip_check=1 to your .mtoolsrc file to skip this test&lt;BR /&gt;Total number of sectors (16384) not a multiple of sectors per track (63)!&lt;BR /&gt;Add mtools_skip_check=1 to your .mtoolsrc file to skip this test&lt;BR /&gt;2+0 records in&lt;BR /&gt;2+0 records out&lt;BR /&gt;8388608 bytes (8.4 MB) copied, 0.011746 s, 714 MB/s&lt;BR /&gt;dd: failed to open ‘/home/user/work/automation/fsl-release-bsp/build-x11/tmp/work/imx6ulmg-poky-linux-gnueabi/volansys-image-gw/1.0-r0/deploy-volansys-image-gw-image-complete/volansys-modular-gateway-imx6ulmg-20180428043413.rootfs.ext4’: No such file or directory&lt;BR /&gt;WARNING: exit code 1 from a shell command.&lt;BR /&gt;ERROR: Function failed: do_image_sdcard (log file is located at /home/user/work/automation/fsl-release-bsp/build-x11/tmp/work/imx6ulmg-poky-linux-gnueabi/volansys-image-gw/1.0-r0/temp/log.do_image_sdcard.1330)&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;Note: I am using build machine Ubuntu 14.04.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Plz suggest me how to fix this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Zafar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 28 Apr 2018 07:33:21 GMT</pubDate>
    <dc:creator>zafariqbal</dc:creator>
    <dc:date>2018-04-28T07:33:21Z</dc:date>
    <item>
      <title>YOCTO build error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/YOCTO-build-error/m-p/779212#M121064</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I recently brought the NXP modular gateway developed by volansys. I nted to develop my stack using the YOCTO and proceeded using same, and package provided by NXP. I followed the instruction as mentioned in the following attached README.txt file.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I am getting one error, log error file I attached below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The error I am getting is as follows:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;DEBUG: Executing python function set_image_size&lt;BR /&gt;DEBUG: Python function set_image_size finished&lt;BR /&gt;DEBUG: Executing shell function do_image_sdcard&lt;BR /&gt;0+0 records in&lt;BR /&gt;0+0 records out&lt;BR /&gt;0 bytes (0 B) copied, 0.000439462 s, 0.0 kB/s&lt;BR /&gt;Model: (file)&lt;BR /&gt;Disk /home/user/work/automation/fsl-release-bsp/build-x11/tmp/work/imx6ulmg-poky-linux-gnueabi/volansys-image-gw/1.0-r0/deploy-volansys-image-gw-image-complete/volansys-modular-gateway-imx6ulmg-20180428043413.rootfs.sdcard: 3129MB&lt;BR /&gt;Sector size (logical/physical): 512B/512B&lt;BR /&gt;Partition Table: msdos&lt;BR /&gt;Disk Flags:&lt;/P&gt;&lt;P&gt;Number Start End Size Type File system Flags&lt;BR /&gt; 1 4194kB 12.6MB 8389kB primary lba&lt;BR /&gt; 2 12.6MB 3125MB 3112MB primary&lt;/P&gt;&lt;P&gt;998+0 records in&lt;BR /&gt;998+0 records out&lt;BR /&gt;510976 bytes (511 kB) copied, 0.0042858 s, 119 MB/s&lt;BR /&gt;mkfs.fat: warning - lowercase labels might not work properly with DOS or Windows&lt;BR /&gt;mkfs.fat 4.0 (2016-05-06)&lt;BR /&gt;Total number of sectors (16384) not a multiple of sectors per track (63)!&lt;BR /&gt;Add mtools_skip_check=1 to your .mtoolsrc file to skip this test&lt;BR /&gt;Total number of sectors (16384) not a multiple of sectors per track (63)!&lt;BR /&gt;Add mtools_skip_check=1 to your .mtoolsrc file to skip this test&lt;BR /&gt;2+0 records in&lt;BR /&gt;2+0 records out&lt;BR /&gt;8388608 bytes (8.4 MB) copied, 0.011746 s, 714 MB/s&lt;BR /&gt;dd: failed to open ‘/home/user/work/automation/fsl-release-bsp/build-x11/tmp/work/imx6ulmg-poky-linux-gnueabi/volansys-image-gw/1.0-r0/deploy-volansys-image-gw-image-complete/volansys-modular-gateway-imx6ulmg-20180428043413.rootfs.ext4’: No such file or directory&lt;BR /&gt;WARNING: exit code 1 from a shell command.&lt;BR /&gt;ERROR: Function failed: do_image_sdcard (log file is located at /home/user/work/automation/fsl-release-bsp/build-x11/tmp/work/imx6ulmg-poky-linux-gnueabi/volansys-image-gw/1.0-r0/temp/log.do_image_sdcard.1330)&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;Note: I am using build machine Ubuntu 14.04.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Plz suggest me how to fix this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Zafar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 28 Apr 2018 07:33:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/YOCTO-build-error/m-p/779212#M121064</guid>
      <dc:creator>zafariqbal</dc:creator>
      <dc:date>2018-04-28T07:33:21Z</dc:date>
    </item>
  </channel>
</rss>