<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Which HW timer is associated to in timer_create()</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Which-HW-timer-is-associated-to-in-timer-create/m-p/778767#M120975</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've checked the link but it did not help a lot.&lt;/P&gt;&lt;P&gt;I need one HW timer in userspace.&lt;/P&gt;&lt;P&gt;If linux&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;timer_create() is actually using that HW timer than it is good enough.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;What I asked before is if &lt;SPAN&gt;timer_create&amp;nbsp;&lt;/SPAN&gt;actually using a HW timer (and not just Linux' tick for example which has less precision).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Thank you,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Ran&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Jan 2018 06:11:07 GMT</pubDate>
    <dc:creator>rans</dc:creator>
    <dc:date>2018-01-17T06:11:07Z</dc:date>
    <item>
      <title>Which HW timer is associated to in timer_create()</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Which-HW-timer-is-associated-to-in-timer-create/m-p/778765#M120973</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I try to understand how to use HW timers from linux userspace.&lt;/P&gt;&lt;P&gt;Is&amp;nbsp; it by calling timer_create ? If yes - which timer number is associated to it ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Ran&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jan 2018 16:58:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Which-HW-timer-is-associated-to-in-timer-create/m-p/778765#M120973</guid>
      <dc:creator>rans</dc:creator>
      <dc:date>2018-01-10T16:58:54Z</dc:date>
    </item>
    <item>
      <title>Re: Which HW timer is associated to in timer_create()</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Which-HW-timer-is-associated-to-in-timer-create/m-p/778766#M120974</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi rashalit,&lt;/P&gt;&lt;P&gt;you may find useful the following thread&lt;A href="https://community.nxp.com/thread/311481"&gt;Reg: Using Timers in IMX&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jan 2018 23:06:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Which-HW-timer-is-associated-to-in-timer-create/m-p/778766#M120974</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2018-01-16T23:06:47Z</dc:date>
    </item>
    <item>
      <title>Re: Which HW timer is associated to in timer_create()</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Which-HW-timer-is-associated-to-in-timer-create/m-p/778767#M120975</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've checked the link but it did not help a lot.&lt;/P&gt;&lt;P&gt;I need one HW timer in userspace.&lt;/P&gt;&lt;P&gt;If linux&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;timer_create() is actually using that HW timer than it is good enough.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;What I asked before is if &lt;SPAN&gt;timer_create&amp;nbsp;&lt;/SPAN&gt;actually using a HW timer (and not just Linux' tick for example which has less precision).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Thank you,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Ran&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jan 2018 06:11:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Which-HW-timer-is-associated-to-in-timer-create/m-p/778767#M120975</guid>
      <dc:creator>rans</dc:creator>
      <dc:date>2018-01-17T06:11:07Z</dc:date>
    </item>
    <item>
      <title>Re: Which HW timer is associated to in timer_create()</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Which-HW-timer-is-associated-to-in-timer-create/m-p/778768#M120976</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;timer_create() used hrtimer that is high res timer. When the board starts, BSP will pass hw timer to kernel that will be used by hrtimer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;kernel_imx/kernel/time/posix-timers.c&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="keyword token"&gt;static&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;common_timer_create&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;struct&lt;/SPAN&gt; k_itimer &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;new_timer&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
 &lt;SPAN class="token function"&gt;hrtimer_init&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;new_timer&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;it&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;real&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;timer&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; new_timer&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;it_clock&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;return&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jan 2018 07:09:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Which-HW-timer-is-associated-to-in-timer-create/m-p/778768#M120976</guid>
      <dc:creator>JayTu</dc:creator>
      <dc:date>2018-01-17T07:09:07Z</dc:date>
    </item>
  </channel>
</rss>