<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX 6 SOLO PWM Output control</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX-6-SOLO-PWM-Output-control/m-p/778179#M120874</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are trying to drive the buzzer in our design through PWM output line from solo processor .Now The buzzer requires minimum of 5 V .But PWM output is not enough to drive the buzzer . I wonder is there any possiblity that we can disable the internal pull-up and provide external pull-up of 5V to the PWM and drive that?&lt;/P&gt;&lt;P&gt;With regards ,&lt;/P&gt;&lt;P&gt;PRADI&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 May 2018 06:23:34 GMT</pubDate>
    <dc:creator>pradeepn</dc:creator>
    <dc:date>2018-05-23T06:23:34Z</dc:date>
    <item>
      <title>IMX 6 SOLO PWM Output control</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX-6-SOLO-PWM-Output-control/m-p/778179#M120874</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are trying to drive the buzzer in our design through PWM output line from solo processor .Now The buzzer requires minimum of 5 V .But PWM output is not enough to drive the buzzer . I wonder is there any possiblity that we can disable the internal pull-up and provide external pull-up of 5V to the PWM and drive that?&lt;/P&gt;&lt;P&gt;With regards ,&lt;/P&gt;&lt;P&gt;PRADI&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 May 2018 06:23:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX-6-SOLO-PWM-Output-control/m-p/778179#M120874</guid>
      <dc:creator>pradeepn</dc:creator>
      <dc:date>2018-05-23T06:23:34Z</dc:date>
    </item>
    <item>
      <title>Re: IMX 6 SOLO PWM Output control</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX-6-SOLO-PWM-Output-control/m-p/778180#M120875</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;No , you can not do that. Here you can do as follow design:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21627iA0EE7C8C5EB28452/image-size/large?v=v2&amp;amp;px=999" title="67BC99F1.PNG" alt="67BC99F1.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Or you can use the LEVEL SHIFT circuit design.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Rita&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 May 2018 02:38:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX-6-SOLO-PWM-Output-control/m-p/778180#M120875</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2018-05-28T02:38:14Z</dc:date>
    </item>
  </channel>
</rss>