<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Error: The image creation script</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Error-The-image-creation-script/m-p/778144#M120870</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello niranjanbc,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would you please provide more details on what hosts are you using? The Yocto NXP works with Ubuntu as that is the preferred host OS. Using other OS may cause errors as some packages are not available to older or newer BSPs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would you please also comment what specific BSP are you using?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 11 Jan 2018 21:09:46 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2018-01-11T21:09:46Z</dc:date>
    <item>
      <title>Error: The image creation script</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-The-image-creation-script/m-p/778143#M120869</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i have build working fine on&amp;nbsp;two Linux&amp;nbsp;PC's and failing one PC. same source and yocto build.&lt;/P&gt;&lt;P&gt;what could be the issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NOTE: Running image creation script for tar: /home/niranjan/fsl-community-bsp/build_emmc/tmp/work/phx_core_pca-poky-linux-gnueabi/core-image-phx-core-pca/1.0-r0/temp/create_image.tar ...&lt;BR /&gt;NOTE: Creating symlinks for squashfs image ...&lt;BR /&gt;NOTE: Creating symlink: core-image-phx-core-pca-phx-core-pca.squashfs -&amp;gt; core-image-phx-core-pca-phx-core-pca-20180108114647.rootfs.squashfs&lt;BR /&gt;NOTE: Creating symlinks for ext3 image ...&lt;BR /&gt;NOTE: Creating symlink: core-image-phx-core-pca-phx-core-pca.ext3 -&amp;gt; core-image-phx-core-pca-phx-core-pca-20180108114647.rootfs.ext3&lt;BR /&gt;NOTE: Creating symlinks for tar image ...&lt;BR /&gt;NOTE: Creating symlink: core-image-phx-core-pca-phx-core-pca.tar.bz2 -&amp;gt; core-image-phx-core-pca-phx-core-pca-20180108114647.rootfs.tar.bz2&lt;BR /&gt;NOTE: Running image creation script for sdcard: /home/niranjan/fsl-community-bsp/build_emmc/tmp/work/phx_core_pca-poky-linux-gnueabi/core-image-phx-core-pca/1.0-r0/temp/create_image.sdcard ...&lt;BR /&gt;ERROR: Error: The image creation script '/home/niranjan/fsl-community-bsp/build_emmc/tmp/work/phx_core_pca-poky-linux-gnueabi/core-image-phx-core-pca/1.0-r0/temp/create_image.sdcard' returned 1:&lt;BR /&gt;0+0 records in&lt;BR /&gt;0+0 records out&lt;BR /&gt;0 bytes (0 B) copied, 2.083e-05 s, 0.0 kB/s&lt;BR /&gt;Model: (file)&lt;BR /&gt;Disk /home/niranjan/fsl-community-bsp/build_emmc/tmp/deploy/images/phx-core-pca/core-image-phx-core-pca-phx-core-pca-20180108114647.rootfs.sdcard: 302MB&lt;BR /&gt;Sector size (logical/physical): 512B/512B&lt;BR /&gt;Partition Table: msdos&lt;BR /&gt;Disk Flags:&lt;/P&gt;&lt;P&gt;Number Start End Size Type File system Flags&lt;BR /&gt; 1 4194kB 12.6MB 8389kB primary lba&lt;BR /&gt; 2 12.6MB 298MB 285MB primary&lt;/P&gt;&lt;P&gt;758+0 records in&lt;BR /&gt;758+0 records out&lt;BR /&gt;388096 bytes (388 kB) copied, 0.000897308 s, 433 MB/s&lt;BR /&gt;mkfs.vfat 2.11 (12 Mar 2005)&lt;BR /&gt;WARNING: exit code 1 from a shell command.&lt;/P&gt;&lt;P&gt;DEBUG: Python function do_rootfs finished&lt;BR /&gt;ERROR: Function failed: do_rootfs&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jan 2018 13:52:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-The-image-creation-script/m-p/778143#M120869</guid>
      <dc:creator>niranjanbc</dc:creator>
      <dc:date>2018-01-10T13:52:45Z</dc:date>
    </item>
    <item>
      <title>Re: Error: The image creation script</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-The-image-creation-script/m-p/778144#M120870</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello niranjanbc,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would you please provide more details on what hosts are you using? The Yocto NXP works with Ubuntu as that is the preferred host OS. Using other OS may cause errors as some packages are not available to older or newer BSPs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would you please also comment what specific BSP are you using?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jan 2018 21:09:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-The-image-creation-script/m-p/778144#M120870</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2018-01-11T21:09:46Z</dc:date>
    </item>
    <item>
      <title>Re: Error: The image creation script</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-The-image-creation-script/m-p/778145#M120871</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i am using Ubuntu 14.04, it is same across all the machines&lt;/P&gt;&lt;P&gt;i am using fido branch bsp.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jan 2018 11:09:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-The-image-creation-script/m-p/778145#M120871</guid>
      <dc:creator>niranjanbc</dc:creator>
      <dc:date>2018-01-12T11:09:18Z</dc:date>
    </item>
  </channel>
</rss>