<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: MIMXRT1050-EVK OCRAM single step debugging</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1050-EVK-OCRAM-single-step-debugging/m-p/777136#M120637</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; perhaps the following helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/985705"&gt;https://community.nxp.com/message/985705&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 31 May 2018 06:58:12 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2018-05-31T06:58:12Z</dc:date>
    <item>
      <title>MIMXRT1050-EVK OCRAM single step debugging</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1050-EVK-OCRAM-single-step-debugging/m-p/777135#M120636</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a MIMXRT1050-EVK (not EVKB) and am running the 2.3.0 SDK with LWIP and FreeRTOS and developing with MCUXpresso IDE.&amp;nbsp; My application is too large to fit into ITC RAM so it is placed in OC RAM.&amp;nbsp; If I load the application and attempt to single step (step into or step over), nothing happens to the M7 registers except the cycle register increases by 11 - the program does not step forward, the PC does not change, etc...&amp;nbsp; If I place a breakpoint further along in the code then "Resume" the code, the application hits the breakpoint; however, single stepping from the breakpoint again results in no change to the PC.&lt;/P&gt;&lt;P&gt;If I completely disable OCRAM caching (TypeExtField = 0, IsShareable = 0, IsCacheable = 0, IsBufferable = 0) then I can single step.&amp;nbsp; Unfortunately, with OCRAM&amp;nbsp; caching disabled the application does not appear to be fast enough to handle high speed USB while running FreeRTOS - interrupts are dumped to the queue faster than the application can service them.&amp;nbsp; I have tried both Write Through (&lt;SPAN&gt;IsCacheable = 1, IsBufferable = 0) and Write Back (IsCacheable = 1, IsBufferable = 1) caching; neither allow me to single step in OCRAM.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;This problem occurs with both the&amp;nbsp;on-board debugger and an external Keil Ulink2 debugger, so I do not think it is a debugger issue.&lt;/P&gt;&lt;P&gt;Likewise, I do not think this is an MCUExpresso issue as I am able to single step with caching off or when the executable is in ITC.&lt;/P&gt;&lt;P&gt;Is there a way to single step the debugger with OCRAM cache enabled?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 May 2018 14:27:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1050-EVK-OCRAM-single-step-debugging/m-p/777135#M120636</guid>
      <dc:creator>michaelwhite</dc:creator>
      <dc:date>2018-05-22T14:27:05Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1050-EVK OCRAM single step debugging</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1050-EVK-OCRAM-single-step-debugging/m-p/777136#M120637</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; perhaps the following helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/985705"&gt;https://community.nxp.com/message/985705&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 May 2018 06:58:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1050-EVK-OCRAM-single-step-debugging/m-p/777136#M120637</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2018-05-31T06:58:12Z</dc:date>
    </item>
  </channel>
</rss>