<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Installing Ubuntu using Mfgtools in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Installing-Ubuntu-using-Mfgtools/m-p/776931#M120616</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Which board are you using? Have your u-boot success boot up, you need to set the kernel parameters in you u-boot.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 May 2018 08:11:59 GMT</pubDate>
    <dc:creator>Rita_Wang</dc:creator>
    <dc:date>2018-05-17T08:11:59Z</dc:date>
    <item>
      <title>Installing Ubuntu using Mfgtools</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Installing-Ubuntu-using-Mfgtools/m-p/776930#M120615</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I really new to this area. I've got complete files of Mfgtools with it's Ubuntu Trusty image (trusty.tgz). I run the mfgtools with serial download mode to install the ubuntu to eMMC, and it works fine. But after I restart the board (boot from eMMC), it's give me only blank screen (trough HDMI). Do you know why? Should I extract the trusty.tgz file under "Mfgtools-HOBBITQ-Ubuntu-1.0\Profiles\MX6Q Linux Update\OS Firmware\files"?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Apr 2018 07:45:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Installing-Ubuntu-using-Mfgtools/m-p/776930#M120615</guid>
      <dc:creator>kovzone</dc:creator>
      <dc:date>2018-04-09T07:45:37Z</dc:date>
    </item>
    <item>
      <title>Re: Installing Ubuntu using Mfgtools</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Installing-Ubuntu-using-Mfgtools/m-p/776931#M120616</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Which board are you using? Have your u-boot success boot up, you need to set the kernel parameters in you u-boot.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 May 2018 08:11:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Installing-Ubuntu-using-Mfgtools/m-p/776931#M120616</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2018-05-17T08:11:59Z</dc:date>
    </item>
  </channel>
</rss>