<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: iMX6quad SABRE SDB</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6quad-SABRE-SDB/m-p/776483#M120543</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Also, Can Android Studio supports 'C ' language or only java ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bharathi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Feb 2018 10:42:57 GMT</pubDate>
    <dc:creator>basinibharathi</dc:creator>
    <dc:date>2018-02-28T10:42:57Z</dc:date>
    <item>
      <title>iMX6quad SABRE SDB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6quad-SABRE-SDB/m-p/776480#M120540</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on iMX6 quad sabre sd board booting with android OS(SD Card). I want to implement some applications related to image processing, video/audio processing using existing interfaces/peripherals.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which is the right platform/software to write the code for the application and integrate the same with the existing OS on the iMX6 and debug/test the same.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please suggest me on the above.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Bharathi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Feb 2018 06:00:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6quad-SABRE-SDB/m-p/776480#M120540</guid>
      <dc:creator>basinibharathi</dc:creator>
      <dc:date>2018-02-27T06:00:08Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6quad SABRE SDB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6quad-SABRE-SDB/m-p/776481#M120541</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is a kind of general Android application development question. So, please refer to the following resource:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fdeveloper.android.com%2Findex.html" rel="nofollow" target="_blank"&gt;https://developer.android.com/index.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Feb 2018 10:02:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6quad-SABRE-SDB/m-p/776481#M120541</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2018-02-28T10:02:20Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6quad SABRE SDB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6quad-SABRE-SDB/m-p/776482#M120542</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Artur,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your&amp;nbsp;input.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I tried to install a new apk file on my SD card and boot iMX6, I am not seeing the application on HDMI screen, even though the application is installed successfully using the below command.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;adb install &lt;EM&gt;&lt;STRONG&gt;application.apk&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any idea what could be the wrong?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bharathi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Feb 2018 10:30:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6quad-SABRE-SDB/m-p/776482#M120542</guid>
      <dc:creator>basinibharathi</dc:creator>
      <dc:date>2018-02-28T10:30:00Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6quad SABRE SDB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6quad-SABRE-SDB/m-p/776483#M120543</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Also, Can Android Studio supports 'C ' language or only java ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bharathi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Feb 2018 10:42:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6quad-SABRE-SDB/m-p/776483#M120543</guid>
      <dc:creator>basinibharathi</dc:creator>
      <dc:date>2018-02-28T10:42:57Z</dc:date>
    </item>
  </channel>
</rss>