<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: EVK-MIMXRT1050 FLEXSPI Hyperflash example not working in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/EVK-MIMXRT1050-FLEXSPI-Hyperflash-example-not-working/m-p/776370#M120526</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Twinkle&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you are right, as xip code is running from flash, all flexspi initializations should be implemented before running test.&lt;BR /&gt;Also as this example erases flash, seems it is necessary to pay attention that xip code was not erased by test.&lt;/P&gt;&lt;P&gt;If the code is executed from hyperflash, image requires a header for the internal ROM to boot the image. &lt;BR /&gt;If the header is not present, the image will not boot after reset. The hello_world_xip demo in the SDK &lt;BR /&gt;has an example of how to build the image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 04 Feb 2018 22:40:12 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-02-04T22:40:12Z</dc:date>
    <item>
      <title>EVK-MIMXRT1050 FLEXSPI Hyperflash example not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/EVK-MIMXRT1050-FLEXSPI-Hyperflash-example-not-working/m-p/776369#M120525</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to run the hyper flash polling transfer example in the sdk_2.3.0_evk-mimxrt1050 on the MIMXRT1050-EVK board. I ran it in the debug mode, with no XIP. The code ran as expected. But when I changed it to a XIP project, it didn't work as expected. It just resets itself.&lt;/P&gt;&lt;P&gt;Looking at the code, I found a FLEXSPI_SoftwareReset function, which does a software reset. As a result whenever the code is run, it enters a loop where it resets itself. This function is called many times (during init, after flash erase, after flash program).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since the code is running as XIP, I'm not sure, if we have to again initialize the FLEXSPI module, as in fsl_flexspi_nor_flash.c (in the XIP folder), I saw some FLEXSPI configurations.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How do we run the example code as XIP? Do we need to skip the initializations...?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Feb 2018 07:35:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/EVK-MIMXRT1050-FLEXSPI-Hyperflash-example-not-working/m-p/776369#M120525</guid>
      <dc:creator>2winkle</dc:creator>
      <dc:date>2018-02-01T07:35:19Z</dc:date>
    </item>
    <item>
      <title>Re: EVK-MIMXRT1050 FLEXSPI Hyperflash example not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/EVK-MIMXRT1050-FLEXSPI-Hyperflash-example-not-working/m-p/776370#M120526</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Twinkle&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you are right, as xip code is running from flash, all flexspi initializations should be implemented before running test.&lt;BR /&gt;Also as this example erases flash, seems it is necessary to pay attention that xip code was not erased by test.&lt;/P&gt;&lt;P&gt;If the code is executed from hyperflash, image requires a header for the internal ROM to boot the image. &lt;BR /&gt;If the header is not present, the image will not boot after reset. The hello_world_xip demo in the SDK &lt;BR /&gt;has an example of how to build the image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 04 Feb 2018 22:40:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/EVK-MIMXRT1050-FLEXSPI-Hyperflash-example-not-working/m-p/776370#M120526</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-02-04T22:40:12Z</dc:date>
    </item>
  </channel>
</rss>