<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックimx6d can't work well when using two capture interface</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6d-can-t-work-well-when-using-two-capture-interface/m-p/776361#M120519</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;the single comes from ds90ub940 and adv7180 ,ds90ub940 config is ipu0、csi1、VC1，adv7180 config is ipu0、csi0、VC0，if&amp;nbsp; ds90ub940's FPDlink is disconnected this two video will lost. this two video device can work well along .can somebody help me thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 Jun 2018 03:14:48 GMT</pubDate>
    <dc:creator>leihe</dc:creator>
    <dc:date>2018-06-13T03:14:48Z</dc:date>
    <item>
      <title>imx6d can't work well when using two capture interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6d-can-t-work-well-when-using-two-capture-interface/m-p/776361#M120519</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;the single comes from ds90ub940 and adv7180 ,ds90ub940 config is ipu0、csi1、VC1，adv7180 config is ipu0、csi0、VC0，if&amp;nbsp; ds90ub940's FPDlink is disconnected this two video will lost. this two video device can work well along .can somebody help me thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jun 2018 03:14:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6d-can-t-work-well-when-using-two-capture-interface/m-p/776361#M120519</guid>
      <dc:creator>leihe</dc:creator>
      <dc:date>2018-06-13T03:14:48Z</dc:date>
    </item>
    <item>
      <title>Re: imx6d can't work well when using two capture interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6d-can-t-work-well-when-using-two-capture-interface/m-p/776362#M120520</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi lei&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;may be helpful to look at several cameras example on&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-328548"&gt;iMX6DQ MAX9286 MIPI CSI2 720P camera surround view solution for Linux BSP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jun 2018 05:54:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6d-can-t-work-well-when-using-two-capture-interface/m-p/776362#M120520</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-06-13T05:54:16Z</dc:date>
    </item>
  </channel>
</rss>