<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx7d external clock source voltage range in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx7d-external-clock-source-voltage-range/m-p/775760#M120464</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Felix,&lt;/P&gt;&lt;P&gt;When the pad is configured to SD card functionality, it will be tight to 3.3V rail; however, when using the pin as CCM_EXT_CLK, it will be tight to 1.8V rail.&lt;/P&gt;&lt;P&gt;As a final note, all of the CCM CLK pins are outputs (the N/P are differential outputs, and the other are single-ended).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this will be useful for you.&lt;/P&gt;&lt;P&gt;Best regards!&lt;/P&gt;&lt;P&gt;/Carlos&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 12 Jan 2018 00:39:28 GMT</pubDate>
    <dc:creator>CarlosCasillas</dc:creator>
    <dc:date>2018-01-12T00:39:28Z</dc:date>
    <item>
      <title>imx7d external clock source voltage range</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx7d-external-clock-source-voltage-range/m-p/775757#M120461</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you tell me the imx7d external clock source voltage range is 1.8V or 3.3V or other voltage range?&lt;/P&gt;&lt;P&gt;PS: the external clock means EXT_CLK1 or&amp;nbsp;&lt;SPAN&gt;EXT_CLK2 ...etc.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/26i6AE75B4BB82EA401/image-size/large?v=v2&amp;amp;px=999" title="CCM.png" alt="CCM.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jan 2018 10:18:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx7d-external-clock-source-voltage-range/m-p/775757#M120461</guid>
      <dc:creator>felixhsu</dc:creator>
      <dc:date>2018-01-10T10:18:15Z</dc:date>
    </item>
    <item>
      <title>Re: imx7d external clock source voltage range</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx7d-external-clock-source-voltage-range/m-p/775758#M120462</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Felix,&lt;/P&gt;&lt;P&gt;You could refer to section 5.3.2 of the i.MX7D Reference Manual, where it is mentioned oscillator pads should be supplied to 1.8V, and higher voltages must not be applied:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/reference-manual/IMX7DRM.pdf"&gt;https://www.nxp.com/docs/en/reference-manual/IMX7DRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this will be useful for you.&lt;/P&gt;&lt;P&gt;Best regards!&lt;/P&gt;&lt;P&gt;/Carlos&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jan 2018 23:34:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx7d-external-clock-source-voltage-range/m-p/775758#M120462</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2018-01-10T23:34:57Z</dc:date>
    </item>
    <item>
      <title>Re: imx7d external clock source voltage range</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx7d-external-clock-source-voltage-range/m-p/775759#M120463</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;If "SD1_DATA1(pin D6)"&amp;nbsp;is set to&amp;nbsp;"CCM_EXT_CLK2" and NVCC_SD1 : 3.3V.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; OSC&amp;nbsp;clock input can not exceed 1.8V too?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/2188i4B9927062CB69C2F/image-size/large?v=v2&amp;amp;px=999" title="擷取0111.PNG" alt="擷取0111.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jan 2018 07:54:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx7d-external-clock-source-voltage-range/m-p/775759#M120463</guid>
      <dc:creator>twhsueh</dc:creator>
      <dc:date>2018-01-11T07:54:45Z</dc:date>
    </item>
    <item>
      <title>Re: imx7d external clock source voltage range</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx7d-external-clock-source-voltage-range/m-p/775760#M120464</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Felix,&lt;/P&gt;&lt;P&gt;When the pad is configured to SD card functionality, it will be tight to 3.3V rail; however, when using the pin as CCM_EXT_CLK, it will be tight to 1.8V rail.&lt;/P&gt;&lt;P&gt;As a final note, all of the CCM CLK pins are outputs (the N/P are differential outputs, and the other are single-ended).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this will be useful for you.&lt;/P&gt;&lt;P&gt;Best regards!&lt;/P&gt;&lt;P&gt;/Carlos&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jan 2018 00:39:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx7d-external-clock-source-voltage-range/m-p/775760#M120464</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2018-01-12T00:39:28Z</dc:date>
    </item>
  </channel>
</rss>