<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: iMX6 JTAG_MOD as GPIO</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-JTAG-MOD-as-GPIO/m-p/775656#M120432</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Artur, why cannot JTAG_MOD be used as GPIO?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And if it cannot, why is this not mentioned in the manual?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks, Leon.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Oct 2018 14:35:08 GMT</pubDate>
    <dc:creator>sidebranch</dc:creator>
    <dc:date>2018-10-25T14:35:08Z</dc:date>
    <item>
      <title>iMX6 JTAG_MOD as GPIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-JTAG-MOD-as-GPIO/m-p/775653#M120429</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using IMX6UL (MCIMX6G3CVM05AB) for custom board and due to limited number of pins want to use JTAG_MOD as GPIO output. At the same time we want to use JTAG for system debug during development phase.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;RM 45.2 states that "this pin is sampled at TRST reset to determine mode of operation" - does that mean that changing this pin to GPIO output high after startup (when TRST is high) won't affect JTAG operation? JTAG_TRST is not used and is pulled high permanently.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Dmitry&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Nov 2017 00:36:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-JTAG-MOD-as-GPIO/m-p/775653#M120429</guid>
      <dc:creator>dmitrykolyadint</dc:creator>
      <dc:date>2017-11-15T00:36:05Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 JTAG_MOD as GPIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-JTAG-MOD-as-GPIO/m-p/775654#M120430</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Although i.MX6UL RM shows the SW_MOD_CTRL register for the JTAG_MOD pad, there is no way to use this pad for any alternate function other than JTAG_MOD, otherwise, the processor may lock. So, there is no way to use the JTAG_MOD pad as GPIO.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Nov 2017 11:33:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-JTAG-MOD-as-GPIO/m-p/775654#M120430</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2017-11-27T11:33:09Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 JTAG_MOD as GPIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-JTAG-MOD-as-GPIO/m-p/775655#M120431</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Artur.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Nov 2017 10:12:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-JTAG-MOD-as-GPIO/m-p/775655#M120431</guid>
      <dc:creator>dmitrykolyadint</dc:creator>
      <dc:date>2017-11-30T10:12:55Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 JTAG_MOD as GPIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-JTAG-MOD-as-GPIO/m-p/775656#M120432</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Artur, why cannot JTAG_MOD be used as GPIO?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And if it cannot, why is this not mentioned in the manual?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks, Leon.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Oct 2018 14:35:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-JTAG-MOD-as-GPIO/m-p/775656#M120432</guid>
      <dc:creator>sidebranch</dc:creator>
      <dc:date>2018-10-25T14:35:08Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 JTAG_MOD as GPIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-JTAG-MOD-as-GPIO/m-p/775657#M120433</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Artur,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does the same apply to the IMXRT1060?&amp;nbsp; I was thinking of using this pin as a GPIO and didn't know if this problem also exists on the RT1060.&amp;nbsp; I tested it out and I am able to toggle the GPIO and still debug using SWD.&amp;nbsp; Please let me know your thoughts.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jake&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 May 2019 22:22:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-JTAG-MOD-as-GPIO/m-p/775657#M120433</guid>
      <dc:creator>jakepollex</dc:creator>
      <dc:date>2019-05-23T22:22:19Z</dc:date>
    </item>
  </channel>
</rss>