<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic HY4635 touch controller not responding properly in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/HY4635-touch-controller-not-responding-properly/m-p/774622#M120252</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using a 7" LCD (800*480)display(RGB interface) with cap touch (I2C interface) and the touch controller used is&amp;nbsp;HY4635 and IMX6 SOLO processor is used. So the response of the touch is not very accurate and when the values are read in terminal window most of the time it shows wrong (X,Y) values like out of bound.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Only some times there is the response . we cannot &amp;nbsp;do the drag operation but once in a while just single touch will respond that to very slowly .&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can anyone please suggest whats the issue?&lt;/P&gt;&lt;P&gt;Any driver changes that need to be done ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 27 Apr 2018 04:54:07 GMT</pubDate>
    <dc:creator>karthikssk</dc:creator>
    <dc:date>2018-04-27T04:54:07Z</dc:date>
    <item>
      <title>HY4635 touch controller not responding properly</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HY4635-touch-controller-not-responding-properly/m-p/774622#M120252</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using a 7" LCD (800*480)display(RGB interface) with cap touch (I2C interface) and the touch controller used is&amp;nbsp;HY4635 and IMX6 SOLO processor is used. So the response of the touch is not very accurate and when the values are read in terminal window most of the time it shows wrong (X,Y) values like out of bound.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Only some times there is the response . we cannot &amp;nbsp;do the drag operation but once in a while just single touch will respond that to very slowly .&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can anyone please suggest whats the issue?&lt;/P&gt;&lt;P&gt;Any driver changes that need to be done ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Apr 2018 04:54:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HY4635-touch-controller-not-responding-properly/m-p/774622#M120252</guid>
      <dc:creator>karthikssk</dc:creator>
      <dc:date>2018-04-27T04:54:07Z</dc:date>
    </item>
    <item>
      <title>Re: HY4635 touch controller not responding properly</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HY4635-touch-controller-not-responding-properly/m-p/774623#M120253</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Karthik&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can test with linux driver provided by HY4635 vendor&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.hycontek.com/wp-content/uploads/Linux_driver_sample_code.zip" title="http://www.hycontek.com/wp-content/uploads/Linux_driver_sample_code.zip"&gt;http://www.hycontek.com/wp-content/uploads/Linux_driver_sample_code.zip&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and try to calibrate using guidelines on&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://boundarydevices.com/tweaking-froyo-for-nitrogen-part-1-touch-support/" title="https://boundarydevices.com/tweaking-froyo-for-nitrogen-part-1-touch-support/"&gt;Tweaking Froyo for Nitrogen Part 1: touch support - Boundary Devices&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 28 Apr 2018 06:31:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HY4635-touch-controller-not-responding-properly/m-p/774623#M120253</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-04-28T06:31:46Z</dc:date>
    </item>
  </channel>
</rss>