<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: not able to boot custom imx6ull board using eMMC</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/not-able-to-boot-custom-imx6ull-board-using-eMMC/m-p/774526#M120234</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;so is there any boot&amp;nbsp;log from eMMC ?&lt;/P&gt;&lt;P&gt;If not any log, connect jtag and check boot configuration reading SRC_SBMR1,2&lt;/P&gt;&lt;P&gt;registers, check emmc signals with oscilloscope during boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 30 Apr 2018 08:03:04 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-04-30T08:03:04Z</dc:date>
    <item>
      <title>not able to boot custom imx6ull board using eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/not-able-to-boot-custom-imx6ull-board-using-eMMC/m-p/774521#M120229</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have created custom u-boot using DCD changes, custom kernel [zImage] with changes for UTP and USB_MASS_STORAGE in defconfig. Able to build the yocto images with customized u-boot, zImage and DTB. Able to flash via serial downloader using mfgtool2. I see all the output such as u-boot and kernel logs correctly on debug uart, But i am not able to get the board booted via eMMC after flashing. I do not see anything on serial. Can anyone faced the same issue.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/b45499"&gt;b45499&lt;/A&gt;‌ - Can you please help ! Added logs after flashing. Also DDR calibration is done for my KINGSTON DDR3L - 4G using DDR stress tester tool. I do not know why it still does not boot from eMMC. I see all the partitions created successfully.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is this some problem with boot partition&amp;nbsp;&lt;/P&gt;&lt;P&gt;in u-boot&amp;nbsp;./include/configs/mx6ullevk.h,&amp;nbsp;CONFIG_SYS_MMC_ENV_PART = 0, is this problem due to it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help is highly appreciated&amp;nbsp; !&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Apr 2018 11:29:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/not-able-to-boot-custom-imx6ull-board-using-eMMC/m-p/774521#M120229</guid>
      <dc:creator>pankajjoshi</dc:creator>
      <dc:date>2018-04-27T11:29:57Z</dc:date>
    </item>
    <item>
      <title>Re: not able to boot custom emx6ull board using eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/not-able-to-boot-custom-imx6ull-board-using-eMMC/m-p/774522#M120230</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pankaj&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;was ddr memory of custom board tested by ddr stress tool&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-105652"&gt;i.MX6/7 DDR Stress Test Tool V2.80&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;New images should be rebuilt with new calibration settings forund from ddr test&lt;/P&gt;&lt;P&gt;(put them in uboot/../mx6ullevk/imximage.cfg).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Apr 2018 23:50:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/not-able-to-boot-custom-imx6ull-board-using-eMMC/m-p/774522#M120230</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-04-27T23:50:37Z</dc:date>
    </item>
    <item>
      <title>Re: not able to boot custom emx6ull board using eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/not-able-to-boot-custom-imx6ull-board-using-eMMC/m-p/774523#M120231</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have used the DDR stress test only with relevant changes in NXP aid script. Below is the calibration result i had&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MMDC registers updated from calibration&lt;/P&gt;&lt;P&gt;Write leveling calibration&lt;BR /&gt; MMDC_MPWLDECTRL0 ch0 (0x021b080c) = 0x00000000&lt;BR /&gt; MMDC_MPWLDECTRL1 ch0 (0x021b0810) = 0x000A000A&lt;/P&gt;&lt;P&gt;Read DQS Gating calibration&lt;BR /&gt; MPDGCTRL0 PHY0 (0x021b083c) = 0x41580154&lt;BR /&gt; MPDGCTRL1 PHY0 (0x021b0840) = 0x00000000&lt;/P&gt;&lt;P&gt;Read calibration&lt;BR /&gt; MPRDDLCTL PHY0 (0x021b0848) = 0x40402E32&lt;/P&gt;&lt;P&gt;Write calibration&lt;BR /&gt; MPWRDLCTL PHY0 (0x021b0850) = 0x40403C38&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I changed according to above calibration coefficient.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please find the flashing logs coming in the debug uart [logsfromflashing.txt]. I see the uboot and kernel and rootfs loaded correctly. I see the partitioning of the eMMC as well. Can there be a problem of boot partition not enabled? Also the imx6ull inc file used for stress testing is attached [imxull.inc]. I used the "mfgtool2-yocto-mx-evk-emmc.vbs" file present in&amp;nbsp; mfgtool2. From flash logs present in&amp;nbsp;&lt;SPAN&gt;logsfromflashing.txt, it looks everything went well. But not still sure why it did not flash from eMMC on reboot.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;If you still suggest, i can run through the DDR stress tester again.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Please help as i am struck in the last step of the complete exercise.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 28 Apr 2018 05:45:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/not-able-to-boot-custom-imx6ull-board-using-eMMC/m-p/774523#M120231</guid>
      <dc:creator>pankajjoshi</dc:creator>
      <dc:date>2018-04-28T05:45:52Z</dc:date>
    </item>
    <item>
      <title>Re: not able to boot custom imx6ull board using eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/not-able-to-boot-custom-imx6ull-board-using-eMMC/m-p/774524#M120232</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pankaj&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;could you clarify what do you mean by:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"&lt;SPAN&gt; But not still sure why it did not flash from eMMC on reboot. &lt;/SPAN&gt;"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So described problem relates to mfg tool programming ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Apr 2018 07:09:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/not-able-to-boot-custom-imx6ull-board-using-eMMC/m-p/774524#M120232</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-04-30T07:09:45Z</dc:date>
    </item>
    <item>
      <title>Re: not able to boot custom imx6ull board using eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/not-able-to-boot-custom-imx6ull-board-using-eMMC/m-p/774525#M120233</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My bad, i meant to say, it is flashing properly via mfgtool2. I see correct logs as well. However it does not boot from eMMC.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Apr 2018 07:19:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/not-able-to-boot-custom-imx6ull-board-using-eMMC/m-p/774525#M120233</guid>
      <dc:creator>pankajjoshi</dc:creator>
      <dc:date>2018-04-30T07:19:31Z</dc:date>
    </item>
    <item>
      <title>Re: not able to boot custom imx6ull board using eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/not-able-to-boot-custom-imx6ull-board-using-eMMC/m-p/774526#M120234</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;so is there any boot&amp;nbsp;log from eMMC ?&lt;/P&gt;&lt;P&gt;If not any log, connect jtag and check boot configuration reading SRC_SBMR1,2&lt;/P&gt;&lt;P&gt;registers, check emmc signals with oscilloscope during boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Apr 2018 08:03:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/not-able-to-boot-custom-imx6ull-board-using-eMMC/m-p/774526#M120234</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-04-30T08:03:04Z</dc:date>
    </item>
    <item>
      <title>Re: not able to boot custom imx6ull board using eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/not-able-to-boot-custom-imx6ull-board-using-eMMC/m-p/774527#M120235</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please have a look on my boot logs.&lt;/P&gt;&lt;P&gt;U-Boot 2017.03-nxp/imx_v2017.03_4.9.11_1.0.0_ga+ga2fea67 (Apr 26 2018 - 10:33:31 +0530)&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX6ULL rev1.0 528 MHz (running at 396 MHz)&lt;BR /&gt;CPU: Industrial temperature grade (-40C to 105C) at 52C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: Freescale i.MX6 ULL 14x14 EVK Board&lt;BR /&gt;Board: MX6ULL 14x14 EVK&lt;BR /&gt;DRAM: 512 MiB&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;BR /&gt;*** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;Display: TFT43AB (480x272)&lt;BR /&gt;Video: 480x272x24&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1(part 0) is current device&lt;BR /&gt;Net: No ethernet found.&lt;BR /&gt;Boot from USB for mfgtools&lt;BR /&gt;Use default environment for mfgtools&lt;BR /&gt;Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;Kernel image @ 0x80800000 [ 0x000000 - 0x6d5178 ]&lt;BR /&gt;## Loading init Ramdisk from Legacy Image at 83800000 ...&lt;BR /&gt; Image Name: fsl-image-mfgtool-initramfs-imx6&lt;BR /&gt; Image Type: ARM Linux RAMDisk Image (gzip compressed)&lt;BR /&gt; Data Size: 8591032 Bytes = 8.2 MiB&lt;BR /&gt; Load Address: 00000000&lt;BR /&gt; Entry Point: 00000000&lt;BR /&gt; Verifying Checksum ... OK&lt;BR /&gt;## Flattened Device Tree blob at 83000000&lt;BR /&gt; Booting using the fdt blob at 0x83000000&lt;BR /&gt; Using Device Tree in place at 83000000, end 8300bda2&lt;BR /&gt;Modify /soc/aips-bus@02200000/epdc@0228c000:status disabled&lt;BR /&gt;ft_system_setup for mx6&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;Booting Linux on physical CPU 0x0&lt;BR /&gt;Linux version 4.9.11-1.0.0+gc27010d (lem@LEM) (gcc version 6.2.0 (GCC) ) #1 SMP PREEMPT Thu Apr 26 15:33:25 IST 2018&lt;BR /&gt;CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c53c7d&lt;BR /&gt;CPU: div instructions available: patching division code&lt;BR /&gt;CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache&lt;BR /&gt;OF: fdt:Machine model: Freescale i.MX6 ULL 14x14 EVK Board&lt;BR /&gt;Reserved memory: created CMA memory pool at 0x8c000000, size 320 MiB&lt;BR /&gt;OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool&lt;BR /&gt;Memory policy: Data cache writealloc&lt;BR /&gt;percpu: Embedded 14 pages/cpu @8bb31000 s25868 r8192 d23284 u57344&lt;BR /&gt;Built 1 zonelists in Zone order, mobility grouping on. Total pages: 130048&lt;BR /&gt;Kernel command line: console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.file=/fat g_mass_storage.ro=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber= clk_ignore_unused&lt;BR /&gt;PID hash table entries: 2048 (order: 1, 8192 bytes)&lt;BR /&gt;Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)&lt;BR /&gt;Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)&lt;BR /&gt;Memory: 167548K/524288K available (9216K kernel code, 485K rwdata, 3236K rodata, 1024K init, 472K bss, 29060K reserved, 327680K cma-reserved, 0K highmem)&lt;BR /&gt;Virtual kernel memory layout:&lt;BR /&gt; vector : 0xffff0000 - 0xffff1000 ( 4 kB)&lt;BR /&gt; fixmap : 0xffc00000 - 0xfff00000 (3072 kB)&lt;BR /&gt; vmalloc : 0xa0800000 - 0xff800000 (1520 MB)&lt;BR /&gt; lowmem : 0x80000000 - 0xa0000000 ( 512 MB)&lt;BR /&gt; pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)&lt;BR /&gt; modules : 0x7f000000 - 0x7fe00000 ( 14 MB)&lt;BR /&gt; .text : 0x80008000 - 0x80a00000 (10208 kB)&lt;BR /&gt; .init : 0x80e00000 - 0x80f00000 (1024 kB)&lt;BR /&gt; .data : 0x80f00000 - 0x80f796a0 ( 486 kB)&lt;BR /&gt; .bss : 0x80f7b000 - 0x80ff10e0 ( 473 kB)&lt;BR /&gt;SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1&lt;BR /&gt;Preemptible hierarchical RCU implementation.&lt;BR /&gt; Build-time adjustment of leaf fanout to 32.&lt;BR /&gt; RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.&lt;BR /&gt;RCU: Adjusting geometry for rcu_fanout_leaf=32, nr_cpu_ids=1&lt;BR /&gt;NR_IRQS:16 nr_irqs:16 16&lt;BR /&gt;Switching to timer-based delay loop, resolution 333ns&lt;BR /&gt;sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns&lt;BR /&gt;clocksource: mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns&lt;BR /&gt;Console: colour dummy device 80x30&lt;BR /&gt;Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)&lt;BR /&gt;pid_max: default: 32768 minimum: 301&lt;BR /&gt;Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)&lt;BR /&gt;Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)&lt;BR /&gt;CPU: Testing write buffer coherency: ok&lt;BR /&gt;/cpus/cpu@0 missing clock-frequency property&lt;BR /&gt;CPU0: thread -1, cpu 0, socket 0, mpidr 80000000&lt;BR /&gt;Setting up static identity map for 0x80100000 - 0x80100058&lt;BR /&gt;Brought up 1 CPUs&lt;BR /&gt;SMP: Total of 1 processors activated (6.00 BogoMIPS).&lt;BR /&gt;CPU: All CPU(s) started in SVC mode.&lt;BR /&gt;devtmpfs: initialized&lt;BR /&gt;VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5&lt;BR /&gt;clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns&lt;BR /&gt;pinctrl core: initialized pinctrl subsystem&lt;BR /&gt;NET: Registered protocol family 16&lt;BR /&gt;DMA: preallocated 256 KiB pool for atomic coherent allocations&lt;BR /&gt;cpuidle: using governor menu&lt;BR /&gt;hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.&lt;BR /&gt;hw-breakpoint: maximum watchpoint size is 8 bytes.&lt;BR /&gt;imx6ul-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver&lt;BR /&gt;imx6ul-pinctrl 2290000.iomuxc-snvs: initialized IMX pinctrl driver&lt;BR /&gt;mxs-dma 1804000.dma-apbh: initialized&lt;BR /&gt;SCSI subsystem initialized&lt;BR /&gt;usbcore: registered new interface driver usbfs&lt;BR /&gt;usbcore: registered new interface driver hub&lt;BR /&gt;usbcore: registered new device driver usb&lt;BR /&gt;i2c i2c-0: IMX I2C adapter registered&lt;BR /&gt;i2c i2c-0: can't use DMA, using PIO instead.&lt;BR /&gt;i2c i2c-1: IMX I2C adapter registered&lt;BR /&gt;i2c i2c-1: can't use DMA, using PIO instead.&lt;BR /&gt;Linux video capture interface: v2.00&lt;BR /&gt;pps_core: LinuxPPS API ver. 1 registered&lt;BR /&gt;&lt;SPAN&gt;pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti &amp;lt;&lt;/SPAN&gt;&lt;A class="jive-link-email-small" href="mailto:giometti@linux.it"&gt;giometti@linux.it&lt;/A&gt;&lt;SPAN&gt;&amp;gt;&lt;/SPAN&gt;&lt;BR /&gt;PTP clock support registered&lt;BR /&gt;MIPI CSI2 driver module loaded&lt;BR /&gt;imx rpmsg driver is registered.&lt;BR /&gt;Advanced Linux Sound Architecture Driver Initialized.&lt;BR /&gt;Bluetooth: Core ver 2.22&lt;BR /&gt;NET: Registered protocol family 31&lt;BR /&gt;Bluetooth: HCI device and connection manager initialized&lt;BR /&gt;Bluetooth: HCI socket layer initialized&lt;BR /&gt;Bluetooth: L2CAP socket layer initialized&lt;BR /&gt;Bluetooth: SCO socket layer initialized&lt;BR /&gt;clocksource: Switched to clocksource mxc_timer1&lt;BR /&gt;VFS: Disk quotas dquot_6.6.0&lt;BR /&gt;VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)&lt;BR /&gt;NET: Registered protocol family 2&lt;BR /&gt;TCP established hash table entries: 4096 (order: 2, 16384 bytes)&lt;BR /&gt;TCP bind hash table entries: 4096 (order: 3, 32768 bytes)&lt;BR /&gt;TCP: Hash tables configured (established 4096 bind 4096)&lt;BR /&gt;UDP hash table entries: 256 (order: 1, 8192 bytes)&lt;BR /&gt;UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)&lt;BR /&gt;NET: Registered protocol family 1&lt;BR /&gt;RPC: Registered named UNIX socket transport module.&lt;BR /&gt;RPC: Registered udp transport module.&lt;BR /&gt;RPC: Registered tcp transport module.&lt;BR /&gt;RPC: Registered tcp NFSv4.1 backchannel transport module.&lt;BR /&gt;Trying to unpack rootfs image as initramfs...&lt;BR /&gt;Freeing initrd memory: 8392K (83800000 - 84032000)&lt;BR /&gt;Bus freq driver module loaded&lt;BR /&gt;futex hash table entries: 256 (order: 2, 16384 bytes)&lt;BR /&gt;workingset: timestamp_bits=30 max_order=17 bucket_order=0&lt;BR /&gt;NFS: Registering the id_resolver key type&lt;BR /&gt;Key type id_resolver registered&lt;BR /&gt;Key type id_legacy registered&lt;BR /&gt;jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.&lt;BR /&gt;fuse init (API version 7.26)&lt;BR /&gt;io scheduler noop registered&lt;BR /&gt;io scheduler deadline registered&lt;BR /&gt;io scheduler cfq registered (default)&lt;BR /&gt;imx-weim 21b8000.weim: Driver registered.&lt;BR /&gt;backlight supply power not found, using dummy regulator&lt;BR /&gt;21c8000.lcdif supply lcd not found, using dummy regulator&lt;BR /&gt;mxsfb 21c8000.lcdif: failed to find mxc display driver&lt;BR /&gt;Console: switching to colour frame buffer device 60x34&lt;BR /&gt;mxsfb 21c8000.lcdif: initialized&lt;BR /&gt;imx-sdma 20ec000.sdma: loaded firmware 3.3&lt;BR /&gt;2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 18, base_baud = 5000000) is a IMX&lt;BR /&gt;random: fast init done&lt;BR /&gt;console [ttymxc0] enabled&lt;BR /&gt;21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 73, base_baud = 5000000) is a IMX&lt;BR /&gt;imx-rng 2284000.rngb: iMX RNG Registered.&lt;BR /&gt;imx sema4 driver is registered.&lt;BR /&gt;[drm] Initialized&lt;BR /&gt;[drm] Initialized vivante 1.0.0 20120216 on minor 0&lt;BR /&gt;brd: module loaded&lt;BR /&gt;loop: module loaded&lt;BR /&gt;fsl-quadspi 21e0000.qspi: unrecognized JEDEC id bytes: ff, ff, ff&lt;BR /&gt;fsl-quadspi 21e0000.qspi: Freescale QuadSPI probe failed&lt;BR /&gt;fsl-quadspi: probe of 21e0000.qspi failed with error -2&lt;BR /&gt;spi_gpio spi4: gpio-miso property not found, switching to no-rx mode&lt;BR /&gt;libphy: Fixed MDIO Bus: probed&lt;BR /&gt;CAN device driver interface&lt;BR /&gt;flexcan 2090000.can: device registered (reg_base=a0a00000, irq=27)&lt;BR /&gt;flexcan 2094000.can: device registered (reg_base=a0a08000, irq=28)&lt;BR /&gt;20b4000.ethernet supply phy not found, using dummy regulator&lt;BR /&gt;pps pps0: new PPS source ptp0&lt;BR /&gt;fec 20b4000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00&lt;BR /&gt;fec 20b4000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: 1e:fb:1e:b2:c9:08&lt;BR /&gt;libphy: fec_enet_mii_bus: probed&lt;BR /&gt;fec 20b4000.ethernet eth0: registered PHC device 0&lt;BR /&gt;2188000.ethernet supply phy not found, using dummy regulator&lt;BR /&gt;pps pps1: new PPS source ptp1&lt;BR /&gt;fec 2188000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00&lt;BR /&gt;fec 2188000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: f2:a9:96:fd:c9:15&lt;BR /&gt;fec 2188000.ethernet eth1: registered PHC device 1&lt;BR /&gt;usbcore: registered new interface driver kaweth&lt;BR /&gt;pegasus: v0.9.3 (2013/04/25), Pegasus/Pegasus II USB Ethernet driver&lt;BR /&gt;usbcore: registered new interface driver pegasus&lt;BR /&gt;usbcore: registered new interface driver rtl8150&lt;BR /&gt;usbcore: registered new interface driver r8152&lt;BR /&gt;usbcore: registered new interface driver asix&lt;BR /&gt;usbcore: registered new interface driver ax88179_178a&lt;BR /&gt;usbcore: registered new interface driver cdc_ether&lt;BR /&gt;usbcore: registered new interface driver net1080&lt;BR /&gt;usbcore: registered new interface driver cdc_subset&lt;BR /&gt;usbcore: registered new interface driver zaurus&lt;BR /&gt;usbcore: registered new interface driver cdc_ncm&lt;BR /&gt;ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver&lt;BR /&gt;ehci-mxc: Freescale On-Chip EHCI Host driver&lt;BR /&gt;usbcore: registered new interface driver usb-storage&lt;BR /&gt;usbcore: registered new interface driver usb_ehset_test&lt;BR /&gt;2184800.usbmisc supply vbus-wakeup not found, using dummy regulator&lt;BR /&gt;2184000.usb supply vbus not found, using dummy regulator&lt;BR /&gt;2184200.usb supply vbus not found, using dummy regulator&lt;BR /&gt;ci_hdrc ci_hdrc.1: EHCI Host Controller&lt;BR /&gt;ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1&lt;BR /&gt;ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00&lt;BR /&gt;hub 1-0:1.0: USB hub found&lt;BR /&gt;hub 1-0:1.0: 1 port detected&lt;BR /&gt;Mass Storage Function, version: 2009/09/11&lt;BR /&gt;LUN: removable file: (no medium)&lt;BR /&gt;LUN: removable read only file: /fat&lt;BR /&gt;Number of LUNs=1&lt;BR /&gt;g_mass_storage gadget: Mass Storage Gadget, version: 2009/09/11&lt;BR /&gt;g_mass_storage gadget: g_mass_storage ready&lt;BR /&gt;mousedev: PS/2 mouse device common for all mice&lt;BR /&gt;input: 20cc000.snvs:snvs-powerkey as /devices/soc0/soc/2000000.aips-bus/20cc000.snvs/20cc000.snvs:snvs-powerkey/input/input0&lt;BR /&gt;input: iMX6UL Touchscreen Controller as /devices/soc0/soc/2000000.aips-bus/2040000.tsc/input/input1&lt;BR /&gt;read sensor who am i (0xfffffffa)error !&lt;BR /&gt;fxls8471: probe of 0-001e failed with error -22&lt;BR /&gt;snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-r as rtc0&lt;BR /&gt;i2c /dev entries driver&lt;BR /&gt;IR NEC protocol handler initialized&lt;BR /&gt;IR RC5(x/sz) protocol handler initialized&lt;BR /&gt;IR RC6 protocol handler initialized&lt;BR /&gt;IR JVC protocol handler initialized&lt;BR /&gt;IR Sony protocol handler initialized&lt;BR /&gt;IR SANYO protocol handler initialized&lt;BR /&gt;IR Sharp protocol handler initialized&lt;BR /&gt;IR MCE Keyboard/mouse protocol handler initialized&lt;BR /&gt;IR XMP protocol handler initialized&lt;BR /&gt;pxp-v4l2 pxp_v4l2: initialized&lt;BR /&gt;0-000e supply vdd not found, using dummy regulator&lt;BR /&gt;0-000e supply vddio not found, using dummy regulator&lt;BR /&gt;mag3110 0-000e: check mag3110 chip ID&lt;BR /&gt;mag3110 0-000e: read chip ID 0xfffffffa is not equal to 0xc4!&lt;BR /&gt;mag3110: probe of 0-000e failed with error -22&lt;BR /&gt;imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)&lt;BR /&gt;Bluetooth: HCI UART driver ver 2.3&lt;BR /&gt;Bluetooth: HCI UART protocol H4 registered&lt;BR /&gt;Bluetooth: HCI UART protocol BCSP registered&lt;BR /&gt;Bluetooth: HCI UART protocol ATH3K registered&lt;BR /&gt;usbcore: registered new interface driver bcm203x&lt;BR /&gt;usbcore: registered new interface driver btusb&lt;BR /&gt;usbcore: registered new interface driver ath3k&lt;BR /&gt;sdhci: Secure Digital Host Controller Interface driver&lt;BR /&gt;sdhci: Copyright(c) Pierre Ossman&lt;BR /&gt;sdhci-pltfm: SDHCI platform and OF driver helper&lt;BR /&gt;sdhci-esdhc-imx 2190000.usdhc: Got CD GPIO&lt;BR /&gt;mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA&lt;BR /&gt;mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA&lt;BR /&gt;g_mass_storage gadget: high-speed config #1: Linux File-Backed Storage&lt;BR /&gt;usbcore: registered new interface driver usbhid&lt;BR /&gt;usbhid: USB HID core driver&lt;BR /&gt;wm8960 1-001a: Failed to issue reset&lt;BR /&gt;imx-wm8960 sound: failed to find codec platform device&lt;BR /&gt;imx-wm8960: probe of sound failed with error -22&lt;BR /&gt;NET: Registered protocol family 26&lt;BR /&gt;NET: Registered protocol family 10&lt;BR /&gt;mmc1: mmc_select_hs200 failed, error -74&lt;BR /&gt;mmc1: new MMC card at address 0001&lt;BR /&gt;sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver&lt;BR /&gt;NET: Registered protocol family 17&lt;BR /&gt;can: controller area network core (rev 20120528 abi 9)&lt;BR /&gt;mmcblk1: mmc1:0001 W62704 3.56 GiB&lt;BR /&gt;NET: Registered protocol family 29&lt;BR /&gt;can: raw protocol (rev 20120528)&lt;BR /&gt;can: broadcast manager protocol (rev 20161123 t)&lt;BR /&gt;mmcblk1boot0: mmc1:0001 W62704 partition 1 2.00 MiB&lt;BR /&gt;can: netlink gateway (rev 20130117) max_hops=1&lt;BR /&gt;Bluetooth: RFCOMM TTY layer initialized&lt;BR /&gt;mmcblk1boot1: mmc1:0001 W62704 partition 2 2.00 MiB&lt;BR /&gt;Bluetooth: RFCOMM socket layer initialized&lt;BR /&gt;Bluetooth: RFCOMM ver 1.11&lt;BR /&gt;Bluetooth: BNEP (Ethernet Emulation) ver 1.3&lt;BR /&gt;mmcblk1rpmb: mmc1:0001 W62704 partition 3 512 KiB&lt;BR /&gt;Bluetooth: BNEP filters: protocol multicast&lt;BR /&gt;Bluetooth: BNEP socket layer initialized&lt;BR /&gt; mmcblk1: p1 p2&lt;BR /&gt;Bluetooth: HIDP (Human Interface Emulation) ver 1.2&lt;BR /&gt;Bluetooth: HIDP socket layer initialized&lt;BR /&gt;8021q: 802.1Q VLAN Support v1.8&lt;BR /&gt;Key type dns_resolver registered&lt;BR /&gt;cpu cpu0: Registered imx6q-cpufreq&lt;BR /&gt;imx_thermal 2000000.aips-bus:tempmon: Industrial CPU temperature grade - max:105C critical:100C passive:95C&lt;BR /&gt;dhd_module_init in&lt;BR /&gt;snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:00:00 UTC (0)&lt;BR /&gt;clk: Not disabling unused clocks&lt;BR /&gt;can-3v3: disabling&lt;BR /&gt;VSD_3V3: disabling&lt;BR /&gt;gpio_dvfs: disabling&lt;BR /&gt;ALSA device list:&lt;BR /&gt; No soundcards found.&lt;BR /&gt;Freeing unused kernel memory: 1024K (80e00000 - 80f00000)&lt;BR /&gt;Starting UTP&lt;BR /&gt;uuc 0.5 [built Sep 16 2016 02:36:28]&lt;BR /&gt;UTP: Waiting for device to appear&lt;BR /&gt;UTP: file/device node /dev/utp already exists&lt;BR /&gt;cpu_id is 0&lt;BR /&gt;UTP: received command 'send'&lt;BR /&gt;UTP: sending Success to kernel for command send.&lt;BR /&gt;UTP: received command '$ tar xf $FILE '&lt;BR /&gt;UTP: executing "tar xf $FILE "&lt;BR /&gt;UTP: sending Success to kernel for command $ tar xf $FILE .&lt;BR /&gt;utp_poll: pass returned.&lt;BR /&gt;UTP: received command '$ sh mksdcard.sh /dev/mmcblk1'&lt;BR /&gt;UTP: executing "sh mksdcard.sh /dev/mmcblk1"&lt;BR /&gt;1+0 records in&lt;BR /&gt;1+0 records out&lt;BR /&gt;1024 bytes (1.0 kB, 1.0 KiB) copied, 0.095254 s, 10.8 kB/s&lt;BR /&gt;Checking that no-one is using this disk right now ... OK&lt;/P&gt;&lt;P&gt;Disk /dev/mmcblk1: 3.6 GiB, 38252 mmcblk1: p1 p2&lt;BR /&gt;05248 bytes, 7471104 sectors&lt;BR /&gt;Units: sectors of 1 * 512 = 512 bytes&lt;BR /&gt;Sector size (logical/physical): 512 bytes / 512 bytes&lt;BR /&gt;I/O size (minimum/optimal): 512 bytes / 512 bytes&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt;&amp;gt; Created a new DOS disklabel with disk identifier 0x459ca873.&lt;BR /&gt;Created a new partition 1 of type 'W95 FAT32 (LBA)' and of size 500 MiB.&lt;BR /&gt;/dev/mmcblk1p2: Created a new partition 2 of type 'Linux' and of size 3 GiB.&lt;BR /&gt;/dev/mmcblk1p3:&lt;BR /&gt;New situation:&lt;/P&gt;&lt;P&gt;Device Boot Start End Sectors Size Id Type&lt;BR /&gt;/dev/mmcblk1p1 20480 1044479 1024000 500M c W95 FAT32 (LBA)&lt;BR /&gt;/dev/mmcblk1p2 1228800 7471103 6242304 3G 83 Linux&lt;/P&gt;&lt;P&gt;The partition table has been altered.&lt;BR /&gt;Calling ioctl() to re-read partition table.&lt;BR /&gt;Syncing disks.&lt;BR /&gt;UTP: sending Success to kernel for command $ sh mksdcard.sh /dev/mmcblk1.&lt;BR /&gt;utp_poll: pass returned.&lt;BR /&gt;UTP: received command '$ dd if=/dev/zero of=/dev/mmcblk1 bs=1k seek=768 conv=fsync count=8'&lt;BR /&gt;UTP: executing "dd if=/dev/zero of=/dev/mmcblk1 bs=1k seek=768 conv=fsync count=8"&lt;BR /&gt;8+0 records in&lt;BR /&gt;8+0 records out&lt;BR /&gt;8192 bytes (8.2 kB, 8.0 KiB) copied, 0.0142733 s, 574 kB/s&lt;BR /&gt;UTP: sending Success to kernel for command $ dd if=/dev/zero of=/dev/mmcblk1 bs=1k seek=768 conv=fsync count=8.&lt;BR /&gt;utp_poll: pass returned.&lt;BR /&gt;UTP: received command '$ echo 0 &amp;gt; /sys/block/mmcblk1boot0/force_ro'&lt;BR /&gt;UTP: executing "echo 0 &amp;gt; /sys/block/mmcblk1boot0/force_ro"&lt;BR /&gt;UTP: sending Success to kernel for command $ echo 0 &amp;gt; /sys/block/mmcblk1boot0/force_ro.&lt;BR /&gt;utp_poll: pass returned.&lt;BR /&gt;UTP: received command 'send'&lt;BR /&gt;UTP: sending Success to kernel for command send.&lt;BR /&gt;UTP: received command '$ dd if=$FILE of=/dev/mmcblk1boot0 bs=512 seek=2'&lt;BR /&gt;UTP: executing "dd if=$FILE of=/dev/mmcblk1boot0 bs=512 seek=2"&lt;BR /&gt;822+0 records in&lt;BR /&gt;822+0 records out&lt;BR /&gt;420864 bytes (421 kB, 411 KiB) copied, 0.208972 s, 2.0 MB/s&lt;BR /&gt;UTP: sending Success to kernel for command $ dd if=$FILE of=/dev/mmcblk1boot0 bs=512 seek=2.&lt;BR /&gt;utp_poll: pass returned.&lt;BR /&gt;UTP: received command '$ echo 1 &amp;gt; /sys/block/mmcblk1boot0/force_ro'&lt;BR /&gt;UTP: executing "echo 1 &amp;gt; /sys/block/mmcblk1boot0/force_ro"&lt;BR /&gt;UTP: sending Success to kernel for command $ echo 1 &amp;gt; /sys/block/mmcblk1boot0/force_ro.&lt;BR /&gt;utp_poll: pass returned.&lt;BR /&gt;UTP: received command '$ mmc bootpart enable 1 1 /dev/mmcblk1'&lt;BR /&gt;UTP: executing "mmc bootpart enable 1 1 /dev/mmcblk1"&lt;BR /&gt;UTP: sending Success to kernel for command $ mmc bootpart enable 1 1 /dev/mmcblk1.&lt;BR /&gt;utp_poll: pass returned.&lt;BR /&gt;UTP: received command '$ while [ ! -e /dev/mmcblk1p1 ]; do sleep 1; echo "waiting..."; done '&lt;BR /&gt;UTP: executing "while [ ! -e /dev/mmcblk1p1 ]; do sleep 1; echo "waiting..."; done "&lt;BR /&gt;UTP: sending Success to kernel for command $ while [ ! -e /dev/mmcblk1p1 ]; do sleep 1; echo "waiting..."; done .&lt;BR /&gt;utp_poll: pass returned.&lt;BR /&gt;UTP: received command '$ mkfs.vfat /dev/mmcblk1p1'&lt;BR /&gt;UTP: executing "mkfs.vfat /dev/mmcblk1p1"&lt;BR /&gt;mkfs.fat 3.0.28 (2015-05-16)&lt;BR /&gt;UTP: sending Success to kernel for command $ mkfs.vfat /dev/mmcblk1p1.&lt;BR /&gt;utp_poll: pass returned.&lt;BR /&gt;UTP: received command '$ mkdir -p /mnt/mmcblk1p1'&lt;BR /&gt;UTP: executing "mkdir -p /mnt/mmcblk1p1"&lt;BR /&gt;UTP: sending Success to kernel for command $ mkdir -p /mnt/mmcblk1p1.&lt;BR /&gt;utp_poll: pass returned.&lt;BR /&gt;UTP: received command '$ mount -t vfat /dev/mmcblk1p1 /mnt/mmcblk1p1'&lt;BR /&gt;UTP: executing "mount -t vfat /dev/mmcblk1p1 /mnt/mmcblk1p1"&lt;BR /&gt;UTP: sending Success to kernel for command $ mount -t vfat /dev/mmcblk1p1 /mnt/mmcblk1p1.&lt;BR /&gt;utp_poll: pass returned.&lt;BR /&gt;UTP: received command 'send'&lt;BR /&gt;UTP: sending Success to kernel for command send.&lt;BR /&gt;UTP: received command '$ cp $FILE /mnt/mmcblk1p1/zImage'&lt;BR /&gt;UTP: executing "cp $FILE /mnt/mmcblk1p1/zImage"&lt;BR /&gt;UTP: sending Success to kernel for command $ cp $FILE /mnt/mmcblk1p1/zImage.&lt;BR /&gt;utp_poll: pass returned.&lt;BR /&gt;UTP: received command 'send'&lt;BR /&gt;UTP: sending Success to kernel for command send.&lt;BR /&gt;UTP: received command '$ cp $FILE /mnt/mmcblk1p1/imx6ull-14x14-evk.dtb'&lt;BR /&gt;UTP: executing "cp $FILE /mnt/mmcblk1p1/imx6ull-14x14-evk.dtb"&lt;BR /&gt;UTP: sending Success to kernel for command $ cp $FILE /mnt/mmcblk1p1/imx6ull-14x14-evk.dtb.&lt;BR /&gt;utp_poll: pass returned.&lt;BR /&gt;UTP: received command '$ mkfs.ext3 -F -E nodiscard /dev/mmcblk1p2'&lt;BR /&gt;UTP: executing "mkfs.ext3 -F -E nodiscard /dev/mmcblk1p2"&lt;BR /&gt;mke2fs 1.43-WIP (18-May-2015)&lt;BR /&gt;/dev/mmcblk1p2 contains a ext3 file system&lt;BR /&gt; last mounted on /mnt/mmcblk1p2 on Thu Jan 1 00:00:17 1970&lt;BR /&gt;Creating filesystem with 780288 4k blocks and 195072 inodes&lt;BR /&gt;Filesystem UUID: 93b59973-2012-44a5-b405-8f3c5ee5a11f&lt;BR /&gt;Superblock backups stored on blocks:&lt;BR /&gt; 32768, 98304, 163840, 229376, 294912&lt;/P&gt;&lt;P&gt;Allocating group tables: done&lt;BR /&gt;Writing inode tables: done&lt;BR /&gt;Creating journal (16384 blocks): done&lt;BR /&gt;Writing superblocks and filesystem accounting information: done&lt;/P&gt;&lt;P&gt;UTP: sending Success to kernel for command $ mkfs.ext3 -F -E nodiscard /dev/mmcblk1p2.&lt;BR /&gt;utp_poll: pass returned.&lt;BR /&gt;UTP: received command '$ mkdir -p /mnt/mmcblk1p2'&lt;BR /&gt;UTP: executing "mkdir -p /mnt/mmcblk1p2"&lt;BR /&gt;UTP: sending Success to kernel for command $ mkdir -p /mnt/mmcblk1p2.&lt;BR /&gt;utp_poll: pass returned.&lt;BR /&gt;UTP: received command '$ mount -t ext3 /dev/mmcblk1p2 /mnt/mmcblk1p2'&lt;BR /&gt;UTP: executing "mount -t ext3 /dev/mmcblk1p2 /mnt/mmcblk1p2"&lt;BR /&gt;EXT4-fs (mmcblk1p2): mounting ext3 file system using the ext4 subsystem&lt;BR /&gt;EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null)&lt;BR /&gt;UTP: sending Success to kernel for command $ mount -t ext3 /dev/mmcblk1p2 /mnt/mmcblk1p2.&lt;BR /&gt;utp_poll: pass returned.&lt;BR /&gt;UTP: received command 'pipe tar -jxv -C /mnt/mmcblk1p2'&lt;BR /&gt;pid is 152, UTP: executing "tar -jxv -C /mnt/mmcblk1p2"&lt;BR /&gt;UTP: sending Success to kernel for command pipe tar -jxv -C /mnt/mmcblk1p2.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Apr 2018 09:54:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/not-able-to-boot-custom-imx6ull-board-using-eMMC/m-p/774527#M120235</guid>
      <dc:creator>pankajjoshi</dc:creator>
      <dc:date>2018-04-30T09:54:15Z</dc:date>
    </item>
  </channel>
</rss>