<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 iMX6_SOLOX_3V3</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-SOLOX-3V3/m-p/774478#M120221</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="margin: 0cm 0cm 0pt;"&gt;My questions are concerning of powering the microprocessor &amp;nbsp;&amp;nbsp;iMX6 SOLOX from a 3.3 volts input power source. For power sequencing I use the preprogrammed PMIC chip MMPF0200F6AEP. But I would like not to use the SW2 output of the PMIC as a source of 3.3 volts for my PCB. I plan to use the input voltage and a load switch instead of use the SW2 output of the PMIC. To control of the load switch I want to use the output voltage of the SW3A output of the PMIC. Is it correct using of PMIC? If so, may I leave unconnected the pins SW2LX, SW2IN, SW2FB of the PMIC chip MMPF0200F6AEP? Or I must connect them as in the MCIMX6SX SDB board &amp;nbsp;(SCH-27962)? Is it mandatory to have 3.3 volts on the SW2 output for correct operation the chip MMPF0200F6AEP?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 26 Feb 2018 11:11:43 GMT</pubDate>
    <dc:creator>victorafanasiev</dc:creator>
    <dc:date>2018-02-26T11:11:43Z</dc:date>
    <item>
      <title>iMX6_SOLOX_3V3</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-SOLOX-3V3/m-p/774478#M120221</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="margin: 0cm 0cm 0pt;"&gt;My questions are concerning of powering the microprocessor &amp;nbsp;&amp;nbsp;iMX6 SOLOX from a 3.3 volts input power source. For power sequencing I use the preprogrammed PMIC chip MMPF0200F6AEP. But I would like not to use the SW2 output of the PMIC as a source of 3.3 volts for my PCB. I plan to use the input voltage and a load switch instead of use the SW2 output of the PMIC. To control of the load switch I want to use the output voltage of the SW3A output of the PMIC. Is it correct using of PMIC? If so, may I leave unconnected the pins SW2LX, SW2IN, SW2FB of the PMIC chip MMPF0200F6AEP? Or I must connect them as in the MCIMX6SX SDB board &amp;nbsp;(SCH-27962)? Is it mandatory to have 3.3 volts on the SW2 output for correct operation the chip MMPF0200F6AEP?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Feb 2018 11:11:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-SOLOX-3V3/m-p/774478#M120221</guid>
      <dc:creator>victorafanasiev</dc:creator>
      <dc:date>2018-02-26T11:11:43Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6_SOLOX_3V3</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-SOLOX-3V3/m-p/774479#M120222</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Viktor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for unused pins connection one can look at&lt;/P&gt;&lt;P&gt;Table 1. MMPF0200 pin connection guidelines AN4751 Schematic guidelines for the MMPF0200&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN4751.pdf" title="https://www.nxp.com/docs/en/application-note/AN4751.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN4751.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;yes one can use external (not pmic) power for processor, provided that&lt;/P&gt;&lt;P&gt;power-up sequence is followed (it is described in i.MX6SX Datasheet).&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fdata-sheet%2FIMX6SXCEC.pdf" rel="nofollow" target="_blank"&gt;https://www.nxp.com/docs/en/data-sheet/IMX6SXCEC.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Feb 2018 00:59:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-SOLOX-3V3/m-p/774479#M120222</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-02-27T00:59:30Z</dc:date>
    </item>
  </channel>
</rss>