<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックMX7/PF3000 ON/OFF Button and 'Power Good'</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MX7-PF3000-ON-OFF-Button-and-Power-Good/m-p/773283#M120060</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;while developing an MX7 module for a given mainboard&amp;nbsp;I ran into a few questions regarding MX7 run modes.&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;The mainboard provides an ON/OFF Button.&lt;/LI&gt;&lt;LI&gt;The mainboard&amp;nbsp;provides 5V as the only power input&lt;OL&gt;&lt;LI&gt;Power for an RTC may or may not be provided, depending on mainboard version&lt;/LI&gt;&lt;/OL&gt;&lt;/LI&gt;&lt;LI&gt;The mainboard signals "power good" on a pin&amp;nbsp;&lt;OL&gt;&lt;LI&gt;The MX7 Module may not boot if this pin is held low&lt;/LI&gt;&lt;/OL&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I understood correctly, the SNVS power domain will trigger the MX7 to go from OFF to RUN mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SNVS is powered from the LICELL input. What happens if LICELL is not used?&lt;/P&gt;&lt;P&gt;Is there a possibility to stop the MX7 from booting if power is applied but the ONOFF button is not pressed?&lt;/P&gt;&lt;P&gt;The PF3000 has no enable pin. Except for cutting power with e.g. an additional FET: is there a way to disable/enable the PMIC with a digital signal?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 06 Apr 2018 15:26:18 GMT</pubDate>
    <dc:creator>demoniacmilk</dc:creator>
    <dc:date>2018-04-06T15:26:18Z</dc:date>
    <item>
      <title>MX7/PF3000 ON/OFF Button and 'Power Good'</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX7-PF3000-ON-OFF-Button-and-Power-Good/m-p/773283#M120060</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;while developing an MX7 module for a given mainboard&amp;nbsp;I ran into a few questions regarding MX7 run modes.&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;The mainboard provides an ON/OFF Button.&lt;/LI&gt;&lt;LI&gt;The mainboard&amp;nbsp;provides 5V as the only power input&lt;OL&gt;&lt;LI&gt;Power for an RTC may or may not be provided, depending on mainboard version&lt;/LI&gt;&lt;/OL&gt;&lt;/LI&gt;&lt;LI&gt;The mainboard signals "power good" on a pin&amp;nbsp;&lt;OL&gt;&lt;LI&gt;The MX7 Module may not boot if this pin is held low&lt;/LI&gt;&lt;/OL&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I understood correctly, the SNVS power domain will trigger the MX7 to go from OFF to RUN mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SNVS is powered from the LICELL input. What happens if LICELL is not used?&lt;/P&gt;&lt;P&gt;Is there a possibility to stop the MX7 from booting if power is applied but the ONOFF button is not pressed?&lt;/P&gt;&lt;P&gt;The PF3000 has no enable pin. Except for cutting power with e.g. an additional FET: is there a way to disable/enable the PMIC with a digital signal?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Apr 2018 15:26:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX7-PF3000-ON-OFF-Button-and-Power-Good/m-p/773283#M120060</guid>
      <dc:creator>demoniacmilk</dc:creator>
      <dc:date>2018-04-06T15:26:18Z</dc:date>
    </item>
    <item>
      <title>Re: MX7/PF3000 ON/OFF Button and 'Power Good'</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX7-PF3000-ON-OFF-Button-and-Power-Good/m-p/773284#M120061</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;For PF3000 please note that VSNVS powers the low-power, SNVS/RTC domain on the processor.&lt;/P&gt;&lt;P&gt;It derives its power from either VIN, or coin cell, and cannot be disabled.&lt;/P&gt;&lt;P&gt;PF3000 has a PWRON pin has function of power ON/OFF input from processor.&lt;/P&gt;&lt;P&gt;For I.MX board please check PF3000 VSNVS connection way.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Apr 2018 07:54:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX7-PF3000-ON-OFF-Button-and-Power-Good/m-p/773284#M120061</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2018-04-11T07:54:00Z</dc:date>
    </item>
  </channel>
</rss>