<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: UART Debug port number in IMX7 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/UART-Debug-port-number-in-IMX7/m-p/772499#M119933</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;On iMX7DSABRESD board J11 connector is used for Debug UART (via USB).&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;According to board schematic: Debug UART1 is intended for Cortex-A7;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Debug UART2 for Cortex-M4. &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp; NXP BSP(s) uses such approach, but customers can use any available UART ports&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;(and pins) for their applications, assuming BSP modification, if needed.&amp;nbsp; &lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 07 Dec 2017 09:15:59 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2017-12-07T09:15:59Z</dc:date>
    <item>
      <title>UART Debug port number in IMX7</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UART-Debug-port-number-in-IMX7/m-p/772497#M119931</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kindly help me, which UART port is used for debugging in IMX7 (Part number # MCIMX7D7DVK10SC)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Logesh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Dec 2017 08:26:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UART-Debug-port-number-in-IMX7/m-p/772497#M119931</guid>
      <dc:creator>logeshs</dc:creator>
      <dc:date>2017-12-07T08:26:11Z</dc:date>
    </item>
    <item>
      <title>Re: UART Debug port number in IMX7</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UART-Debug-port-number-in-IMX7/m-p/772498#M119932</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Also Kindly suggest shall we use any of below UART ports for debugging,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. UART1 (Pin# D16 &amp;amp; D7)&lt;/P&gt;&lt;P&gt;2. UART2 (Pin# G28 &amp;amp; D20)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If we are not able to use the above ports for debugging kindly request you to provide correct the UART port ID with pin numbers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards&lt;/P&gt;&lt;P&gt;Logesh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Dec 2017 08:43:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UART-Debug-port-number-in-IMX7/m-p/772498#M119932</guid>
      <dc:creator>logeshs</dc:creator>
      <dc:date>2017-12-07T08:43:15Z</dc:date>
    </item>
    <item>
      <title>Re: UART Debug port number in IMX7</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UART-Debug-port-number-in-IMX7/m-p/772499#M119933</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;On iMX7DSABRESD board J11 connector is used for Debug UART (via USB).&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;According to board schematic: Debug UART1 is intended for Cortex-A7;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Debug UART2 for Cortex-M4. &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp; NXP BSP(s) uses such approach, but customers can use any available UART ports&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;(and pins) for their applications, assuming BSP modification, if needed.&amp;nbsp; &lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Dec 2017 09:15:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UART-Debug-port-number-in-IMX7/m-p/772499#M119933</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2017-12-07T09:15:59Z</dc:date>
    </item>
  </channel>
</rss>