<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to enable apt-get  on IMX? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-enable-apt-get-on-IMX/m-p/771904#M119839</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm a beginner in Yocto Project and bought a IMX8 EVB. I successfully&amp;nbsp;built&amp;nbsp;"core-image-sato" image with the following configuration to enable apt-get command.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;IMAGE_FEATURES += "&amp;nbsp; package-management ssh-server-openssh "&lt;/P&gt;&lt;P&gt;IMAGE_INSTALL_append +=" apt"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But&amp;nbsp;when tyring to "apt-get install vim" on the EVB board, the following errors are occurred.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="mailto:root@cl-som-imx8"&gt;root@cl-som-imx8&lt;/A&gt;:~# apt-get install vim&lt;BR /&gt;Reading package lists... Error!&lt;BR /&gt;E: flAbsPath on /var/lib/dpkg/status failed - realpath (2: No such file or directory)&lt;BR /&gt;E: Could not open file&amp;nbsp; - open (2: No such file or directory)&lt;BR /&gt;E: Problem opening&lt;BR /&gt;E: The package lists or status file could not be parsed or opened.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can the errors be fixed?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 26 Feb 2018 01:12:50 GMT</pubDate>
    <dc:creator>byunggukchoi</dc:creator>
    <dc:date>2018-02-26T01:12:50Z</dc:date>
    <item>
      <title>How to enable apt-get  on IMX?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-enable-apt-get-on-IMX/m-p/771904#M119839</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm a beginner in Yocto Project and bought a IMX8 EVB. I successfully&amp;nbsp;built&amp;nbsp;"core-image-sato" image with the following configuration to enable apt-get command.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;IMAGE_FEATURES += "&amp;nbsp; package-management ssh-server-openssh "&lt;/P&gt;&lt;P&gt;IMAGE_INSTALL_append +=" apt"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But&amp;nbsp;when tyring to "apt-get install vim" on the EVB board, the following errors are occurred.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="mailto:root@cl-som-imx8"&gt;root@cl-som-imx8&lt;/A&gt;:~# apt-get install vim&lt;BR /&gt;Reading package lists... Error!&lt;BR /&gt;E: flAbsPath on /var/lib/dpkg/status failed - realpath (2: No such file or directory)&lt;BR /&gt;E: Could not open file&amp;nbsp; - open (2: No such file or directory)&lt;BR /&gt;E: Problem opening&lt;BR /&gt;E: The package lists or status file could not be parsed or opened.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can the errors be fixed?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Feb 2018 01:12:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-enable-apt-get-on-IMX/m-p/771904#M119839</guid>
      <dc:creator>byunggukchoi</dc:creator>
      <dc:date>2018-02-26T01:12:50Z</dc:date>
    </item>
    <item>
      <title>Re: How to enable apt-get  on IMX?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-enable-apt-get-on-IMX/m-p/771905#M119840</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;it seems apt-get command is for linux, did you build linux OS on the board? try to confirm that you need to install the vim to the board or ubuntu (build environment)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Mar 2018 08:21:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-enable-apt-get-on-IMX/m-p/771905#M119840</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2018-03-02T08:21:49Z</dc:date>
    </item>
    <item>
      <title>Re: How to enable apt-get  on IMX?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-enable-apt-get-on-IMX/m-p/771906#M119841</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Having apt-get available as a program is one thing, having a web server with a repository is another.&lt;/P&gt;&lt;P&gt;Maybe these documents answer some of your questions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-328199"&gt;Yocto Project Package Management - smart&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://imxdev.gitlab.io/tutorial/How_to_apt-get_to_the_Yocto_Project_image/" title="https://imxdev.gitlab.io/tutorial/How_to_apt-get_to_the_Yocto_Project_image/"&gt;How to install apt-get to the Yocto Project image - i.MXDev Blog&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Mar 2018 14:25:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-enable-apt-get-on-IMX/m-p/771906#M119841</guid>
      <dc:creator>bernhardfink</dc:creator>
      <dc:date>2018-03-02T14:25:17Z</dc:date>
    </item>
  </channel>
</rss>