<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: VDD_SNVS_IN voltage range</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/VDD-SNVS-IN-voltage-range/m-p/771868#M119833</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Your reply confirms i&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;MX6DualPlus/6QuadPlus&amp;nbsp;&lt;/SPAN&gt;range for both&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;VDD_SNVS_IN and VDD_HIGH_IN is:&amp;nbsp; 2.8V - 3.6V&lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;As listed in datasheet.&lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;1. Can you therefore clarify why I cannot connect both to a 3.3V supply with tolerance of +5% (Maximum of 3.465V)&lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;2. Your requirements of VDD_SNVS_IN being supplied prior to VDD_HIGH_IN contradicts datasheet recommendation below. Please clarify.&lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/646i1C558DC0244870CC/image-size/large?v=v2&amp;amp;px=999" title="Capture.PNG" alt="Capture.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Thanks&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 May 2018 09:17:28 GMT</pubDate>
    <dc:creator>jhones</dc:creator>
    <dc:date>2018-05-03T09:17:28Z</dc:date>
    <item>
      <title>VDD_SNVS_IN voltage range</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/VDD-SNVS-IN-voltage-range/m-p/771866#M119831</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;I have seen a contradiction in the i.MX 6DualPlus/6QuadPlus datasheet regarding VDD_SNVS_IN voltage range:&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Table 6. Operating Ranges: 2.8V - 3.6V&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Table 4. Absolute Maximum Ratings: -0.3V - 3.4V&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Can you confirm that 3.6V is the absolute maximum of VDD_SNVS_IN for the i.MX 6DualPlus/6QuadPlus?&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;It this is correct, does this range (-0.3 - 3.6V) apply for all iMX6 family i.MX6Quad/Dual/DualLight/Solo?&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;I would like to short VDD_HIGH_IN VDD_SNVS_IN and connect both to a 3.3V supply.&lt;BR /&gt;Supply has a %5 tolerance which may end up at 3.465V. VDD_HIGH_IN can withstand this question is can VDD_SNVS_IN operate at 3.465V?&lt;BR /&gt;(Adding a &lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;schottky&lt;/SPAN&gt; diode between VDD_HIGH_IN to VDD_SNVS_IN for lowering the voltage of VDD_SNVS_IN does not seem to be a solution since drop is negligible in the VSNVS max current of 275uA)&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Thank you for your support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Apr 2018 07:03:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/VDD-SNVS-IN-voltage-range/m-p/771866#M119831</guid>
      <dc:creator>jhones</dc:creator>
      <dc:date>2018-04-26T07:03:39Z</dc:date>
    </item>
    <item>
      <title>Re: VDD_SNVS_IN voltage range</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/VDD-SNVS-IN-voltage-range/m-p/771867#M119832</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Aviad,&lt;BR /&gt;The 3.6v is the maximum of VDD_SNVS_IN for the i.MX6DualPlus/6QuadPlus. But in generally use the VDD_SNVS_IN is given 3.0 V power. The i.MX6Quad/Dual/DualLight/Solo are different from i.MX6DualPlus/6QuadPlus, the voltage rangs you can see details in the datasheet.&lt;BR /&gt;You action is not right "I would like to short VDD_HIGH_IN VDD_SNVS_IN and connect both to a 3.3V supply"&lt;BR /&gt;For that you can not power up VDD_HIGH_IN and VDD_SNVS_IN. T at the same time. The VDD_SNVS_IN need firstly given 3.0v power. The VDD_HIGH_IN can be power up later but not too late.&lt;BR /&gt;And here the 3.465V is not allowed, you can try to adjust it under 3.3V.&lt;BR /&gt;Hope the above reply can do help for you.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Rita&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 May 2018 07:52:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/VDD-SNVS-IN-voltage-range/m-p/771867#M119832</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2018-05-03T07:52:59Z</dc:date>
    </item>
    <item>
      <title>Re: VDD_SNVS_IN voltage range</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/VDD-SNVS-IN-voltage-range/m-p/771868#M119833</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Your reply confirms i&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;MX6DualPlus/6QuadPlus&amp;nbsp;&lt;/SPAN&gt;range for both&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;VDD_SNVS_IN and VDD_HIGH_IN is:&amp;nbsp; 2.8V - 3.6V&lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;As listed in datasheet.&lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;1. Can you therefore clarify why I cannot connect both to a 3.3V supply with tolerance of +5% (Maximum of 3.465V)&lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;2. Your requirements of VDD_SNVS_IN being supplied prior to VDD_HIGH_IN contradicts datasheet recommendation below. Please clarify.&lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/646i1C558DC0244870CC/image-size/large?v=v2&amp;amp;px=999" title="Capture.PNG" alt="Capture.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Thanks&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 May 2018 09:17:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/VDD-SNVS-IN-voltage-range/m-p/771868#M119833</guid>
      <dc:creator>jhones</dc:creator>
      <dc:date>2018-05-03T09:17:28Z</dc:date>
    </item>
  </channel>
</rss>