<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Double H264 Encoding on sabrelite in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Double-H264-Encoding-on-sabrelite/m-p/771650#M119805</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I use a sabrelite board (BD-SL-I.MX6) to develop an encoder and an H264 IP/UDP streamer.&lt;/P&gt;&lt;P&gt;I can capture video stream from the J16 connector (Nit6X_5MP_MIPI camera).&lt;BR /&gt;This configuration work well.&lt;/P&gt;&lt;P&gt;Now, I whish acquire and stream simultaneously 2 H264 video stream.&lt;/P&gt;&lt;P&gt;The goal is :&lt;/P&gt;&lt;P&gt;- capture at same time 2 video stream from J16 (Nit6X_5MP_MIPI camera) and from J5 (Nit6X_5MP) in 1280x720p25&lt;/P&gt;&lt;P&gt;- encode and generate 2 H264 video stream&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;In the documentaion, it's look like that is possible, but in fact, I don't found post which talk about this type of configurtaion.&lt;/P&gt;&lt;P&gt;Nobody have try to do this ?&lt;BR /&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 30 Jan 2018 11:26:34 GMT</pubDate>
    <dc:creator>mercadiernicola</dc:creator>
    <dc:date>2018-01-30T11:26:34Z</dc:date>
    <item>
      <title>Double H264 Encoding on sabrelite</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Double-H264-Encoding-on-sabrelite/m-p/771650#M119805</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I use a sabrelite board (BD-SL-I.MX6) to develop an encoder and an H264 IP/UDP streamer.&lt;/P&gt;&lt;P&gt;I can capture video stream from the J16 connector (Nit6X_5MP_MIPI camera).&lt;BR /&gt;This configuration work well.&lt;/P&gt;&lt;P&gt;Now, I whish acquire and stream simultaneously 2 H264 video stream.&lt;/P&gt;&lt;P&gt;The goal is :&lt;/P&gt;&lt;P&gt;- capture at same time 2 video stream from J16 (Nit6X_5MP_MIPI camera) and from J5 (Nit6X_5MP) in 1280x720p25&lt;/P&gt;&lt;P&gt;- encode and generate 2 H264 video stream&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;In the documentaion, it's look like that is possible, but in fact, I don't found post which talk about this type of configurtaion.&lt;/P&gt;&lt;P&gt;Nobody have try to do this ?&lt;BR /&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jan 2018 11:26:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Double-H264-Encoding-on-sabrelite/m-p/771650#M119805</guid>
      <dc:creator>mercadiernicola</dc:creator>
      <dc:date>2018-01-30T11:26:34Z</dc:date>
    </item>
    <item>
      <title>Re: Double H264 Encoding on sabrelite</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Double-H264-Encoding-on-sabrelite/m-p/771651#M119806</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi mercadiernicolas&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for vpu examples of multiple instances encoding one can look&lt;/P&gt;&lt;P&gt;at unit tests: imx-test (../test/mxc_vpu_test)&lt;BR /&gt;&lt;A href="http://www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz"&gt;www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jan 2018 23:04:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Double-H264-Encoding-on-sabrelite/m-p/771651#M119806</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-01-30T23:04:30Z</dc:date>
    </item>
  </channel>
</rss>