<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックProblems using mfgtool</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Problems-using-mfgtool/m-p/771474#M119783</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;I am using mfg tool together with imx6ull evk.&lt;/P&gt;&lt;P&gt;I have connected my computer to the USB OTG of the imx6ull evk.&lt;/P&gt;&lt;P&gt;When starting the scirpt "mfgtool2-yocto-mx-evk-sdcard-sd2" the tool starts and the device is shown as ."HID-compliant device"&lt;/P&gt;&lt;P&gt;When klicking start, the following steps are shown and the progress is shown on the upper bar, the lower bar is never showing any progress:&lt;/P&gt;&lt;P&gt;1. loading u-boot&lt;/P&gt;&lt;P&gt;2. loading kernel&lt;/P&gt;&lt;P&gt;3. loading initramfs&lt;/P&gt;&lt;P&gt;4. jumping to os&lt;/P&gt;&lt;P&gt;5. after jumping os, the first step is executed again and the compete progress starts from the beginning.&lt;/P&gt;&lt;P&gt;Why does this happen?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There should be also a debug output of the mfgTool.&lt;/P&gt;&lt;P&gt;The driver does not offer any additional serial interface.&lt;/P&gt;&lt;P&gt;The other USB interface (/ttyUSB0) does not show any debug output&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have here 2 computer.&lt;/P&gt;&lt;P&gt;1. computer Windows 7&lt;/P&gt;&lt;P&gt;On this computer I am running the mfgTool connected to J1102&lt;/P&gt;&lt;P&gt;2. Computer ubuntu16.04&lt;/P&gt;&lt;P&gt;On this computer I am running the log from ttyUSB0 (J1901)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My questions:&lt;/P&gt;&lt;P&gt;1. Why does the mfgTool run endless?&lt;/P&gt;&lt;P&gt;2. How can I see the debug output of the mfgTool&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Apr 2018 11:25:32 GMT</pubDate>
    <dc:creator>cb1</dc:creator>
    <dc:date>2018-04-26T11:25:32Z</dc:date>
    <item>
      <title>Problems using mfgtool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-using-mfgtool/m-p/771474#M119783</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;I am using mfg tool together with imx6ull evk.&lt;/P&gt;&lt;P&gt;I have connected my computer to the USB OTG of the imx6ull evk.&lt;/P&gt;&lt;P&gt;When starting the scirpt "mfgtool2-yocto-mx-evk-sdcard-sd2" the tool starts and the device is shown as ."HID-compliant device"&lt;/P&gt;&lt;P&gt;When klicking start, the following steps are shown and the progress is shown on the upper bar, the lower bar is never showing any progress:&lt;/P&gt;&lt;P&gt;1. loading u-boot&lt;/P&gt;&lt;P&gt;2. loading kernel&lt;/P&gt;&lt;P&gt;3. loading initramfs&lt;/P&gt;&lt;P&gt;4. jumping to os&lt;/P&gt;&lt;P&gt;5. after jumping os, the first step is executed again and the compete progress starts from the beginning.&lt;/P&gt;&lt;P&gt;Why does this happen?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There should be also a debug output of the mfgTool.&lt;/P&gt;&lt;P&gt;The driver does not offer any additional serial interface.&lt;/P&gt;&lt;P&gt;The other USB interface (/ttyUSB0) does not show any debug output&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have here 2 computer.&lt;/P&gt;&lt;P&gt;1. computer Windows 7&lt;/P&gt;&lt;P&gt;On this computer I am running the mfgTool connected to J1102&lt;/P&gt;&lt;P&gt;2. Computer ubuntu16.04&lt;/P&gt;&lt;P&gt;On this computer I am running the log from ttyUSB0 (J1901)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My questions:&lt;/P&gt;&lt;P&gt;1. Why does the mfgTool run endless?&lt;/P&gt;&lt;P&gt;2. How can I see the debug output of the mfgTool&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Apr 2018 11:25:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-using-mfgtool/m-p/771474#M119783</guid>
      <dc:creator>cb1</dc:creator>
      <dc:date>2018-04-26T11:25:32Z</dc:date>
    </item>
    <item>
      <title>Re: Problems using mfgtool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-using-mfgtool/m-p/771475#M119784</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can see the debug output of the mfgTool with the UART interface of the board, you only need to connect it to a serial terminal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Furthermore, when you&amp;nbsp;can get the serial output, can you please share with us the log file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Apr 2018 19:23:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-using-mfgtool/m-p/771475#M119784</guid>
      <dc:creator>diegoadrian</dc:creator>
      <dc:date>2018-04-30T19:23:19Z</dc:date>
    </item>
  </channel>
</rss>