<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックHarash driving detection</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Harash-driving-detection/m-p/771449#M119781</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How can I detect Huge Acceleration/Brake with MMA8653 accelerometer?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Apr 2018 10:50:31 GMT</pubDate>
    <dc:creator>anishkumar</dc:creator>
    <dc:date>2018-04-26T10:50:31Z</dc:date>
    <item>
      <title>Harash driving detection</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Harash-driving-detection/m-p/771449#M119781</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How can I detect Huge Acceleration/Brake with MMA8653 accelerometer?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Apr 2018 10:50:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Harash-driving-detection/m-p/771449#M119781</guid>
      <dc:creator>anishkumar</dc:creator>
      <dc:date>2018-04-26T10:50:31Z</dc:date>
    </item>
    <item>
      <title>Re: Harash driving detection</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Harash-driving-detection/m-p/771450#M119782</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Anish Kumar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could identify the acceleration changes using the data registers of the device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note that the MMA8653 device has embedded functionalities which might help detecting the events that you mentioned. Freefall is detected when the acceleration magnitude is less than the configured threshold.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A huge acceleration/brake will generate a ‘spike’ on the data register that can be identified as below:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/13401iA317895F1CAEAE80/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can use the example project bellow as a reference for your project:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-101192"&gt;MMA8652FC - Bare metal example project&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope this information helps.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;David &amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Apr 2018 16:29:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Harash-driving-detection/m-p/771450#M119782</guid>
      <dc:creator>david_diaz</dc:creator>
      <dc:date>2018-04-27T16:29:30Z</dc:date>
    </item>
  </channel>
</rss>