<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Weston Wayland g2d_buf_from_virt_addr undefined in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Weston-Wayland-g2d-buf-from-virt-addr-undefined/m-p/770841#M119700</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Donahoe,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You are using a different kernel of the BSP 4.1.44, try to use the BSP and you will see the g2d.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 25 May 2018 14:14:30 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2018-05-25T14:14:30Z</dc:date>
    <item>
      <title>Weston Wayland g2d_buf_from_virt_addr undefined</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Weston-Wayland-g2d-buf-from-virt-addr-undefined/m-p/770840#M119699</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Weston Wayland imx6 Yocto rocko. &amp;nbsp;Trying to run with&amp;nbsp;&lt;SPAN&gt;--use-g2d=1 and get the following. &amp;nbsp;I was looking in&amp;nbsp;imx-gpu-viv-5.0.11.p8.6 to see if one of the libraries contains&amp;nbsp;&lt;SPAN&gt;g2d_buf_from_virt_addr, but I did not see it. &amp;nbsp;What am I missing? &amp;nbsp;Thanks&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;[01:31:12.155] weston 2.0.0&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwayland.freedesktop.org" rel="nofollow" target="_blank"&gt;http://wayland.freedesktop.org&lt;/A&gt;&lt;BR /&gt;&lt;SPAN&gt;Bug reports to: &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fbugs.freedesktop.org%2Fenter_bug.cgi%3Fproduct%3DWayland%26component%3Dweston%26version%3D2.0.0" rel="nofollow" target="_blank"&gt;https://bugs.freedesktop.org/enter_bug.cgi?product=Wayland&amp;amp;component=weston&amp;amp;version=2.0.0&lt;/A&gt;&lt;BR /&gt;Build: 2.0.0-22-g506dc2d-dirty compositor-drm: Ignore non-KMS devices (2017-10-13 17:42:08 -0500)&lt;BR /&gt;[01:31:12.155] Command line: weston --log=/dev/console --use-g2d=1&lt;BR /&gt;[01:31:12.155] OS: Linux, 4.1.44+g0d698de4, #13 SMP PREEMPT Tue May 15 14:33:37 CDT 2018, armv7l&lt;BR /&gt;[01:31:12.156] Starting with no config file.&lt;BR /&gt;[01:31:12.156] Output repaint window is 7 ms maximum.&lt;BR /&gt;[01:31:12.156] Loading module '/usr/lib/libweston-2/fbdev-backend.so'&lt;BR /&gt;[01:31:12.158] initializing fbdev backend&lt;BR /&gt;[01:31:12.158] Loading module '/usr/lib/libweston-2/g2d-renderer.so'&lt;BR /&gt;[01:31:12.159] Failed to load module: /usr/lib/libweston-2/g2d-renderer.so: undefined symbol: g2d_buf_from_virt_addr&lt;BR /&gt;[01:31:12.160] could not load g2d renderer&lt;BR /&gt;[01:31:12.310] fatal: failed to create compositor backend&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 May 2018 23:22:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Weston-Wayland-g2d-buf-from-virt-addr-undefined/m-p/770840#M119699</guid>
      <dc:creator>michaeldonahoe</dc:creator>
      <dc:date>2018-05-18T23:22:14Z</dc:date>
    </item>
    <item>
      <title>Re: Weston Wayland g2d_buf_from_virt_addr undefined</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Weston-Wayland-g2d-buf-from-virt-addr-undefined/m-p/770841#M119700</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Donahoe,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You are using a different kernel of the BSP 4.1.44, try to use the BSP and you will see the g2d.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 May 2018 14:14:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Weston-Wayland-g2d-buf-from-virt-addr-undefined/m-p/770841#M119700</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2018-05-25T14:14:30Z</dc:date>
    </item>
    <item>
      <title>Re: Weston Wayland g2d_buf_from_virt_addr undefined</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Weston-Wayland-g2d-buf-from-virt-addr-undefined/m-p/770842#M119701</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can you provide some more details I don't follow? &amp;nbsp;g2d is working on the system as I can use the g2d gstreamer&amp;nbsp;elements just fine.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 May 2018 16:32:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Weston-Wayland-g2d-buf-from-virt-addr-undefined/m-p/770842#M119701</guid>
      <dc:creator>michaeldonahoe</dc:creator>
      <dc:date>2018-05-25T16:32:06Z</dc:date>
    </item>
  </channel>
</rss>