<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx537 with linux3.0.101 gpio interrupt not respond</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx537-with-linux3-0-101-gpio-interrupt-not-respond/m-p/770666#M119667</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi dizhu&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try to debug it using AN4553 Using Open Source Debugging&lt;/P&gt;&lt;P&gt;Tools for Linux on i.MX Processors&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fapplication-note%2FAN4553.pdf" rel="nofollow" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN4553.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;and sect.2.1 Interrupts attached Linux Manual&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 20 Mar 2018 23:01:06 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-03-20T23:01:06Z</dc:date>
    <item>
      <title>imx537 with linux3.0.101 gpio interrupt not respond</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx537-with-linux3-0-101-gpio-interrupt-not-respond/m-p/770664#M119665</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;大家好：&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;我移植linux3.0.101到IMX537上，系统可以起来，fec、uart等中断可以响应，GPIO中断不能响应，同样的GPIO驱动在linux2.6.35上可以正常使用，我不知道问题出现在哪里，希望能得到帮助。&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;HI：（google translate）&lt;/P&gt;&lt;P&gt;Hello everyone:&lt;BR /&gt;I transplant linux3.0.101 to IMX537, the system can be up, fec, uart and other interrupts can respond, GPIO interrupt can not respond, the same GPIO driver can be used normally on linux2.6.35, I do not know where the problem occurs, hoping to get help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;root@freescale ~$ cat /proc/interrupts &lt;BR /&gt; CPU0 &lt;BR /&gt; 1: 2348 MXC_TZIC mxsdhci&lt;BR /&gt; 13: 7994 MXC_TZIC IMX-uart&lt;BR /&gt; 39: 59680 MXC_TZIC i.MX Timer Tick&lt;BR /&gt; 64: 14 MXC_TZIC imx-i2c&lt;BR /&gt; 87: 64 MXC_TZIC fec&lt;BR /&gt;225: 0 GPIO da9052_eh&lt;BR /&gt;333: 0 GPIO adc_irq&lt;BR /&gt;Err: 0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;adc-irq open&lt;BR /&gt;irq_no = 333&lt;BR /&gt;gpio_set_irq_type 333 gpio = 205&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&lt;BR /&gt;gpio_unmakse_irq 333 gpio = 205 [gpio / 32] = 6 gpio &amp;amp;0x1f = 13&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Mar 2018 10:03:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx537-with-linux3-0-101-gpio-interrupt-not-respond/m-p/770664#M119665</guid>
      <dc:creator>dizhuyuan</dc:creator>
      <dc:date>2018-03-19T10:03:40Z</dc:date>
    </item>
    <item>
      <title>Re: imx537 with linux3.0.101 gpio interrupt not respond</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx537-with-linux3-0-101-gpio-interrupt-not-respond/m-p/770665#M119666</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;为什么没有人回答我，是我没有把问题描述清楚吗？GPIO配置我已经确认过了，如果我在request_irq的时候把irq直接填为107号中断时，自己通过操作寄存器来GPIO，中断就没法退出，我在想是不是与TZIC控制器有关，但在源码内没有找到GPIO中断与TZIC相关联的代码。&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Mar 2018 13:34:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx537-with-linux3-0-101-gpio-interrupt-not-respond/m-p/770665#M119666</guid>
      <dc:creator>dizhuyuan</dc:creator>
      <dc:date>2018-03-20T13:34:15Z</dc:date>
    </item>
    <item>
      <title>Re: imx537 with linux3.0.101 gpio interrupt not respond</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx537-with-linux3-0-101-gpio-interrupt-not-respond/m-p/770666#M119667</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi dizhu&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try to debug it using AN4553 Using Open Source Debugging&lt;/P&gt;&lt;P&gt;Tools for Linux on i.MX Processors&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fapplication-note%2FAN4553.pdf" rel="nofollow" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN4553.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;and sect.2.1 Interrupts attached Linux Manual&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Mar 2018 23:01:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx537-with-linux3-0-101-gpio-interrupt-not-respond/m-p/770666#M119667</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-03-20T23:01:06Z</dc:date>
    </item>
  </channel>
</rss>