<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: How to configure DDR initialization script with 933MHz DDR3LMemory ?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-configure-DDR-initialization-script-with-933MHz/m-p/770504#M119647</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Customers can use DDR3 script for i.MX6Q:&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-105963"&gt;i.MX6DQ SABRE SDP/B DDR3 Register Programming Aid&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, the following may be helpful:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-101708"&gt;Freescale i.MX6 DRAM Port Application Guide-DDR3&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I.MX6 MMDC supports memory up to 532MHz, there fore all timings&lt;/P&gt;&lt;P&gt;should be selected based on this maximal frequency, say DDR3-800 or DDR3-1060&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 09 Apr 2018 06:38:07 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2018-04-09T06:38:07Z</dc:date>
    <item>
      <title>How to configure DDR initialization script with 933MHz DDR3LMemory ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-configure-DDR-initialization-script-with-933MHz/m-p/770503#M119646</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is a custom hardware design with;&lt;/P&gt;&lt;P&gt;Processor - iMAX6Q -&amp;nbsp;MCIMX6Q6AVT10AC&lt;/P&gt;&lt;P&gt;RAM - 933MHz Micron DDR3L -&amp;nbsp;MT41K256M16TW-107 IT:P&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;1) Here is the configuration for the script. Can you check and tell me the configurations are correct or not ?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/17231i4007CCE555FF75DD/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;2) Don't you have different script generator for DDR3L type memories (Low Power RAM) ?&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;3) In memory type I don't have to select DDR3L-933 option. What should I select ?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;4) In DRAM clock frequency I don't have to select any option for 933MHz. What should I select ?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;5) Under SI configuration section what should I select for&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;DRAM DSE Setting - DQ/DQM (ohm)&lt;/P&gt;&lt;P&gt;DRAM DSE Setting - ADDR/CMD/CTL (ohm)&lt;/P&gt;&lt;P&gt;....etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you give me an idea on this SI configuration parameters. Under which conditions of the memory should we change those values and how ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Waiting for a detailed explanation for this.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards &amp;amp; Thanks,&lt;/P&gt;&lt;P&gt;Peter.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Apr 2018 10:39:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-configure-DDR-initialization-script-with-933MHz/m-p/770503#M119646</guid>
      <dc:creator>peteramond</dc:creator>
      <dc:date>2018-04-06T10:39:08Z</dc:date>
    </item>
    <item>
      <title>Re: How to configure DDR initialization script with 933MHz DDR3LMemory ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-configure-DDR-initialization-script-with-933MHz/m-p/770504#M119647</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Customers can use DDR3 script for i.MX6Q:&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-105963"&gt;i.MX6DQ SABRE SDP/B DDR3 Register Programming Aid&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, the following may be helpful:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-101708"&gt;Freescale i.MX6 DRAM Port Application Guide-DDR3&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I.MX6 MMDC supports memory up to 532MHz, there fore all timings&lt;/P&gt;&lt;P&gt;should be selected based on this maximal frequency, say DDR3-800 or DDR3-1060&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Apr 2018 06:38:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-configure-DDR-initialization-script-with-933MHz/m-p/770504#M119647</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2018-04-09T06:38:07Z</dc:date>
    </item>
  </channel>
</rss>