<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Segmentation fault when running qt5 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Segmentation-fault-when-running-qt5/m-p/770465#M119626</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using an imx6 board (imx6, lec from adlink).&lt;/P&gt;&lt;P&gt;I first used the rovided lec-imx6 recipe for image, which is based on fsl-image-qt5, and I got on startup gnome desktop environment.&lt;/P&gt;&lt;P&gt;But since it is based on old packages (glibc, gstreamer, etc), I had to update to a more updated package.&lt;/P&gt;&lt;P&gt;So, I have bitbake &lt;SPAN&gt;imx-morty -m imx-4.9.11-1.0.0_ga.xml :&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-morty -m imx-4.9.11-1.0.0_ga.xml&lt;BR /&gt;repo sync&lt;BR /&gt; DISTRO=fsl-imx-x11 MACHINE=imx6qsabresd source fsl-setup-release.sh -b build-x11&lt;BR /&gt;bitbake fsl-image-qt5-validation-imx&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use it with the previous (4.1.31) /boot folder (the previous kernel + dtb for the lec blard).&lt;/P&gt;&lt;P&gt;and also copied /lib/modules folder from 4.1.31 kernel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I try to start qt5 example, but it also fails as following:&lt;/P&gt;&lt;P&gt;root@imx6qsabresd:/usr/share/qt5/examples/gui/analogclock# DISPLAY=:0 ./analogclock&lt;BR /&gt;Segmentation fault (core dumped)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The kernel version I am using with&amp;nbsp;NXP i.MX Release Distro 4.9.11-1.0.0 is :&lt;/P&gt;&lt;P&gt;Linux imx6qsabresd 4.1.31-1.2.0+g77f6154 #1 SMP Thu Nov 9 16:01:51 MST 2017 armv7l armv7l armv7l GNU/Linux&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for any suggestion.&lt;/P&gt;&lt;P&gt;Ran&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 Nov 2017 11:24:19 GMT</pubDate>
    <dc:creator>rans</dc:creator>
    <dc:date>2017-11-13T11:24:19Z</dc:date>
    <item>
      <title>Segmentation fault when running qt5</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Segmentation-fault-when-running-qt5/m-p/770465#M119626</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using an imx6 board (imx6, lec from adlink).&lt;/P&gt;&lt;P&gt;I first used the rovided lec-imx6 recipe for image, which is based on fsl-image-qt5, and I got on startup gnome desktop environment.&lt;/P&gt;&lt;P&gt;But since it is based on old packages (glibc, gstreamer, etc), I had to update to a more updated package.&lt;/P&gt;&lt;P&gt;So, I have bitbake &lt;SPAN&gt;imx-morty -m imx-4.9.11-1.0.0_ga.xml :&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-morty -m imx-4.9.11-1.0.0_ga.xml&lt;BR /&gt;repo sync&lt;BR /&gt; DISTRO=fsl-imx-x11 MACHINE=imx6qsabresd source fsl-setup-release.sh -b build-x11&lt;BR /&gt;bitbake fsl-image-qt5-validation-imx&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use it with the previous (4.1.31) /boot folder (the previous kernel + dtb for the lec blard).&lt;/P&gt;&lt;P&gt;and also copied /lib/modules folder from 4.1.31 kernel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I try to start qt5 example, but it also fails as following:&lt;/P&gt;&lt;P&gt;root@imx6qsabresd:/usr/share/qt5/examples/gui/analogclock# DISPLAY=:0 ./analogclock&lt;BR /&gt;Segmentation fault (core dumped)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The kernel version I am using with&amp;nbsp;NXP i.MX Release Distro 4.9.11-1.0.0 is :&lt;/P&gt;&lt;P&gt;Linux imx6qsabresd 4.1.31-1.2.0+g77f6154 #1 SMP Thu Nov 9 16:01:51 MST 2017 armv7l armv7l armv7l GNU/Linux&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for any suggestion.&lt;/P&gt;&lt;P&gt;Ran&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Nov 2017 11:24:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Segmentation-fault-when-running-qt5/m-p/770465#M119626</guid>
      <dc:creator>rans</dc:creator>
      <dc:date>2017-11-13T11:24:19Z</dc:date>
    </item>
  </channel>
</rss>