<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックMfgTool: flash multiple devices in parallel and pass a specific input argument different for each board</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MfgTool-flash-multiple-devices-in-parallel-and-pass-a-specific/m-p/770342#M119604</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using MfgTool (IMX6_L4.9.11_1.0.0_MFG_TOOL) to flash up to 4 devices in parallel for my custom board based on imx6q.&lt;/P&gt;&lt;P&gt;I have my custom .vbs file and everything works fine meaning I am able to flash 4 images properly specifying PortMgrDlg=4 (or -p 4&amp;nbsp; as argument of mfgtoo2.exe).&amp;nbsp; So far so good.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now I would like to extend my usage to flash a board-specific parameter (e.g. MAC address).&lt;/P&gt;&lt;P&gt;As hard requirement I still want to flash 4 boards in parallel (to save time while producing the boards) and I want this input parameter to be different for each of the 4 board (e.g. specific MAC address per board).&lt;/P&gt;&lt;P&gt;I know I can add a custom input argument (in cfg.ini or as extra option with -s while running mfgtool2.exe) but if I do like this, the same extra input argument will be applied to all the 4 devices.&lt;/P&gt;&lt;P&gt;Is there any way to do it per specific board? I mean - one parameter/value for the board connected to port1, another one for the one connected&amp;nbsp; to port2 ,&amp;nbsp; port 3 and port4 respectively?&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 11 Jun 2018 09:09:48 GMT</pubDate>
    <dc:creator>paololacamera</dc:creator>
    <dc:date>2018-06-11T09:09:48Z</dc:date>
    <item>
      <title>MfgTool: flash multiple devices in parallel and pass a specific input argument different for each board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MfgTool-flash-multiple-devices-in-parallel-and-pass-a-specific/m-p/770342#M119604</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using MfgTool (IMX6_L4.9.11_1.0.0_MFG_TOOL) to flash up to 4 devices in parallel for my custom board based on imx6q.&lt;/P&gt;&lt;P&gt;I have my custom .vbs file and everything works fine meaning I am able to flash 4 images properly specifying PortMgrDlg=4 (or -p 4&amp;nbsp; as argument of mfgtoo2.exe).&amp;nbsp; So far so good.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now I would like to extend my usage to flash a board-specific parameter (e.g. MAC address).&lt;/P&gt;&lt;P&gt;As hard requirement I still want to flash 4 boards in parallel (to save time while producing the boards) and I want this input parameter to be different for each of the 4 board (e.g. specific MAC address per board).&lt;/P&gt;&lt;P&gt;I know I can add a custom input argument (in cfg.ini or as extra option with -s while running mfgtool2.exe) but if I do like this, the same extra input argument will be applied to all the 4 devices.&lt;/P&gt;&lt;P&gt;Is there any way to do it per specific board? I mean - one parameter/value for the board connected to port1, another one for the one connected&amp;nbsp; to port2 ,&amp;nbsp; port 3 and port4 respectively?&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Jun 2018 09:09:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MfgTool-flash-multiple-devices-in-parallel-and-pass-a-specific/m-p/770342#M119604</guid>
      <dc:creator>paololacamera</dc:creator>
      <dc:date>2018-06-11T09:09:48Z</dc:date>
    </item>
    <item>
      <title>Re: MfgTool: flash multiple devices in parallel and pass a specific input argument different for each board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MfgTool-flash-multiple-devices-in-parallel-and-pass-a-specific/m-p/770343#M119605</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Paolo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check documentation in&amp;nbsp;Document folder, but I am afraid passing parameter&lt;/P&gt;&lt;P&gt;for particular board is not supported. In general one can customize tool according one's&lt;/P&gt;&lt;P&gt;needs using mfg tool sources:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://github.com/codeauroraforum/mfgtools" title="https://github.com/codeauroraforum/mfgtools"&gt;GitHub - codeauroraforum/mfgtools: Freescale/NXP I.MX Chip image deploy tools.&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jun 2018 10:05:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MfgTool-flash-multiple-devices-in-parallel-and-pass-a-specific/m-p/770343#M119605</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-06-12T10:05:59Z</dc:date>
    </item>
    <item>
      <title>Re: MfgTool: flash multiple devices in parallel and pass a specific input argument different for each board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MfgTool-flash-multiple-devices-in-parallel-and-pass-a-specific/m-p/770344#M119606</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;thanks for your reply.&lt;/P&gt;&lt;P&gt;I've followed your suggestion and I've customized the tool to accept also parameter per hub-port.&lt;/P&gt;&lt;P&gt;My request is now part of the windows branch and was merged (see&amp;nbsp;&lt;A class="link-titled" href="https://github.com/codeauroraforum/mfgtools/pull/30" title="https://github.com/codeauroraforum/mfgtools/pull/30"&gt;Add the possibility to specify parameters specific per hub/port by sigurpol · Pull Request #30 · codeauroraforum/mfgtool…&lt;/A&gt;&amp;nbsp;) .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;Paolo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jun 2018 09:12:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MfgTool-flash-multiple-devices-in-parallel-and-pass-a-specific/m-p/770344#M119606</guid>
      <dc:creator>paololacamera</dc:creator>
      <dc:date>2018-06-20T09:12:50Z</dc:date>
    </item>
  </channel>
</rss>