<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックCustomized QuadSPI Look-up Table/Flash Access Scheme</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Customized-QuadSPI-Look-up-Table-Flash-Access-Scheme/m-p/769567#M119498</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i.MX 7Dual Applications Processor Reference Manual, Rev. 0.1, 08/2016&lt;/P&gt;&lt;P&gt;implies (Section Flash Devices) that a user can create customized QuadSPI Instruction with Look-up Table and Programmable Sequence Engine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Figure 10-17. Serial Flash Access Scheme illustrates a pattern:&lt;/P&gt;&lt;P&gt;Instruction (1 Byte) – Address (3/4 Byte) – Mode &amp;nbsp;(1 Byte) – Dummy (max 64 Byte) – Data&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My Quad-SPI Device expects scheme:&lt;/P&gt;&lt;P&gt;Instruction (1 Byte) – Address (4 Byte) – Value (2+ Byte) – Dummy (max 16) – Data&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With “Value” are two byte sent from i.MX to the device (like length of the data to be read/written)&lt;/P&gt;&lt;P&gt;Is it possible to define such a scheme?&lt;/P&gt;&lt;P&gt;How should the Look-Up Table be defined?&lt;/P&gt;&lt;P&gt;CMD&amp;nbsp;&amp;nbsp; | 0xAB&lt;/P&gt;&lt;P&gt;ADDR&amp;nbsp; | 0x20&lt;/P&gt;&lt;P&gt;???? | 0x0004&lt;/P&gt;&lt;P&gt;DUMMY | 0x0A&lt;/P&gt;&lt;P&gt;READ&amp;nbsp; | 0x04&lt;/P&gt;&lt;P&gt;STOP&amp;nbsp; | 0x00&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #212121;"&gt;Martin&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 08 Jan 2018 15:51:18 GMT</pubDate>
    <dc:creator>martinzohlhuber</dc:creator>
    <dc:date>2018-01-08T15:51:18Z</dc:date>
    <item>
      <title>Customized QuadSPI Look-up Table/Flash Access Scheme</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Customized-QuadSPI-Look-up-Table-Flash-Access-Scheme/m-p/769567#M119498</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i.MX 7Dual Applications Processor Reference Manual, Rev. 0.1, 08/2016&lt;/P&gt;&lt;P&gt;implies (Section Flash Devices) that a user can create customized QuadSPI Instruction with Look-up Table and Programmable Sequence Engine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Figure 10-17. Serial Flash Access Scheme illustrates a pattern:&lt;/P&gt;&lt;P&gt;Instruction (1 Byte) – Address (3/4 Byte) – Mode &amp;nbsp;(1 Byte) – Dummy (max 64 Byte) – Data&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My Quad-SPI Device expects scheme:&lt;/P&gt;&lt;P&gt;Instruction (1 Byte) – Address (4 Byte) – Value (2+ Byte) – Dummy (max 16) – Data&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With “Value” are two byte sent from i.MX to the device (like length of the data to be read/written)&lt;/P&gt;&lt;P&gt;Is it possible to define such a scheme?&lt;/P&gt;&lt;P&gt;How should the Look-Up Table be defined?&lt;/P&gt;&lt;P&gt;CMD&amp;nbsp;&amp;nbsp; | 0xAB&lt;/P&gt;&lt;P&gt;ADDR&amp;nbsp; | 0x20&lt;/P&gt;&lt;P&gt;???? | 0x0004&lt;/P&gt;&lt;P&gt;DUMMY | 0x0A&lt;/P&gt;&lt;P&gt;READ&amp;nbsp; | 0x04&lt;/P&gt;&lt;P&gt;STOP&amp;nbsp; | 0x00&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #212121;"&gt;Martin&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Jan 2018 15:51:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Customized-QuadSPI-Look-up-Table-Flash-Access-Scheme/m-p/769567#M119498</guid>
      <dc:creator>martinzohlhuber</dc:creator>
      <dc:date>2018-01-08T15:51:18Z</dc:date>
    </item>
    <item>
      <title>Re: Customized QuadSPI Look-up Table/Flash Access Scheme</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Customized-QuadSPI-Look-up-Table-Flash-Access-Scheme/m-p/769568#M119499</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Martin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes such sequence can be defined, please look at examples in&lt;/P&gt;&lt;P&gt;sect.10.2.8.1 Example Sequences i.MX7D Reference Manual&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf"&gt;http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jan 2018 08:21:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Customized-QuadSPI-Look-up-Table-Flash-Access-Scheme/m-p/769568#M119499</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-01-09T08:21:07Z</dc:date>
    </item>
  </channel>
</rss>