<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX28 USB Boot Driver and MfgTool in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-USB-Boot-Driver-and-MfgTool/m-p/206404#M11922</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;I am looking for documentation on the USB boot driver in i.MX28. Especially documentation on the Boot loader transaction controller (BLTC) and Plug-in transaction controller (PITC). Also looking for the sourcecode for the updater.sb used with MfgTool and the sources for the OtpAccess.IMG28.sb which seems to be embedded within BitBurner.exe for i.MX28.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;The reason for this is that I would like to modify MfgTool and friends to fetch a new MAC/Serialnr from an external source when a new device is plugged into a USB port.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Anyone got any suggestions?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Best Regards&lt;/P&gt;&lt;P&gt;Odd Skancke&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 30 Jan 2012 14:19:47 GMT</pubDate>
    <dc:creator>OddSkancke</dc:creator>
    <dc:date>2012-01-30T14:19:47Z</dc:date>
    <item>
      <title>i.MX28 USB Boot Driver and MfgTool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-USB-Boot-Driver-and-MfgTool/m-p/206404#M11922</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;I am looking for documentation on the USB boot driver in i.MX28. Especially documentation on the Boot loader transaction controller (BLTC) and Plug-in transaction controller (PITC). Also looking for the sourcecode for the updater.sb used with MfgTool and the sources for the OtpAccess.IMG28.sb which seems to be embedded within BitBurner.exe for i.MX28.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;The reason for this is that I would like to modify MfgTool and friends to fetch a new MAC/Serialnr from an external source when a new device is plugged into a USB port.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Anyone got any suggestions?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Best Regards&lt;/P&gt;&lt;P&gt;Odd Skancke&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jan 2012 14:19:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX28-USB-Boot-Driver-and-MfgTool/m-p/206404#M11922</guid>
      <dc:creator>OddSkancke</dc:creator>
      <dc:date>2012-01-30T14:19:47Z</dc:date>
    </item>
  </channel>
</rss>