<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX7D M4 and eMMC</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7D-M4-and-eMMC/m-p/767478#M119200</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We did something similar using the M4 on the imx6sx but connected to a SD card reader (see &lt;A _jive_internal="true" href="https://community.nxp.com/thread/454825"&gt;SD Card interfacing from M4 via SPI&lt;/A&gt;). Points to note:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. You may not be able to use DMA as this is controlled from the Linux side.&lt;/P&gt;&lt;P&gt;2. If A7 is in sleep mode then certain clocks may not be available or running at reduce speed which will effect data transfer rate.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 23 Feb 2018 08:28:52 GMT</pubDate>
    <dc:creator>mtx512</dc:creator>
    <dc:date>2018-02-23T08:28:52Z</dc:date>
    <item>
      <title>i.MX7D M4 and eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7D-M4-and-eMMC/m-p/767476#M119198</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can M4 have access to eMMC while A7 cores are in sleep?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Feb 2018 12:39:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7D-M4-and-eMMC/m-p/767476#M119198</guid>
      <dc:creator>indirokanovic</dc:creator>
      <dc:date>2018-02-22T12:39:28Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX7D M4 and eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7D-M4-and-eMMC/m-p/767477#M119199</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Indir,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it should be possible, but in this case you must have a driver for M4 to access eMMC and NXP does not provide such driver. With a driver you should be able to access directly to the memory to read/write raw data or you may use a file system.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Carlos&lt;BR /&gt;NXP Technical Support&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Feb 2018 21:48:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7D-M4-and-eMMC/m-p/767477#M119199</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2018-02-22T21:48:07Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX7D M4 and eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7D-M4-and-eMMC/m-p/767478#M119200</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We did something similar using the M4 on the imx6sx but connected to a SD card reader (see &lt;A _jive_internal="true" href="https://community.nxp.com/thread/454825"&gt;SD Card interfacing from M4 via SPI&lt;/A&gt;). Points to note:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. You may not be able to use DMA as this is controlled from the Linux side.&lt;/P&gt;&lt;P&gt;2. If A7 is in sleep mode then certain clocks may not be available or running at reduce speed which will effect data transfer rate.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Feb 2018 08:28:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7D-M4-and-eMMC/m-p/767478#M119200</guid>
      <dc:creator>mtx512</dc:creator>
      <dc:date>2018-02-23T08:28:52Z</dc:date>
    </item>
  </channel>
</rss>