<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: prelink: /usr/sbin/application: Dependency tracing failed</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/prelink-usr-sbin-application-Dependency-tracing-failed/m-p/767460#M119193</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Anshul Khare,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Current i.MX6 BSPs are based in Yocto so there is no documentation regarding PTXdist. Hopefully some community user may be able to provide some insight but I would recommend also posting your question in more PTXdist centric forums.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 27 Feb 2018 16:05:00 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2018-02-27T16:05:00Z</dc:date>
    <item>
      <title>prelink: /usr/sbin/application: Dependency tracing failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/prelink-usr-sbin-application-Dependency-tracing-failed/m-p/767459#M119192</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on imx6 board.&lt;/P&gt;&lt;P&gt;I have created a linux package named "application" using ptxdist. I was able to generate the binary for the application and integrated at /usr/sbin/application. I am able to see the same at the above path.&lt;/P&gt;&lt;P&gt;But, while booting up of the system prelink error occurs for this application. And if I try to run this application, it is saying:&lt;/P&gt;&lt;P&gt;"root@MBa6UL:/usr/sbin application&lt;BR /&gt;-sh: application: not found"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can see from the booting logs that prelink is failed for this particular application only:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"prelink: /usr/sbin/genl-ctrl-list: Using /lib/ld-linux-armhf.so.3, not /lib/ld-linux.so.3 as dynamic linker&lt;BR /&gt;prelink: /usr/sbin/smsc9303: Using /lib/ld-linux-armhf.so.3, not /lib/ld-linux.so.3 as dynamic linker&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;prelink: /usr/sbin/application: Dependency tracing failed&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;prelink: /usr/sbin/partprobe: Using /lib/ld-linux-armhf.so.3, not /lib/ld-linux.so.3 as dynamic linker&lt;BR /&gt;prelink: /usr/sbin/nl-pktloc-lookup: Using /lib/ld-linux-armhf.so.3, not /lib/ld-linux.so.3 as dynamic linker"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kindly tell us what might have gone wrong?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Feb 2018 13:20:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/prelink-usr-sbin-application-Dependency-tracing-failed/m-p/767459#M119192</guid>
      <dc:creator>anshulkhare</dc:creator>
      <dc:date>2018-02-22T13:20:40Z</dc:date>
    </item>
    <item>
      <title>Re: prelink: /usr/sbin/application: Dependency tracing failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/prelink-usr-sbin-application-Dependency-tracing-failed/m-p/767460#M119193</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Anshul Khare,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Current i.MX6 BSPs are based in Yocto so there is no documentation regarding PTXdist. Hopefully some community user may be able to provide some insight but I would recommend also posting your question in more PTXdist centric forums.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Feb 2018 16:05:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/prelink-usr-sbin-application-Dependency-tracing-failed/m-p/767460#M119193</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2018-02-27T16:05:00Z</dc:date>
    </item>
  </channel>
</rss>