<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Latest libGAL and friends</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Latest-libGAL-and-friends/m-p/767227#M119150</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is the only source for the iMX6 GPU in the Yocto project?&lt;/P&gt;&lt;P&gt;&amp;nbsp;-&amp;gt;&amp;nbsp;downloads.yoctoproject.org/mirror/sources/imx-gpu-viv-5.0.11.p8.3-hfp.bin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there an up-to-date version somewhere?&amp;nbsp; This was from 2016 &amp;gt;&amp;lt; and have long since expired since the xserver uses new ABIs and such.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 08 Jun 2018 16:31:26 GMT</pubDate>
    <dc:creator>natesigrist</dc:creator>
    <dc:date>2018-06-08T16:31:26Z</dc:date>
    <item>
      <title>Latest libGAL and friends</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Latest-libGAL-and-friends/m-p/767227#M119150</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is the only source for the iMX6 GPU in the Yocto project?&lt;/P&gt;&lt;P&gt;&amp;nbsp;-&amp;gt;&amp;nbsp;downloads.yoctoproject.org/mirror/sources/imx-gpu-viv-5.0.11.p8.3-hfp.bin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there an up-to-date version somewhere?&amp;nbsp; This was from 2016 &amp;gt;&amp;lt; and have long since expired since the xserver uses new ABIs and such.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Jun 2018 16:31:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Latest-libGAL-and-friends/m-p/767227#M119150</guid>
      <dc:creator>natesigrist</dc:creator>
      <dc:date>2018-06-08T16:31:26Z</dc:date>
    </item>
    <item>
      <title>Re: Latest libGAL and friends</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Latest-libGAL-and-friends/m-p/767228#M119151</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nate&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at latest Linux 4.9.88_2.0.0 BSP, use Yocto Guide for bilding:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/webapp/Download?colCode=L4.9.88_2.0.0_LINUX_DOCS&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product" title="https://www.nxp.com/webapp/Download?colCode=L4.9.88_2.0.0_LINUX_DOCS&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product"&gt;https://www.nxp.com/webapp/Download?colCode=L4.9.88_2.0.0_LINUX_DOCS&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageTyp…&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 Jun 2018 03:25:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Latest-libGAL-and-friends/m-p/767228#M119151</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-06-09T03:25:03Z</dc:date>
    </item>
    <item>
      <title>Re: Latest libGAL and friends</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Latest-libGAL-and-friends/m-p/767229#M119152</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/igorpadykov"&gt;igorpadykov&lt;/A&gt;‌ Thanks for the documentation :-)&amp;nbsp; However, my question was about the most recent location to &lt;EM&gt;find&lt;/EM&gt; these binaries.&amp;nbsp; Obviously, Preferably source code...&amp;nbsp; So where might I find these library files???&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Jun 2018 15:35:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Latest-libGAL-and-friends/m-p/767229#M119152</guid>
      <dc:creator>natesigrist</dc:creator>
      <dc:date>2018-06-11T15:35:55Z</dc:date>
    </item>
    <item>
      <title>Re: Latest libGAL and friends</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Latest-libGAL-and-friends/m-p/767230#M119153</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Also, why is this assumed answered?!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Jun 2018 15:37:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Latest-libGAL-and-friends/m-p/767230#M119153</guid>
      <dc:creator>natesigrist</dc:creator>
      <dc:date>2018-06-11T15:37:48Z</dc:date>
    </item>
    <item>
      <title>Re: Latest libGAL and friends</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Latest-libGAL-and-friends/m-p/767231#M119154</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Here is a reference to the work I've done in so far in implementing the proprietary binaries,&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/477594"&gt;https://community.nxp.com/thread/477594&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Jun 2018 18:42:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Latest-libGAL-and-friends/m-p/767231#M119154</guid>
      <dc:creator>natesigrist</dc:creator>
      <dc:date>2018-06-11T18:42:53Z</dc:date>
    </item>
  </channel>
</rss>