<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックiMX27 Advanced Toolkit adding new NAND type</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX27-Advanced-Toolkit-adding-new-NAND-type/m-p/765996#M118974</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a legacy iMX27 based processor board that requires support for a new type of NAND FLASH as the old one is obsolete.&amp;nbsp; I found this application note which details the procedure to add a custom NAND support to Advanced toolkit:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN3985.pdf" title="https://www.nxp.com/docs/en/application-note/AN3985.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN3985.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Problem is I am unable to find any of the prerequisite source code on the NXP site, all links I had were from the old Freescale site and are no longer valid.&amp;nbsp; In particular I need the Tool and Source Code Packages as shown in section 1.1 of the PDF:&lt;/P&gt;&lt;P&gt;------------&lt;BR /&gt;Download the latest ATK tool and source code packages from Freescale website. If they are not available&lt;BR /&gt;in the website, contact the Freescale representative to get access to the following packages.&lt;BR /&gt;• FSL_ATK_STD_v_vv.zip&lt;BR /&gt;— FSL_ATK_TOOL_STD_v_vv&lt;BR /&gt;a) ATK User's Guide Standard Version.pdf&lt;BR /&gt;b) FSL_ATK_TOOL_WINS_STD_INSTALL_v_vv.exe&lt;BR /&gt;— FSL_ATK_SRC_STD_v_vv&lt;BR /&gt;a) ATK Reference Manual Standard Version.pdf&lt;BR /&gt;b) FSL_ATK_SOURCE_CODE_STD_v_vv.exe&lt;BR /&gt;NOTE&lt;BR /&gt;v_vv is the version number corresponding to the latest ATK release.&lt;BR /&gt;Install the packages using the setup (.exe) files. Note the folder path where the software&lt;/P&gt;&lt;P&gt;------------&lt;/P&gt;&lt;P&gt;The old (invalid) link to these files was&amp;nbsp;&lt;A class="jivelink2" href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX25PDK&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX25PDK&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX25PDK&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyone know of an updated link to these files?&lt;/P&gt;&lt;P&gt;Also, wrt to the cygwin based development tools does anyone know of an alternate tool to use to build the binaries?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;--&lt;/P&gt;&lt;P&gt;Al&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Apr 2018 19:21:56 GMT</pubDate>
    <dc:creator>ambw</dc:creator>
    <dc:date>2018-04-24T19:21:56Z</dc:date>
    <item>
      <title>iMX27 Advanced Toolkit adding new NAND type</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX27-Advanced-Toolkit-adding-new-NAND-type/m-p/765996#M118974</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a legacy iMX27 based processor board that requires support for a new type of NAND FLASH as the old one is obsolete.&amp;nbsp; I found this application note which details the procedure to add a custom NAND support to Advanced toolkit:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN3985.pdf" title="https://www.nxp.com/docs/en/application-note/AN3985.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN3985.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Problem is I am unable to find any of the prerequisite source code on the NXP site, all links I had were from the old Freescale site and are no longer valid.&amp;nbsp; In particular I need the Tool and Source Code Packages as shown in section 1.1 of the PDF:&lt;/P&gt;&lt;P&gt;------------&lt;BR /&gt;Download the latest ATK tool and source code packages from Freescale website. If they are not available&lt;BR /&gt;in the website, contact the Freescale representative to get access to the following packages.&lt;BR /&gt;• FSL_ATK_STD_v_vv.zip&lt;BR /&gt;— FSL_ATK_TOOL_STD_v_vv&lt;BR /&gt;a) ATK User's Guide Standard Version.pdf&lt;BR /&gt;b) FSL_ATK_TOOL_WINS_STD_INSTALL_v_vv.exe&lt;BR /&gt;— FSL_ATK_SRC_STD_v_vv&lt;BR /&gt;a) ATK Reference Manual Standard Version.pdf&lt;BR /&gt;b) FSL_ATK_SOURCE_CODE_STD_v_vv.exe&lt;BR /&gt;NOTE&lt;BR /&gt;v_vv is the version number corresponding to the latest ATK release.&lt;BR /&gt;Install the packages using the setup (.exe) files. Note the folder path where the software&lt;/P&gt;&lt;P&gt;------------&lt;/P&gt;&lt;P&gt;The old (invalid) link to these files was&amp;nbsp;&lt;A class="jivelink2" href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX25PDK&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX25PDK&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX25PDK&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyone know of an updated link to these files?&lt;/P&gt;&lt;P&gt;Also, wrt to the cygwin based development tools does anyone know of an alternate tool to use to build the binaries?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;--&lt;/P&gt;&lt;P&gt;Al&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Apr 2018 19:21:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX27-Advanced-Toolkit-adding-new-NAND-type/m-p/765996#M118974</guid>
      <dc:creator>ambw</dc:creator>
      <dc:date>2018-04-24T19:21:56Z</dc:date>
    </item>
    <item>
      <title>Re: iMX27 Advanced Toolkit adding new NAND type</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX27-Advanced-Toolkit-adding-new-NAND-type/m-p/765997#M118975</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Allan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for obtaining atk sources one can create service request&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-329745"&gt;How to submit a new question for NXP Support&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Apr 2018 23:03:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX27-Advanced-Toolkit-adding-new-NAND-type/m-p/765997#M118975</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-04-24T23:03:44Z</dc:date>
    </item>
  </channel>
</rss>