<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: im53 QSB Android Boot hangs up in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/im53-QSB-Android-Boot-hangs-up/m-p/206204#M11873</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You need to enable "Stay awake" in Settings | Applications | Development&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 30 Jan 2012 09:24:16 GMT</pubDate>
    <dc:creator>rlorriaux</dc:creator>
    <dc:date>2012-01-30T09:24:16Z</dc:date>
    <item>
      <title>im53 QSB Android Boot hangs up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/im53-QSB-Android-Boot-hangs-up/m-p/206197#M11866</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;Finally I managed to build android image for imx53 QSB but now I can not get into &amp;nbsp;Android Home Screen because CPU hangs up somewhere. I believe it's is due to touch &amp;nbsp;screen calibration but could not find how to disable touch screeen calibration at startup. I know it's about bootargs in uBoot but documentation is not clear enought to understand the way yo disable it. Attached is the serial log during boot up.&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/discussions/385-putty.log" target="_self"&gt;Serial log of boot&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Last traces are these:&lt;/P&gt;&lt;P&gt;Freeing init memory: 196K&lt;BR /&gt; init: cannot open '/initlogo.rle'&lt;BR /&gt; EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)&lt;BR /&gt; EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)&lt;BR /&gt; EXT4-fs (mmcblk0p5): recovery complete&lt;BR /&gt; EXT4-fs (mmcblk0p5): mounted filesystem with ordered data mode. Opts: nodelalloc&lt;BR /&gt; EXT4-fs (mmcblk0p6): recovery complete&lt;BR /&gt; EXT4-fs (mmcblk0p6): mounted filesystem with ordered data mode. Opts: (null)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jan 2012 07:45:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/im53-QSB-Android-Boot-hangs-up/m-p/206197#M11866</guid>
      <dc:creator>TugrulGuclu</dc:creator>
      <dc:date>2012-01-30T07:45:39Z</dc:date>
    </item>
    <item>
      <title>Re: im53 QSB Android Boot hangs up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/im53-QSB-Android-Boot-hangs-up/m-p/206198#M11867</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Try booting by removing any connected USB device. Be patient, first boot takes some time, since some SD card contents recreated. (i think because of dex file decompression or smtg similar. )&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jan 2012 08:20:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/im53-QSB-Android-Boot-hangs-up/m-p/206198#M11867</guid>
      <dc:creator>AhmetYUCE</dc:creator>
      <dc:date>2012-01-30T08:20:18Z</dc:date>
    </item>
    <item>
      <title>Re: im53 QSB Android Boot hangs up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/im53-QSB-Android-Boot-hangs-up/m-p/206199#M11868</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I removed my USB &amp;nbsp;keyboard - nothing happened.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Then from uBoot settings I removed "calibration" in lcd variable. Now it still hangs up but now traces are different. see the attached file please&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jan 2012 08:36:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/im53-QSB-Android-Boot-hangs-up/m-p/206199#M11868</guid>
      <dc:creator>TugrulGuclu</dc:creator>
      <dc:date>2012-01-30T08:36:43Z</dc:date>
    </item>
    <item>
      <title>Re: im53 QSB Android Boot hangs up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/im53-QSB-Android-Boot-hangs-up/m-p/206200#M11869</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I'm using iMX53-QSB without touchscreen using vga monitor. Didn't get such an issue. The only change i've made to u-boot params was changing default display from lcd to vga.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jan 2012 08:47:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/im53-QSB-Android-Boot-hangs-up/m-p/206200#M11869</guid>
      <dc:creator>AhmetYUCE</dc:creator>
      <dc:date>2012-01-30T08:47:55Z</dc:date>
    </item>
    <item>
      <title>Re: im53 QSB Android Boot hangs up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/im53-QSB-Android-Boot-hangs-up/m-p/206201#M11870</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I modified them too. Below is the output from U-Boot&amp;gt;printenv&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MX53-LOCO U-Boot &amp;gt; printenv vga&lt;BR /&gt;vga=setenv bootargs di1_primary video=mxcdi1fb:GBR24,1024x768@60 vga&lt;BR /&gt;MX53-LOCO U-Boot &amp;gt; vga=setenv bootargs di1_primary video=mxcdi1fb:GBR24,1024x768@60 vga&lt;BR /&gt;Unknown command 'vga=setenv' - try 'help'&lt;BR /&gt;MX53-LOCO U-Boot &amp;gt; printenv&lt;BR /&gt;baudrate=115200&lt;BR /&gt;loadaddr=0x70800000&lt;BR /&gt;netdev=eth0&lt;BR /&gt;ethprime=FEC0&lt;BR /&gt;uboot=u-boot.bin&lt;BR /&gt;kernel=uImage&lt;BR /&gt;loadaddr=0x70800000&lt;BR /&gt;rd_loadaddr=0x70D00000&lt;BR /&gt;nfsroot=/opt/eldk/arm&lt;BR /&gt;bootargs_base=setenv bootargs console=ttymxc0,115200&lt;BR /&gt;hdmi_720p=setenv bootargs ${bootargs} di0_primary video=mxcdi0fb:RGB24,1280x720M@60 hdmi gpu_nommu gpu_memory=64M&lt;BR /&gt;hdmi_1080p=setenv bootargs ${bootargs} di0_primary video=mxcdi0fb:RGB24,1080P60 hdmi gpu_nommu gpu_memory=64M&lt;BR /&gt;claa_lcd=setenv bootargs ${bootargs} di0_primary video=mxcdi0fb:RGB565,CLAA-WVGA calibration&lt;BR /&gt;set_display=run lcd&lt;BR /&gt;bootargs_android=setenv bootargs ${bootargs} init=/init androidboot.console=ttymxc0&lt;BR /&gt;bootcmd=run bootcmd_SD&lt;BR /&gt;bootcmd_SD=run bootcmd_SD1 bootcmd_SD2&lt;BR /&gt;bootcmd_SD1=run bootargs_base set_display bootargs_android&lt;BR /&gt;bootcmd_SD2=mmc read 0 ${loadaddr} 0x800 0x2000;mmc read 0 ${rd_loadaddr} 0x3000 0x300;bootm ${loadaddr} ${rd_loadaddr}&lt;BR /&gt;bootargs_nfs=setenv bootargs ${bootargs} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp&lt;BR /&gt;bootcmd_net=run bootargs_base bootargs_nfs; tftpboot ${loadaddr} ${kernel}; bootm&lt;BR /&gt;bootcmd_android_recovery=run bootargs_base bootargs_android_recovery;mmc read 0 ${loadaddr} 0x800 0x2000;bootm&lt;BR /&gt;bootargs_android_recovery=setenv bootargs ${bootargs} init=/init root=/dev/mmcblk0p4 rootfs=ext4&lt;BR /&gt;ethact=FEC0&lt;BR /&gt;bootdelay=3&lt;BR /&gt;bootdelay=3&lt;BR /&gt;lcd=setenv bootargs di0_primary calibration&lt;BR /&gt;vga=setenv bootargs di1_primary video=mxcdi1fb:GBR24,1024x768@60 vga&lt;BR /&gt;stdin=serial&lt;BR /&gt;stdout=serial&lt;BR /&gt;stderr=serial&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jan 2012 08:56:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/im53-QSB-Android-Boot-hangs-up/m-p/206201#M11870</guid>
      <dc:creator>TugrulGuclu</dc:creator>
      <dc:date>2012-01-30T08:56:51Z</dc:date>
    </item>
    <item>
      <title>Re: im53 QSB Android Boot hangs up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/im53-QSB-Android-Boot-hangs-up/m-p/206202#M11871</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It worked.&lt;/P&gt;&lt;P&gt;I changed&amp;nbsp;&lt;SPAN&gt;set_display=run vga&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jan 2012 08:59:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/im53-QSB-Android-Boot-hangs-up/m-p/206202#M11871</guid>
      <dc:creator>TugrulGuclu</dc:creator>
      <dc:date>2012-01-30T08:59:07Z</dc:date>
    </item>
    <item>
      <title>Re: im53 QSB Android Boot hangs up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/im53-QSB-Android-Boot-hangs-up/m-p/206203#M11872</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;VGA connection is suspended after a while.&lt;/P&gt;&lt;P&gt;I think it's about suspend mode. Do you know how to disable suspend mode ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jan 2012 09:09:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/im53-QSB-Android-Boot-hangs-up/m-p/206203#M11872</guid>
      <dc:creator>TugrulGuclu</dc:creator>
      <dc:date>2012-01-30T09:09:28Z</dc:date>
    </item>
    <item>
      <title>Re: im53 QSB Android Boot hangs up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/im53-QSB-Android-Boot-hangs-up/m-p/206204#M11873</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You need to enable "Stay awake" in Settings | Applications | Development&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jan 2012 09:24:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/im53-QSB-Android-Boot-hangs-up/m-p/206204#M11873</guid>
      <dc:creator>rlorriaux</dc:creator>
      <dc:date>2012-01-30T09:24:16Z</dc:date>
    </item>
    <item>
      <title>Re: im53 QSB Android Boot hangs up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/im53-QSB-Android-Boot-hangs-up/m-p/206205#M11874</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm not sure if it's related, but I found that a similar issue was triggered by trying to mount an EXT4 partition that didn't exist on an i.MX6 SABRE Lite board.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A href="http://boundarydevices.com/android-r13-4-ga-for-i-mx6-in-stages-stage-2-booting-sd-card/#update" title="http://boundarydevices.com/android-r13-4-ga-for-i-mx6-in-stages-stage-2-booting-sd-card/#update"&gt;http://boundarydevices.com/android-r13-4-ga-for-i-mx6-in-stages-stage-2-booting-sd-card/#update&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the i.MX6 case, the system call &amp;lt;tt&amp;gt;mount_bdev&amp;lt;/tt&amp;gt; wouldn't return until a wake event (hard key or USB plug/unplug).&lt;/P&gt;&lt;P&gt;A mount error message was generated, but the system call didn't return. It appears that the system entered a sleep state at some point in the return path. More details are available in this Linaro bug report.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://bugs.launchpad.net/linaro-android/+bug/966114/comments/7" title="https://bugs.launchpad.net/linaro-android/+bug/966114/comments/7"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Comment #7 : Bug #966114 : Bugs : Linaro Android&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Oct 2012 23:53:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/im53-QSB-Android-Boot-hangs-up/m-p/206205#M11874</guid>
      <dc:creator>EricNelson</dc:creator>
      <dc:date>2012-10-25T23:53:25Z</dc:date>
    </item>
  </channel>
</rss>