<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.mx7 without internal RTC but SNVS tamper</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-mx7-without-internal-RTC-but-SNVS-tamper/m-p/764002#M118684</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lars&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it is not possible to disable the internal RTC, please refer to its description in i.MX7D Datasheet&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcache.nxp.com%2Ffiles%2F32bit%2Fdoc%2Fdata_sheet%2FIMX7DCEC.pdf" rel="nofollow" target="_blank"&gt;http://cache.nxp.com/files/32bit/doc/data_sheet/IMX7DCEC.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;May the RTC Oscillator/Pins be left unconnected if an externl RTC is used?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;recommended to tie&amp;nbsp;RTC_XTALI to GND and RTC_XTALO leave unconnected, so the on-chip&lt;BR /&gt;oscillator is automatically engaged.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;Does this have any effect on this power domain setup?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;no&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 Nov 2017 23:35:37 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-11-09T23:35:37Z</dc:date>
    <item>
      <title>i.mx7 without internal RTC but SNVS tamper</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx7-without-internal-RTC-but-SNVS-tamper/m-p/764001#M118683</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello community!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Quick question on the possibility of the following:&lt;/P&gt;&lt;P&gt;Both tamper detection and RTC are needed. Based on &lt;A href="https://community.nxp.com/thread/459594"&gt;i.MX7/PF3000 RTC Backup Power&lt;/A&gt;&amp;nbsp;an external RTC will be used. Tamper and internal RTC are both powered by SNVS power domain.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to disable the internal RTC while still using tamper detection?&lt;BR /&gt;May the RTC Oscillator/Pins be left unconnected if an externl RTC is used?&amp;nbsp;Does this have any effect on this power domain setup?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;BR /&gt;Lars&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Nov 2017 13:40:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx7-without-internal-RTC-but-SNVS-tamper/m-p/764001#M118683</guid>
      <dc:creator>demoniacmilk</dc:creator>
      <dc:date>2017-11-09T13:40:47Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx7 without internal RTC but SNVS tamper</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx7-without-internal-RTC-but-SNVS-tamper/m-p/764002#M118684</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lars&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it is not possible to disable the internal RTC, please refer to its description in i.MX7D Datasheet&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcache.nxp.com%2Ffiles%2F32bit%2Fdoc%2Fdata_sheet%2FIMX7DCEC.pdf" rel="nofollow" target="_blank"&gt;http://cache.nxp.com/files/32bit/doc/data_sheet/IMX7DCEC.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;May the RTC Oscillator/Pins be left unconnected if an externl RTC is used?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;recommended to tie&amp;nbsp;RTC_XTALI to GND and RTC_XTALO leave unconnected, so the on-chip&lt;BR /&gt;oscillator is automatically engaged.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;Does this have any effect on this power domain setup?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;no&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Nov 2017 23:35:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx7-without-internal-RTC-but-SNVS-tamper/m-p/764002#M118684</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-11-09T23:35:37Z</dc:date>
    </item>
  </channel>
</rss>