<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Python-Opencv based on Yocto in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Python-Opencv-based-on-Yocto/m-p/763656#M118629</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm currently working on a project related to python programming.&lt;/P&gt;&lt;P&gt;I need to use python-openCV for the project, which will later run in I.MX6 board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, I will need to bind the prebuild openCV package in Yocto to python (not C/C++)&lt;/P&gt;&lt;P&gt;How can it be done in Yocto?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Because usually, python-openCv and openCv will give different library when installed in computer.&lt;/P&gt;&lt;P&gt;Fyi, the image i'm building is the core-image-weston.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 27 Jan 2018 09:56:51 GMT</pubDate>
    <dc:creator>nurulhidayah</dc:creator>
    <dc:date>2018-01-27T09:56:51Z</dc:date>
    <item>
      <title>Python-Opencv based on Yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Python-Opencv-based-on-Yocto/m-p/763656#M118629</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm currently working on a project related to python programming.&lt;/P&gt;&lt;P&gt;I need to use python-openCV for the project, which will later run in I.MX6 board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, I will need to bind the prebuild openCV package in Yocto to python (not C/C++)&lt;/P&gt;&lt;P&gt;How can it be done in Yocto?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Because usually, python-openCv and openCv will give different library when installed in computer.&lt;/P&gt;&lt;P&gt;Fyi, the image i'm building is the core-image-weston.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 27 Jan 2018 09:56:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Python-Opencv-based-on-Yocto/m-p/763656#M118629</guid>
      <dc:creator>nurulhidayah</dc:creator>
      <dc:date>2018-01-27T09:56:51Z</dc:date>
    </item>
    <item>
      <title>Re: Python-Opencv based on Yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Python-Opencv-based-on-Yocto/m-p/763657#M118630</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;You can refer to&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/451174"&gt;Install python-opencv module&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-335197"&gt;opencv 3.1 supports on the mx6q board&lt;/A&gt; &lt;BR /&gt;Have a great day,&lt;BR /&gt;Rita&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jan 2018 08:48:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Python-Opencv-based-on-Yocto/m-p/763657#M118630</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2018-01-30T08:48:19Z</dc:date>
    </item>
  </channel>
</rss>